QSPI Device Read Instruction Configuration Structure.

Public Attributes#

uint8_t

Read opcode in non-xip mode.

uint8_t

Number of dummy read clock cycles.

Transfer type used for address.

Transfer type used for data.

Transfer type used for instruction.

Public Attribute Documentation#

opCode#

uint8_t QSPI_ReadConfig_TypeDef::opCode

Read opcode in non-xip mode.


Definition at line 79 of file platform/emlib/inc/em_qspi.h

dummyCycles#

uint8_t QSPI_ReadConfig_TypeDef::dummyCycles

Number of dummy read clock cycles.


Definition at line 82 of file platform/emlib/inc/em_qspi.h

addrTransfer#

QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::addrTransfer

Transfer type used for address.


Definition at line 85 of file platform/emlib/inc/em_qspi.h

dataTransfer#

QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::dataTransfer

Transfer type used for data.


Definition at line 88 of file platform/emlib/inc/em_qspi.h

instTransfer#

QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::instTransfer

Transfer type used for instruction.


Definition at line 91 of file platform/emlib/inc/em_qspi.h