Alternate excitation descriptor structure.

Public Attributes#

bool

Configure alternate excitation pins.

Configure idle phase setup of alternate excitation pins.

bool

Configure how to control external alternate excitation pins.

Public Attribute Documentation#

enablePin#

bool LESENSE_AltExDesc_TypeDef::enablePin

Configure alternate excitation pins.

If set, the corresponding alternate excitation pin/signal is enabled.


Definition at line 1210 of file platform/emlib/inc/em_lesense.h

idleConf#

LESENSE_AltExPinIdle_TypeDef LESENSE_AltExDesc_TypeDef::idleConf

Configure idle phase setup of alternate excitation pins.

The idleConf parameter is not valid when altExMap==lesenseAltExMapACMP.


Definition at line 1215 of file platform/emlib/inc/em_lesense.h

alwaysEx#

bool LESENSE_AltExDesc_TypeDef::alwaysEx

Configure how to control external alternate excitation pins.

Only applies if altExMap has been set to lesenseAltExMapALTEX. If true, excitation happens on the corresponding alternate excitation pin during excitation periods of all the enabled channels. If false, excitation happens on the corresponding alternate excitation pin ONLY during excitation period of the corresponding channel. The alwaysEx parameter is not valid when altExMap==lesenseAltExMapACMP.


Definition at line 1224 of file platform/emlib/inc/em_lesense.h