RMU - Reset Management Unit#
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Enumerations#
RMU reset modes.
RMU controlled peripheral reset control and reset source control.
Functions#
Disable/enable reset for various peripherals and signal sources.
Clear the reset cause register.
Get the cause of the last reset.
Set user reset state.
Get user reset state.
Macros#
RMU_LockupResetDisable kept for backwards compatibility.
Enumeration Documentation#
RMU_ResetMode_TypeDef#
RMU_ResetMode_TypeDef
RMU reset modes.
| Enumerator | |
|---|---|
| rmuResetModeDisabled | Reset mode disabled. |
| rmuResetModeLimited | Reset mode limited. |
| rmuResetModeExtended | Reset mode extended. |
| rmuResetModeFull | Reset mode full. |
RMU_Reset_TypeDef#
RMU_Reset_TypeDef
RMU controlled peripheral reset control and reset source control.
| Enumerator | |
|---|---|
| rmuResetLockUp | Cortex lockup reset select. |
| rmuResetWdog | WDOG reset select. |
| rmuResetCoreLockup | Cortex lockup reset select. |
| rmuResetSys | SYSRESET select. |
| rmuResetPin | Pin reset select. |
Function Documentation#
RMU_ResetControl#
void RMU_ResetControl (RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode)
Disable/enable reset for various peripherals and signal sources.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RMU_Reset_TypeDef | [in] | reset | Reset types to enable/disable.s |
| RMU_ResetMode_TypeDef | [in] | mode | Reset mode. |
RMU_ResetCauseClear#
void RMU_ResetCauseClear (void )
Clear the reset cause register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet().
RMU_ResetCauseGet#
uint32_t RMU_ResetCauseGet (void )
Get the cause of the last reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear(). This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
Returns
A reset cause mask. See the reference manual for a description of the reset cause mask.
RMU_UserResetStateSet#
void RMU_UserResetStateSet (uint32_t userState)
Set user reset state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | userState | User state to set |
Reset only by a Power-on-reset and a pin reset.
RMU_UserResetStateGet#
uint32_t RMU_UserResetStateGet (void )
Get user reset state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Reset only by a Power-on-reset and a pin reset.
Returns
Reset surviving user state.