You are viewing documentation for version:
HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
uint8_t
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.
bool
Enable/disable glitch detector.
Public Attribute Documentation#
boost#
uint8_t CMU_HFXOInit_TypeDef::boost
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.
timeout#
uint8_t CMU_HFXOInit_TypeDef::timeout
Startup delay.
glitchDetector#
bool CMU_HFXOInit_TypeDef::glitchDetector
Enable/disable glitch detector.
mode#
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode
Oscillator mode.