VDAC - Voltage DAC#
Digital to Analog Voltage Converter (VDAC) Peripheral API.
This module contains functions to control the VDAC peripheral of Silicon Labs' 32-bit MCUs and SoCs. VDAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. VDAC is designed for low energy consumption, but can also provide very good performance.
The following steps are necessary for basic operation:
Clock enable:
CMU_ClockEnable(cmuClock_VDAC0, true);
Initialize the VDAC with default settings and modify selected fields:
VDAC_Init_TypeDef vdacInit = VDAC_INIT_DEFAULT;
VDAC_InitChannel_TypeDef vdacChInit = VDAC_INITCHANNEL_DEFAULT;
// Set prescaler to get 1 MHz VDAC clock frequency.
vdacInit.prescaler = VDAC_PrescaleCalc(1000000, true, 0); // function call for series 0/1
VDAC_Init(VDAC0, &vdacInit);
vdacChInit.enable = true;
VDAC_InitChannel(VDAC0, &vdacChInit, 0);
Perform a conversion:
VDAC_ChannelOutputSet(VDAC0, 0, 250);
Note
The output stage of a VDAC channel consists of an on-chip operational amplifier (OPAMP) in the OPAMP module. This OPAMP is highly configurable; and to exploit the VDAC functionality fully, configure the OPAMP using the OPAMP API. Using the OPAMP API also loads OPAMP calibration values. The default (reset) settings of OPAMP is sufficient for many applications.
Modules#
Enumerations#
Channel refresh period.
Reference voltage for VDAC.
Peripheral Reflex System signal used to trigger VDAC channel conversion.
Channel conversion trigger mode.
Functions#
Set the output signal of a VDAC channel to a given value.
Enable/disable the VDAC channel.
Initialize VDAC.
Initialize a VDAC channel.
Set the output signal of VDAC channel 0 to a given value.
Set the output signal of VDAC channel 1 to a given value.
Clear one or more pending VDAC interrupts.
Disable one or more VDAC interrupts.
Enable one or more VDAC interrupts.
Get pending VDAC interrupt flags.
Get enabled and pending VDAC interrupt flags.
Set one or more pending VDAC interrupts from SW.
Calculate the prescaler value used to determine VDAC clock.
Reset VDAC to same state that it was in after a hardwares reset.
Macros#
Default configuration for VDAC initialization structure.
Default configuration for VDAC channel initialization structure.
Enumeration Documentation#
VDAC_Refresh_TypeDef#
VDAC_Refresh_TypeDef
Channel refresh period.
| Enumerator | |
|---|---|
| vdacRefresh8 | Refresh every 8 clock cycles. |
| vdacRefresh16 | Refresh every 16 clock cycles. |
| vdacRefresh32 | Refresh every 32 clock cycles. |
| vdacRefresh64 | Refresh every 64 clock cycles. |
VDAC_Ref_TypeDef#
VDAC_Ref_TypeDef
Reference voltage for VDAC.
| Enumerator | |
|---|---|
| vdacRef1V25Ln | Internal low noise 1.25 V band gap reference. |
| vdacRef2V5Ln | Internal low noise 2.5 V band gap reference. |
| vdacRef1V25 | Internal 1.25 V band gap reference. |
| vdacRef2V5 | Internal 2.5 V band gap reference. |
| vdacRefAvdd | AVDD reference. |
| vdacRefExtPin | External pin reference. |
VDAC_PrsSel_TypeDef#
VDAC_PrsSel_TypeDef
Peripheral Reflex System signal used to trigger VDAC channel conversion.
| Enumerator | |
|---|---|
| vdacPrsSelCh0 | PRS ch 0 triggers conversion. |
| vdacPrsSelCh1 | PRS ch 1 triggers conversion. |
| vdacPrsSelCh2 | PRS ch 2 triggers conversion. |
| vdacPrsSelCh3 | PRS ch 3 triggers conversion. |
| vdacPrsSelCh4 | PRS ch 4 triggers conversion. |
| vdacPrsSelCh5 | PRS ch 5 triggers conversion. |
| vdacPrsSelCh6 | PRS ch 6 triggers conversion. |
| vdacPrsSelCh7 | PRS ch 7 triggers conversion. |
VDAC_TrigMode_TypeDef#
VDAC_TrigMode_TypeDef
Channel conversion trigger mode.
| Enumerator | |
|---|---|
| vdacTrigModeSw | Channel is triggered by CHnDATA or COMBDATA write. |
| vdacTrigModePrs | Channel is triggered by PRS input. |
| vdacTrigModeRefresh | Channel is triggered by Refresh timer. |
| vdacTrigModeSwPrs | Channel is triggered by CHnDATA/COMBDATA write or PRS input. |
| vdacTrigModeSwRefresh | Channel is triggered by CHnDATA/COMBDATA write or Refresh timer. |
| vdacTrigModeLesense | Channel is triggered by LESENSE. |
Function Documentation#
VDAC_ChannelOutputSet#
void VDAC_ChannelOutputSet (VDAC_TypeDef * vdac, unsigned int channel, uint32_t value)
Set the output signal of a VDAC channel to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | A pointer to the VDAC peripheral register block. |
| unsigned int | [in] | channel | A channel number to set the output of. |
| uint32_t | [in] | value | A value to write to the channel output register CHnDATA. |
This function sets the output signal of a VDAC channel by writing value to the corresponding CHnDATA register.
VDAC_Enable#
void VDAC_Enable (VDAC_TypeDef * vdac, unsigned int ch, bool enable)
Enable/disable the VDAC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | A pointer to the VDAC peripheral register block. |
| unsigned int | [in] | ch | A channel to enable/disable. |
| bool | [in] | enable | True to enable VDAC channel, false to disable. |
VDAC_Init#
void VDAC_Init (VDAC_TypeDef * vdac, const VDAC_Init_TypeDef * init)
Initialize VDAC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | A pointer to the VDAC peripheral register block. |
| const VDAC_Init_TypeDef * | [in] | init | A pointer to the VDAC initialization structure. |
Initializes the common parts for both channels. This function will also load calibration values from the Device Information (DI) page into the VDAC calibration register. To complete a VDAC setup, channel control configuration must also be done. See VDAC_InitChannel().
Note
This function will disable both channels prior to configuration.
VDAC_InitChannel#
void VDAC_InitChannel (VDAC_TypeDef * vdac, const VDAC_InitChannel_TypeDef * init, unsigned int ch)
Initialize a VDAC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | A pointer to the VDAC peripheral register block. |
| const VDAC_InitChannel_TypeDef * | [in] | init | A pointer to the VDAC channel initialization structure. |
| unsigned int | [in] | ch | A channel number to initialize. |
VDAC_Channel0OutputSet#
void VDAC_Channel0OutputSet (VDAC_TypeDef * vdac, uint32_t value)
Set the output signal of VDAC channel 0 to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | value | Value to write to channel 0 output register CH0DATA. |
This function sets the output signal of VDAC channel 0 by writing value to the CH0DATA register.
VDAC_Channel1OutputSet#
void VDAC_Channel1OutputSet (VDAC_TypeDef * vdac, uint32_t value)
Set the output signal of VDAC channel 1 to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | value | Value to write to channel 1 output register CH1DATA. |
This function sets the output signal of VDAC channel 1 by writing value to the CH1DATA register.
VDAC_IntClear#
void VDAC_IntClear (VDAC_TypeDef * vdac, uint32_t flags)
Clear one or more pending VDAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | flags | Pending VDAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn). |
VDAC_IntDisable#
void VDAC_IntDisable (VDAC_TypeDef * vdac, uint32_t flags)
Disable one or more VDAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | flags | VDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn). |
VDAC_IntEnable#
void VDAC_IntEnable (VDAC_TypeDef * vdac, uint32_t flags)
Enable one or more VDAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | flags | VDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn). |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using VDAC_IntClear() prior to enabling the interrupt.
VDAC_IntGet#
uint32_t VDAC_IntGet (VDAC_TypeDef * vdac)
Get pending VDAC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
Note
The event bits are not cleared by the use of this function.
Returns
VDAC interrupt sources pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
VDAC_IntGetEnabled#
uint32_t VDAC_IntGetEnabled (VDAC_TypeDef * vdac)
Get enabled and pending VDAC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled VDAC interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in VDACx_IEN_nnn register (VDACx_IEN_nnn) and
the OR combination of valid interrupt flags of the VDAC module (VDACx_IF_nnn).
VDAC_IntSet#
void VDAC_IntSet (VDAC_TypeDef * vdac, uint32_t flags)
Set one or more pending VDAC interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | Pointer to VDAC peripheral register block. |
| uint32_t | [in] | flags | VDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn). |
VDAC_PrescaleCalc#
uint32_t VDAC_PrescaleCalc (uint32_t vdacFreq, bool syncMode, uint32_t hfperFreq)
Calculate the prescaler value used to determine VDAC clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | vdacFreq | VDAC frequency target. The frequency will automatically be adjusted to be below maximum allowed VDAC clock. |
| bool | [in] | syncMode | Set to true if you intend to use VDAC in synchronous mode. |
| uint32_t | [in] | hfperFreq | Frequency in Hz of HFPERCLK/HFPERCCLK oscillator. Set to 0 to use the currently defined HFPERCLK/HFPERCCLK clock setting. This parameter is only used when syncMode is set to true. |
The VDAC clock is given by the input clock divided by the prescaler+1.
VDAC_CLK = IN_CLK / (prescale + 1)
The maximum VDAC clock is 1 MHz. The input clock is HFPERCLK/HFPERCCLK when VDAC synchronous mode is selected, or an internal oscillator of 10 MHz +/- 20% when asynchronous mode is selected.
Note
If the requested VDAC frequency is low and the maximum prescaler value can't adjust the actual VDAC frequency lower than requested, the maximum prescaler value is returned resulting in a higher VDAC frequency than requested.
Returns
A prescaler value to use for VDAC to achieve a clock value less than or equal to
vdacFreq.
VDAC_Reset#
void VDAC_Reset (VDAC_TypeDef * vdac)
Reset VDAC to same state that it was in after a hardwares reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| VDAC_TypeDef * | [in] | vdac | A pointer to the VDAC peripheral register block. |