Deprecated Functions#
Deprecated Functions.
Modules#
Functions#
Function Documentation#
SE_initOTP#
SE_Response_t SE_initOTP (SE_OTPInit_t * otp_init)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SE_OTPInit_t * | [in] | otp_init | SE_OTPInit_t structure containing the SE configuration. |
Initialize SE one-time-programmable (OTP) configuration.
Configuration is performed by setting the desired options in the SE_OTPInit_t structure.
This function can be used to enable secure boot, to configure flash page locking, and to enable anti-rollback protection when using the SE to perform an application upgrade, typically a Gecko bootloader upgrade.
Before secure boot can be enabled, the public key used for secure boot verification must be uploaded using SE_initPubkey().
Warnings
This command can only be executed once per device! When the configuration has been programmed it is not possible to update any of the fields.
Returns
One of the SE_RESPONSE return codes.
Return values
SE_RESPONSE_OK: when the command was executed successfully
SE_initPubkey#
SE_Response_t SE_initPubkey (uint32_t key_type, void * pubkey, uint32_t numBytes, bool signature)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | key_type | ID of key type to initialize. |
| void * | [in] | pubkey | Pointer to a buffer that contains the public key or signature. Must be word aligned and have a length of 64 bytes. |
| uint32_t | [in] | numBytes | Length of pubkey buffer (64 bytes). |
| bool | [in] | signature | If true, initialize signature for the specified key type instead of the public key itself. |
Init pubkey or pubkey signature.
Initialize public key stored in the SE, or its corresponding signature. The command can be used to write:
SE_KEY_TYPE_BOOT – public key used to perform secure boot
SE_KEY_TYPE_AUTH – public key used to perform secure debug
Note
These keys can not be overwritten, so this command can only be issued once per key per part.
Returns
One of the SE_RESPONSE return codes.
Return values
SE_RESPONSE_OK: when the command was executed successfully
SE_RESPONSE_TEST_FAILED: when the pubkey is not set
SE_RESPONSE_INVALID_PARAMETER: when an invalid type is passed