BURTC - Backup RTC#
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
Modules#
Enumerations#
BURTC clock selection.
BURTC mode of operation.
BURTC low power mode.
Functions#
Initialize BURTC.
Enable or Disable BURTC peripheral reset and start counter.
Set BURTC compare channel.
Get the BURTC compare value.
Reset counter.
Restore BURTC to reset state.
Get the clock frequency of the BURTC.
Clear one or more pending BURTC interrupts.
Disable one or more BURTC interrupts.
Enable one or more BURTC interrupts.
Get pending BURTC interrupt flags.
Get enabled and pending BURTC interrupt flags.
Set one or more pending BURTC interrupts from SW.
Status of BURTC RAM, timestamp and LP Mode.
Clear and reset BURTC status register.
Wait for the BURTC to complete all synchronization of register changes and commands.
Get BURTC counter.
Get BURTC timestamp for entering BU.
Freeze register updates until enabled.
Shut down power to retention register bank.
Set a value in one of the retention registers.
Read a value from one of the retention registers.
Lock BURTC registers, which will protect from writing new config settings.
Unlock BURTC registers, which will enable write access to change configuration.
Macros#
BURTC clock divisors.
Divide clock by 2.
Divide clock by 4.
Divide clock by 8.
Divide clock by 16.
Divide clock by 32.
Divide clock by 64.
Divide clock by 128.
Default configuration for BURTC initialization structure.
Enumeration Documentation#
BURTC_ClkSel_TypeDef#
BURTC_ClkSel_TypeDef
BURTC clock selection.
Enumerator | |
---|---|
burtcClkSelULFRCO | Ultra low frequency (1 kHz) clock. |
burtcClkSelLFRCO | Low frequency RC oscillator. |
burtcClkSelLFXO | Low frequency crystal oscillator. |
BURTC_Mode_TypeDef#
BURTC_Mode_TypeDef
BURTC mode of operation.
Enumerator | |
---|---|
burtcModeDisable | Disable BURTC. |
burtcModeEM2 | Enable and start BURTC counter in EM0 to EM2. |
burtcModeEM3 | Enable and start BURTC counter in EM0 to EM3. |
burtcModeEM4 | Enable and start BURTC counter in EM0 to EM4. |
BURTC_LP_TypeDef#
BURTC_LP_TypeDef
BURTC low power mode.
Enumerator | |
---|---|
burtcLPDisable | Low Power Mode is disabled. |
burtcLPEnable | Low Power Mode is always enabled. |
burtcLPBU | Low Power Mode when system enters backup mode. |
Function Documentation#
BURTC_Init#
void BURTC_Init (const BURTC_Init_TypeDef * burtcInit)
Initialize BURTC.
Type | Direction | Argument Name | Description |
---|---|---|---|
const BURTC_Init_TypeDef * | [in] | burtcInit | A pointer to the BURTC initialization structure. |
Configures the BURTC peripheral.
Note
Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
* RMU_ResetControl(rmuResetBU, rmuResetModeClear); *
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
BURTC_Enable#
void BURTC_Enable (bool enable)
Enable or Disable BURTC peripheral reset and start counter.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | enable | If true; asserts reset to BURTC, halts counter, if false; deassert reset |
BURTC_CompareSet#
void BURTC_CompareSet (unsigned int comp, uint32_t value)
Set BURTC compare channel.
Type | Direction | Argument Name | Description |
---|---|---|---|
unsigned int | [in] | comp | Compare the channel index, must be 0 for current devices. |
uint32_t | [in] | value | New compare value. |
BURTC_CompareGet#
uint32_t BURTC_CompareGet (unsigned int comp)
Get the BURTC compare value.
Type | Direction | Argument Name | Description |
---|---|---|---|
unsigned int | [in] | comp | Compare the channel index value, must be 0 for Giant/Leopard Gecko. |
Returns
The currently configured value for this compare channel.
BURTC_CounterReset#
void BURTC_CounterReset (void )
Reset counter.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
BURTC_Reset#
void BURTC_Reset (void )
Restore BURTC to reset state.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Note
Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
BURTC_ClockFreqGet#
uint32_t BURTC_ClockFreqGet (void )
Get the clock frequency of the BURTC.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
The current frequency in Hz.
BURTC_IntClear#
void BURTC_IntClear (uint32_t flags)
Clear one or more pending BURTC interrupts.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | flags | BURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). |
BURTC_IntDisable#
void BURTC_IntDisable (uint32_t flags)
Disable one or more BURTC interrupts.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | flags | BURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). |
BURTC_IntEnable#
void BURTC_IntEnable (uint32_t flags)
Enable one or more BURTC interrupts.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | flags | BURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). |
Note
Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
BURTC_IntGet#
uint32_t BURTC_IntGet (void )
Get pending BURTC interrupt flags.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Note
This function does not clear the event bits.
Returns
Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
BURTC_IntGetEnabled#
uint32_t BURTC_IntGetEnabled (void )
Get enabled and pending BURTC interrupt flags.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Note
The event bits are not cleared by the use of this function.
Returns
Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
BURTC_IntSet#
void BURTC_IntSet (uint32_t flags)
Set one or more pending BURTC interrupts from SW.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | flags | BURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). |
BURTC_Status#
uint32_t BURTC_Status (void )
Status of BURTC RAM, timestamp and LP Mode.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
A mask logically OR-ed status bits
BURTC_StatusClear#
void BURTC_StatusClear (void )
Clear and reset BURTC status register.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
BURTC_SyncWait#
void BURTC_SyncWait (void )
Wait for the BURTC to complete all synchronization of register changes and commands.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
BURTC_CounterGet#
uint32_t BURTC_CounterGet (void )
Get BURTC counter.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
BURTC counter value
BURTC_TimestampGet#
uint32_t BURTC_TimestampGet (void )
Get BURTC timestamp for entering BU.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
BURTC Time Stamp value
BURTC_FreezeEnable#
void BURTC_FreezeEnable (bool enable)
Freeze register updates until enabled.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | enable | If true, registers are not updated until enabled again. |
BURTC_Powerdown#
void BURTC_Powerdown (bool enable)
Shut down power to retention register bank.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | enable | If true, shuts off power to retention registers. |
Note
When power retention is disabled, it can't be enabled again (until reset).
BURTC_RetRegSet#
void BURTC_RetRegSet (uint32_t num, uint32_t data)
Set a value in one of the retention registers.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | num | Register to set |
uint32_t | [in] | data | Value to put into register |
BURTC_RetRegGet#
uint32_t BURTC_RetRegGet (uint32_t num)
Read a value from one of the retention registers.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | num | Retention Register to read |
Returns
Value of the retention register
BURTC_Lock#
void BURTC_Lock (void )
Lock BURTC registers, which will protect from writing new config settings.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
BURTC_Unlock#
void BURTC_Unlock (void )
Unlock BURTC registers, which will enable write access to change configuration.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |