RFF PLL initialization structure.

When using this structure you need to modify the X, Y and N factor and the desired host target frequency to match the components placed on the board (namely the RFFPLL reference clock). X, Y, N values for a 39MHz HFXO:

  • Formula for host clock output: frequency = (freq HFXO * dividerN / 2) / dividerY

  • Formula for radio clock output: freq = (freq HFXO * dividerN / 2) / (dividerX / 2)

Public Attributes#

uint32_t

Host target frequency.

bool

Disable on-demand requests.

bool

Force oscillator enable.

bool

Enable register lock.

uint8_t

Divider Y for digital.

uint8_t

Divider X for Radio.

uint8_t

Feedback divider N.

Public Attribute Documentation#

frequency#

uint32_t CMU_RFFPLL_Init_TypeDef::frequency

Host target frequency.


Definition at line 1308 of file platform/emlib/inc/em_cmu.h

disOnDemand#

bool CMU_RFFPLL_Init_TypeDef::disOnDemand

Disable on-demand requests.


Definition at line 1309 of file platform/emlib/inc/em_cmu.h

forceEn#

bool CMU_RFFPLL_Init_TypeDef::forceEn

Force oscillator enable.


Definition at line 1310 of file platform/emlib/inc/em_cmu.h

regLock#

bool CMU_RFFPLL_Init_TypeDef::regLock

Enable register lock.


Definition at line 1311 of file platform/emlib/inc/em_cmu.h

dividerY#

uint8_t CMU_RFFPLL_Init_TypeDef::dividerY

Divider Y for digital.


Definition at line 1312 of file platform/emlib/inc/em_cmu.h

dividerX#

uint8_t CMU_RFFPLL_Init_TypeDef::dividerX

Divider X for Radio.


Definition at line 1313 of file platform/emlib/inc/em_cmu.h

dividerN#

uint8_t CMU_RFFPLL_Init_TypeDef::dividerN

Feedback divider N.


Definition at line 1314 of file platform/emlib/inc/em_cmu.h