Deprecated Functions#
Deprecated Functions.
Functions#
SE_readPubkey(uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature)
Function Documentation#
SE_readPubkey#
SE_Response_t SE_readPubkey (uint32_t key_type, void * pubkey, uint32_t numBytes, bool signature)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | key_type | ID of key type to read. |
| void * | [out] | pubkey | Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. |
| uint32_t | [in] | numBytes | Length of pubkey buffer (64 bytes). |
| bool | [in] | signature | If true, the function will return the signature programmed for the specified public key instead of the public key itself. |
Read pubkey or pubkey signature.
Read out a public key stored in the SE, or its signature. The command can be used to read:
SE_KEY_TYPE_BOOT
SE_KEY_TYPE_AUTH
Returns
One of the SE_RESPONSE return codes.
Return values
SE_RESPONSE_OK: when the command was executed successfully
SE_RESPONSE_TEST_FAILED: when the pubkey is not set
SE_RESPONSE_INVALID_PARAMETER: when an invalid type is passed