Button#

Sample API functions for using push-buttons.

See button.h for source code.

Button State Definitions#

A set of numerical definitions for use with the button APIs indicating the state of a button.

#define
BUTTON_PRESSED 1

Button state is pressed.

#define
BUTTON_RELEASED 0

Button state is released.

Functions#

void

Initializes the buttons.

uint8_t
halButtonState(uint8_t button)

Returns the current state (pressed or released) of a button.

uint8_t
halButtonPinState(uint8_t button)

Returns the current state (pressed or released) of the pin associated with a button.

void
halButtonIsr(uint8_t button, uint8_t state)

A callback called in interrupt context whenever a button changes its state.

Button State Definitions Documentation#

Function Documentation#

halInternalInitButton#

void halInternalInitButton (void )

Initializes the buttons.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is automatically called by halInit().


halButtonState#

uint8_t halButtonState (uint8_t button)

Returns the current state (pressed or released) of a button.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Abutton

The button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER.

Note

  • This function is correlated with halButtonIsr() and so returns the shadow state rather than reading the actual state of the pin.

Returns


halButtonPinState#

uint8_t halButtonPinState (uint8_t button)

Returns the current state (pressed or released) of the pin associated with a button.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Abutton

The button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER.

This reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.

Returns


halButtonIsr#

void halButtonIsr (uint8_t button, uint8_t state)

A callback called in interrupt context whenever a button changes its state.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Abutton

The button which has changed state, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER.

uint8_tN/Astate

The new state of the button referenced by the button parameter, either BUTTON_PRESSED if the button has been pressed or BUTTON_RELEASED if the button has been released.

Must be implemented by the application. This function should contain the functionality to be executed in response to changes of state in each of the buttons, or callbacks to the appropriate functionality.