A Simple RGB LED PWM instance.
Public Attributes#
Inherit from the Common LED Driver.
void(*
Member function to set RGB.
void(*
Member function to get RGB.
Public Attribute Documentation#
led_common#
sl_led_t sl_led_rgb_pwm_t::led_common
Inherit from the Common LED Driver.
Definition at line
86
of file platform/driver/leddrv/inc/sl_simple_rgb_pwm_led.h
set_rgb_color#
void(* sl_led_rgb_pwm_t::set_rgb_color) (void *context, uint16_t red, uint16_t green, uint16_t blue)
Member function to set RGB.
Definition at line
87
of file platform/driver/leddrv/inc/sl_simple_rgb_pwm_led.h
get_rgb_color#
void(* sl_led_rgb_pwm_t::get_rgb_color) (void *context, uint16_t *red, uint16_t *green, uint16_t *blue)
Member function to get RGB.
Definition at line
91
of file platform/driver/leddrv/inc/sl_simple_rgb_pwm_led.h