KEYSCAN - Keyboard Scan#
Keyscan (KEYSCAN) Peripheral API.
This module contains functions to control the KEYSCAN peripheral of Silicon Labs 32-bit MCUs and SoCs. The KEYSCAN module connects through rows and columns of GPIOs to an external mechanical keypad.
Modules#
Enumerations#
KEYSCAN configuration delay values.
Functions#
Initializes KEYSCAN module.
Enables KEYSCAN module.
Disables KEYSCAN module.
Waits for the KEYSCAN to complete reseting or disabling procedure.
Waits for the KEYSCAN to complete all synchronization of register changes and commands.
Starts KEYSCAN scan.
Stops the KEYSCAN scan.
Restores KEYSCAN to its reset state.
Gets KEYSCAN STATUS register value.
Enables one or more KEYSCAN interrupts.
Disables one or more KEYSCAN interrupts.
Clears one or more pending KEYSCAN interrupts.
Gets pending KEYSCAN interrupt flags.
Gets enabled and pending KEYSCAN interrupt flags.
Sets one or more pending KEYSCAN interrupts from Software.
Macros#
Suggested default values for KEYSCAN configuration structure.
Enumeration Documentation#
sl_hal_keyscan_delay_t#
sl_hal_keyscan_delay_t
KEYSCAN configuration delay values.
| Enumerator | |
|---|---|
| SL_HAL_KEYSCAN_DELAY_2MS | 2 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_4MS | 4 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_6MS | 6 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_8MS | 8 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_10MS | 10 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_12MS | 12 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_14MS | 14 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_16MS | 16 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_18MS | 18 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_20MS | 20 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_22MS | 22 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_24MS | 24 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_26MS | 26 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_28MS | 28 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_30MS | 30 ms delay. | 
| SL_HAL_KEYSCAN_DELAY_32MS | 32 ms delay. | 
Function Documentation#
sl_hal_keyscan_init#
void sl_hal_keyscan_init (const sl_hal_keyscan_config_t * p_config)
Initializes KEYSCAN module.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const sl_hal_keyscan_config_t * | [in] | p_config | A pointer to the KEYSCAN initialization structure variable. | 
sl_hal_keyscan_enable#
void sl_hal_keyscan_enable (void )
Enables KEYSCAN module.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
sl_hal_keyscan_disable#
void sl_hal_keyscan_disable (void )
Disables KEYSCAN module.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Note
- The disabling of the module could take some time. This function will not wait for the disabling to finish before returning. Use the function sl_hal_keyscan_wait_ready to wait for the module to be fully disable. 
sl_hal_keyscan_wait_ready#
void sl_hal_keyscan_wait_ready (void )
Waits for the KEYSCAN to complete reseting or disabling procedure.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
sl_hal_keyscan_wait_sync#
void sl_hal_keyscan_wait_sync (void )
Waits for the KEYSCAN to complete all synchronization of register changes and commands.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
sl_hal_keyscan_start_scan#
void sl_hal_keyscan_start_scan (void )
Starts KEYSCAN scan.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Note
- This function will send a start command to the KEYSCAN peripheral. The sl_hal_keyscan_wait_sync function can be used to wait for the start command to be executed. 
- This function requires the KEYSCAN to be enabled. 
sl_hal_keyscan_stop_scan#
void sl_hal_keyscan_stop_scan (void )
Stops the KEYSCAN scan.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Note
- This function will send a stop command to the KEYSCAN peripheral. The sl_hal_keyscan_wait_sync function can be used to wait for the stop command to be executed. 
- This function requires the KEYSCAN to be enabled. 
sl_hal_keyscan_reset#
void sl_hal_keyscan_reset (void )
Restores KEYSCAN to its reset state.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Note
- The resetting of the module could take some time. This function will not wait for the resetting to finish before returning. Use the function sl_hal_keyscan_wait_ready to wait for the module to be fully reset. 
- The register STATUS get reset value after enabling the module because it is of type RSYNC 
sl_hal_keyscan_get_status#
uint32_t sl_hal_keyscan_get_status (void )
Gets KEYSCAN STATUS register value.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
- Current STATUS register value. 
sl_hal_keyscan_enable_interrupts#
void sl_hal_keyscan_enable_interrupts (uint32_t flags)
Enables one or more KEYSCAN interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | flags | KEYSCAN interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources. | 
Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_keyscan_clear_interrupts prior to enabling the interrupt. 
sl_hal_keyscan_disable_interrupts#
void sl_hal_keyscan_disable_interrupts (uint32_t flags)
Disables one or more KEYSCAN interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | flags | KEYSCAN interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources. | 
sl_hal_keyscan_clear_interrupts#
void sl_hal_keyscan_clear_interrupts (uint32_t flags)
Clears one or more pending KEYSCAN interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | flags | KEYSCAN interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources. | 
sl_hal_keyscan_get_interrupts#
uint32_t sl_hal_keyscan_get_interrupts (void )
Gets pending KEYSCAN interrupt flags.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Note
- Event bits are not cleared by using this function. 
Returns
- Pending KEYSCAN interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources. 
sl_hal_keyscan_get_enabled_interrupts#
uint32_t sl_hal_keyscan_get_enabled_interrupts (void )
Gets enabled and pending KEYSCAN interrupt flags.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Useful for handling more interrupt sources in the same interrupt handler.
Note
- Interrupt flags are not cleared by using this function. 
Returns
- Pending and enabled KEYSCAN interrupt sources. The return value is the bitwise AND of - the enabled interrupt sources in KEYSCAN_IEN and 
- the pending interrupt flags KEYSCAN_IF. 
 
sl_hal_keyscan_set_interrupts#
void sl_hal_keyscan_set_interrupts (uint32_t flags)
Sets one or more pending KEYSCAN interrupts from Software.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | flags | KEYSCAN interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources. |