SE - Secure Element#
Secure Element peripheral API.
Abstraction of the Secure Element's mailbox interface.
For series 2 devices with a part number that is xG23 or higher, the following step is necessary for basic operation:
Clock enable:
CMU_ClockEnable(cmuClock_SEMAILBOX, true);
Note
The high-level SE API has been moved to the SE manager, and the implementation in em_se should not be used.
Using the SE's mailbox is not thread-safe in EMLIB, and accessing the SE's mailbox both in regular and IRQ context is not safe. SE operations should be performed using the SE manager if possible.
Modules#
Typedefs#
SE DMA transfer descriptor.
SE Command structure.
Possible responses to a command.
Functions#
Write to FIFO.
Add input data to a command.
Add output data to a command.
Add a parameter to a command.
Execute the passed command.
Check whether the running command has completed.
Read the status of the previously executed command.
Wait for completion of the current command.
Disable one or more SE interrupts.
Enable one or more SE interrupts.
Macros#
Response status codes for the Secure Element.
Command executed successfully or signature was successfully validated.
Maximum amount of parameters supported by the hardware FIFO.
Stop datatransfer.
Discard datatransfer.
Realign datatransfer.
Datatransfer Const Address.
Stop Length Mask.
Maximum amount of parameters for largest command in defined command set.
Default initialization of data transfer struct.
Default initialization of command struct.
Typedef Documentation#
SE_DataTransfer_t#
typedef sli_se_datatransfer_t SE_DataTransfer_t
SE DMA transfer descriptor.
Can be linked to each other to provide scatter-gather behavior.
133
of file platform/emlib/inc/em_se.h
SE_Command_t#
typedef sli_se_mailbox_command_t SE_Command_t
SE Command structure.
See
146
of file platform/emlib/inc/em_se.h
SE_Response_t#
typedef sli_se_mailbox_response_t SE_Response_t
Possible responses to a command.
159
of file platform/emlib/inc/em_se.h
Function Documentation#
writeToFifo#
void writeToFifo (uint32_t value)
Write to FIFO.
N/A | value | Value to write to FIFO |
147
of file platform/emlib/src/em_se.c
SE_addDataInput#
void SE_addDataInput (SE_Command_t * command, SE_DataTransfer_t * data)
Add input data to a command.
[in] | command | Pointer to an SE command structure. |
[in] | data | Pointer to a data transfer structure. |
This function adds a buffer of input data to the given SE command structure The buffer gets appended by reference at the end of the list of already added buffers.
Note
Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
184
of file platform/emlib/src/em_se.c
SE_addDataOutput#
void SE_addDataOutput (SE_Command_t * command, SE_DataTransfer_t * data)
Add output data to a command.
[in] | command | Pointer to an SE command structure. |
[in] | data | Pointer to a data transfer structure. |
This function adds a buffer of output data to the given command structure The buffer gets appended by reference at the end of the list of already added buffers.
Note
Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
217
of file platform/emlib/src/em_se.c
SE_addParameter#
void SE_addParameter (SE_Command_t * command, uint32_t parameter)
Add a parameter to a command.
[in] | command | Pointer to a filled-out SE command structure. |
[in] | parameter | Parameter to add. |
This function adds a parameter word to the passed command.
Note
Make sure to not exceed SE_MAX_PARAMETERS.
246
of file platform/emlib/src/em_se.c
SE_executeCommand#
void SE_executeCommand (SE_Command_t * command)
Execute the passed command.
[in] | command | Pointer to a filled-out SE command structure. |
This function starts the execution of the passed command by the secure element. When started, wait for the RXINT interrupt flag, or call SE_waitCommandCompletion to busy-wait. After completion, you have to call SE_readCommandResponse to get the command's execution status.
271
of file platform/emlib/src/em_se.c
SE_isCommandCompleted#
bool SE_isCommandCompleted (void )
Check whether the running command has completed.
N/A |
This function polls the SE-to-host mailbox interrupt flag.
Returns
True if a command has completed and the result is available
210
of file platform/emlib/inc/em_se.h
SE_readCommandResponse#
SE_Response_t SE_readCommandResponse (void )
Read the status of the previously executed command.
N/A |
This function reads the status of the previously executed command.
Note
The command response needs to be read for every executed command, and can only be read once per executed command (FIFO behavior).
Returns
One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully or a signature was successfully verified.
233
of file platform/emlib/inc/em_se.h
SE_waitCommandCompletion#
void SE_waitCommandCompletion (void )
Wait for completion of the current command.
N/A |
This function "busy"-waits until the execution of the ongoing instruction has completed.
249
of file platform/emlib/inc/em_se.h
SE_disableInterrupt#
void SE_disableInterrupt (uint32_t flags)
Disable one or more SE interrupts.
[in] | flags | SE interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SE_CONFIGURATION_(TX/RX)INTEN). |
265
of file platform/emlib/inc/em_se.h
SE_enableInterrupt#
void SE_enableInterrupt (uint32_t flags)
Enable one or more SE interrupts.
[in] | flags | SE interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SEMAILBOX_CONFIGURATION_TXINTEN or SEMAILBOX_CONFIGURATION_RXINTEN). |
283
of file platform/emlib/inc/em_se.h
Macro Definition Documentation#
SE_RESPONSE_MASK#
#define SE_RESPONSE_MASKValue:
0x000F0000UL
Response status codes for the Secure Element.
97
of file platform/emlib/inc/em_se.h
SE_RESPONSE_OK#
#define SE_RESPONSE_OKValue:
0x00000000UL
Command executed successfully or signature was successfully validated.
99
of file platform/emlib/inc/em_se.h
SE_FIFO_MAX_PARAMETERS#
#define SE_FIFO_MAX_PARAMETERSValue:
13U
Maximum amount of parameters supported by the hardware FIFO.
102
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_STOP#
#define SE_DATATRANSFER_STOPValue:
0x00000001UL
Stop datatransfer.
105
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_DISCARD#
#define SE_DATATRANSFER_DISCARDValue:
0x40000000UL
Discard datatransfer.
107
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_REALIGN#
#define SE_DATATRANSFER_REALIGNValue:
0x20000000UL
Realign datatransfer.
109
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_CONSTADDRESS#
#define SE_DATATRANSFER_CONSTADDRESSValue:
0x10000000UL
Datatransfer Const Address.
111
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_LENGTH_MASK#
#define SE_DATATRANSFER_LENGTH_MASKValue:
0x0FFFFFFFUL
Stop Length Mask.
113
of file platform/emlib/inc/em_se.h
SE_MAX_PARAMETERS#
#define SE_MAX_PARAMETERSValue:
4U
Maximum amount of parameters for largest command in defined command set.
117
of file platform/emlib/inc/em_se.h
SE_DATATRANSFER_DEFAULT#
#define SE_DATATRANSFER_DEFAULTValue:
Default initialization of data transfer struct.
136
of file platform/emlib/inc/em_se.h
SE_COMMAND_DEFAULT#
#define SE_COMMAND_DEFAULTValue:
Default initialization of command struct.
149
of file platform/emlib/inc/em_se.h