You are viewing documentation for version:
Struct representing an I/O Stream EUSART context. 
Public Attribute Documentation#
context#
sl_iostream_uart_context_t sl_iostream_eusart_context_t::context
context 
eusart#
sl_peripheral_t sl_iostream_eusart_context_t::eusart
eusart 
bus_clock#
sl_bus_clock_t sl_iostream_eusart_context_t::bus_clock
Peripheral Clock. 
tx_port#
uint8_t sl_iostream_eusart_context_t::tx_port
Transmit port. 
tx_pin#
uint8_t sl_iostream_eusart_context_t::tx_pin
Transmit pin. 
rx_port#
uint8_t sl_iostream_eusart_context_t::rx_port
Receive port. 
rx_pin#
uint8_t sl_iostream_eusart_context_t::rx_pin
Receive pin. 
cts_port#
uint8_t sl_iostream_eusart_context_t::cts_port
Flow control, CTS port. 
cts_pin#
uint8_t sl_iostream_eusart_context_t::cts_pin
Flow control, CTS pin. 
rts_port#
uint8_t sl_iostream_eusart_context_t::rts_port
Flow control, RTS port. 
rts_pin#
uint8_t sl_iostream_eusart_context_t::rts_pin
Flow control, RTS pin. 
flags#
uint8_t sl_iostream_eusart_context_t::flags
Configuration flags. 
node#
sl_slist_node_t sl_iostream_eusart_context_t::node