ACMP - Analog Comparator#

Analog Comparator peripheral API.


Introduction#

This module contains functions to control the Analog Comparator (ACMP) peripheral of Silicon Labs' 32-bit MCUs and SoCs.

The Analog Comparator compares the voltage of two analog inputs and outputs a digital signal indicating which input voltage is higher. Inputs can either be from internal references or from external pins. Response time, and thereby the current consumption, can be configured by altering the current supply to the comparator.


Example#

This example shows how to use the em_acmp.h API for comparing an input pin to an internal 2.5 V reference voltage.

ACMP Base example:

{
  #define GPIO_ACMPOUT    PD1  // Pin location for ACMP OUT varies depending on the device.

  // Enable bus clocks.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_ACMP0);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);

  // Initialize with default settings.
  sl_hal_acmp_init_t init = SL_HAL_ACMP_INIT_DEFAULT;

  sl_hal_acmp_init(ACMP0, &init);
  sl_hal_acmp_enable(ACMP0);

  // Now we select the two inputs to compare. Here we compare the SL_HAL_ACMP_INPUT_PD2
  // input to the internal 2.5V reference. When SL_HAL_ACMP_INPUT_PD2 is lower than
  // 2.5 V then the ACMP output is 0 and when SL_HAL_ACMP_INPUT_PD2 is higher than
  // 2.5 V then the ACMP output is 1.
  sl_hal_acmp_set_input(ACMP0, SL_HAL_ACMP_INPUT_VREFDIV2V5, SL_HAL_ACMP_INPUT_PD2);

  // Allocate CDEVEN0 to ACMP0 to be able to use the input.
  GPIO->CDBUSALLOC = GPIO_CDBUSALLOC_CDEVEN0_ACMP0;

  // To be able to probe the output we can send the ACMP output to a pin.
  sl_hal_acmp_setup_gpio_inversion(ACMP0, false);
  GPIO->ACMPROUTE[ACMP_NUM(ACMP0)].ACMPOUTROUTE = (GPIO_ACMPOUT->port << _GPIO_ACMP_ACMPOUTROUTE_PORT_SHIFT)
                                                | (GPIO_ACMPOUT->pin << _GPIO_ACMP_ACMPOUTROUTE_PIN_SHIFT);
  GPIO->ACMPROUTE[ACMP_NUM(ACMP0)].ROUTEEN = GPIO_ACMP_ROUTEEN_ACMPOUTPEN;
}

Modules#

sl_hal_acmp_init_t

Enumerations#

enum
SL_HAL_ACMP_HYSTERESIS_DISABLED = _ACMP_CFG_HYST_DISABLED
SL_HAL_ACMP_HYSTERESIS_SYM_10MV = _ACMP_CFG_HYST_SYM10MV
SL_HAL_ACMP_HYSTERESIS_SYM_20MV = _ACMP_CFG_HYST_SYM20MV
SL_HAL_ACMP_HYSTERESIS_SYM_30MV = _ACMP_CFG_HYST_SYM30MV
SL_HAL_ACMP_HYSTERESIS_POS_10MV = _ACMP_CFG_HYST_POS10MV
SL_HAL_ACMP_HYSTERESIS_POS_20MV = _ACMP_CFG_HYST_POS20MV
SL_HAL_ACMP_HYSTERESIS_POS_30MV = _ACMP_CFG_HYST_POS30MV
SL_HAL_ACMP_HYSTERESIS_NEG_10MV = _ACMP_CFG_HYST_NEG10MV
SL_HAL_ACMP_HYSTERESIS_NEG_20MV = _ACMP_CFG_HYST_NEG20MV
SL_HAL_ACMP_HYSTERESIS_NEG_30MV = _ACMP_CFG_HYST_NEG30MV
}

Hysteresis level.

enum
SL_HAL_ACMP_INPUT_RANGE_FULL = _ACMP_CFG_INPUTRANGE_FULL
SL_HAL_ACMP_INPUT_RANGE_REDUCED = _ACMP_CFG_INPUTRANGE_REDUCED
}

vcm/input range.

enum
SL_HAL_ACMP_ACCURACY_LOW = _ACMP_CFG_ACCURACY_LOW
SL_HAL_ACMP_ACCURACY_HIGH = _ACMP_CFG_ACCURACY_HIGH
}

Accuracy mode.

enum
SL_HAL_ACMP_INPUT_VSS = _ACMP_INPUTCTRL_POSSEL_VSS
SL_HAL_ACMP_INPUT_VREFDIVAVDD = _ACMP_INPUTCTRL_POSSEL_VREFDIVAVDD
SL_HAL_ACMP_INPUT_VREFDIVAVDDLP = _ACMP_INPUTCTRL_POSSEL_VREFDIVAVDDLP
SL_HAL_ACMP_INPUT_VREFDIV1V25 = _ACMP_INPUTCTRL_POSSEL_VREFDIV1V25
SL_HAL_ACMP_INPUT_VREFDIV1V25LP = _ACMP_INPUTCTRL_POSSEL_VREFDIV1V25LP
SL_HAL_ACMP_INPUT_VREFDIV2V5 = _ACMP_INPUTCTRL_POSSEL_VREFDIV2V5
SL_HAL_ACMP_INPUT_VREFDIV2V5LP = _ACMP_INPUTCTRL_POSSEL_VREFDIV2V5LP
SL_HAL_ACMP_INPUT_VSENSE01DIV4 = _ACMP_INPUTCTRL_POSSEL_VSENSE01DIV4
SL_HAL_ACMP_INPUT_VSENSE01DIV4LP = _ACMP_INPUTCTRL_POSSEL_VSENSE01DIV4LP
SL_HAL_ACMP_INPUT_VSENSE11DIV4 = _ACMP_INPUTCTRL_POSSEL_VSENSE11DIV4
SL_HAL_ACMP_INPUT_VSENSE11DIV4LP = _ACMP_INPUTCTRL_POSSEL_VSENSE11DIV4LP
SL_HAL_ACMP_INPUT_EXTPA = _ACMP_INPUTCTRL_POSSEL_EXTPA
SL_HAL_ACMP_INPUT_EXTPB = _ACMP_INPUTCTRL_POSSEL_EXTPB
SL_HAL_ACMP_INPUT_EXTPC = _ACMP_INPUTCTRL_POSSEL_EXTPC
SL_HAL_ACMP_INPUT_EXTPD = _ACMP_INPUTCTRL_POSSEL_EXTPD
SL_HAL_ACMP_INPUT_PA0 = _ACMP_INPUTCTRL_POSSEL_PA0
SL_HAL_ACMP_INPUT_PA1 = _ACMP_INPUTCTRL_POSSEL_PA1
SL_HAL_ACMP_INPUT_PA2 = _ACMP_INPUTCTRL_POSSEL_PA2
SL_HAL_ACMP_INPUT_PA3 = _ACMP_INPUTCTRL_POSSEL_PA3
SL_HAL_ACMP_INPUT_PA4 = _ACMP_INPUTCTRL_POSSEL_PA4
SL_HAL_ACMP_INPUT_PA5 = _ACMP_INPUTCTRL_POSSEL_PA5
SL_HAL_ACMP_INPUT_PA6 = _ACMP_INPUTCTRL_POSSEL_PA6
SL_HAL_ACMP_INPUT_PA7 = _ACMP_INPUTCTRL_POSSEL_PA7
SL_HAL_ACMP_INPUT_PA8 = _ACMP_INPUTCTRL_POSSEL_PA8
SL_HAL_ACMP_INPUT_PA9 = _ACMP_INPUTCTRL_POSSEL_PA9
SL_HAL_ACMP_INPUT_PA10 = _ACMP_INPUTCTRL_POSSEL_PA10
SL_HAL_ACMP_INPUT_PA11 = _ACMP_INPUTCTRL_POSSEL_PA11
SL_HAL_ACMP_INPUT_PA12 = _ACMP_INPUTCTRL_POSSEL_PA12
SL_HAL_ACMP_INPUT_PA13 = _ACMP_INPUTCTRL_POSSEL_PA13
SL_HAL_ACMP_INPUT_PA14 = _ACMP_INPUTCTRL_POSSEL_PA14
SL_HAL_ACMP_INPUT_PA15 = _ACMP_INPUTCTRL_POSSEL_PA15
SL_HAL_ACMP_INPUT_PB0 = _ACMP_INPUTCTRL_POSSEL_PB0
SL_HAL_ACMP_INPUT_PB1 = _ACMP_INPUTCTRL_POSSEL_PB1
SL_HAL_ACMP_INPUT_PB2 = _ACMP_INPUTCTRL_POSSEL_PB2
SL_HAL_ACMP_INPUT_PB3 = _ACMP_INPUTCTRL_POSSEL_PB3
SL_HAL_ACMP_INPUT_PB4 = _ACMP_INPUTCTRL_POSSEL_PB4
SL_HAL_ACMP_INPUT_PB5 = _ACMP_INPUTCTRL_POSSEL_PB5
SL_HAL_ACMP_INPUT_PB6 = _ACMP_INPUTCTRL_POSSEL_PB6
SL_HAL_ACMP_INPUT_PB7 = _ACMP_INPUTCTRL_POSSEL_PB7
SL_HAL_ACMP_INPUT_PB8 = _ACMP_INPUTCTRL_POSSEL_PB8
SL_HAL_ACMP_INPUT_PB9 = _ACMP_INPUTCTRL_POSSEL_PB9
SL_HAL_ACMP_INPUT_PB10 = _ACMP_INPUTCTRL_POSSEL_PB10
SL_HAL_ACMP_INPUT_PB11 = _ACMP_INPUTCTRL_POSSEL_PB11
SL_HAL_ACMP_INPUT_PB12 = _ACMP_INPUTCTRL_POSSEL_PB12
SL_HAL_ACMP_INPUT_PB13 = _ACMP_INPUTCTRL_POSSEL_PB13
SL_HAL_ACMP_INPUT_PB14 = _ACMP_INPUTCTRL_POSSEL_PB14
SL_HAL_ACMP_INPUT_PB15 = _ACMP_INPUTCTRL_POSSEL_PB15
SL_HAL_ACMP_INPUT_PC0 = _ACMP_INPUTCTRL_POSSEL_PC0
SL_HAL_ACMP_INPUT_PC1 = _ACMP_INPUTCTRL_POSSEL_PC1
SL_HAL_ACMP_INPUT_PC2 = _ACMP_INPUTCTRL_POSSEL_PC2
SL_HAL_ACMP_INPUT_PC3 = _ACMP_INPUTCTRL_POSSEL_PC3
SL_HAL_ACMP_INPUT_PC4 = _ACMP_INPUTCTRL_POSSEL_PC4
SL_HAL_ACMP_INPUT_PC5 = _ACMP_INPUTCTRL_POSSEL_PC5
SL_HAL_ACMP_INPUT_PC6 = _ACMP_INPUTCTRL_POSSEL_PC6
SL_HAL_ACMP_INPUT_PC7 = _ACMP_INPUTCTRL_POSSEL_PC7
SL_HAL_ACMP_INPUT_PC8 = _ACMP_INPUTCTRL_POSSEL_PC8
SL_HAL_ACMP_INPUT_PC9 = _ACMP_INPUTCTRL_POSSEL_PC9
SL_HAL_ACMP_INPUT_PC10 = _ACMP_INPUTCTRL_POSSEL_PC10
SL_HAL_ACMP_INPUT_PC11 = _ACMP_INPUTCTRL_POSSEL_PC11
SL_HAL_ACMP_INPUT_PC12 = _ACMP_INPUTCTRL_POSSEL_PC12
SL_HAL_ACMP_INPUT_PC13 = _ACMP_INPUTCTRL_POSSEL_PC13
SL_HAL_ACMP_INPUT_PC14 = _ACMP_INPUTCTRL_POSSEL_PC14
SL_HAL_ACMP_INPUT_PC15 = _ACMP_INPUTCTRL_POSSEL_PC15
SL_HAL_ACMP_INPUT_PD0 = _ACMP_INPUTCTRL_POSSEL_PD0
SL_HAL_ACMP_INPUT_PD1 = _ACMP_INPUTCTRL_POSSEL_PD1
SL_HAL_ACMP_INPUT_PD2 = _ACMP_INPUTCTRL_POSSEL_PD2
SL_HAL_ACMP_INPUT_PD3 = _ACMP_INPUTCTRL_POSSEL_PD3
SL_HAL_ACMP_INPUT_PD4 = _ACMP_INPUTCTRL_POSSEL_PD4
SL_HAL_ACMP_INPUT_PD5 = _ACMP_INPUTCTRL_POSSEL_PD5
SL_HAL_ACMP_INPUT_PD6 = _ACMP_INPUTCTRL_POSSEL_PD6
SL_HAL_ACMP_INPUT_PD7 = _ACMP_INPUTCTRL_POSSEL_PD7
SL_HAL_ACMP_INPUT_PD8 = _ACMP_INPUTCTRL_POSSEL_PD8
SL_HAL_ACMP_INPUT_PD9 = _ACMP_INPUTCTRL_POSSEL_PD9
SL_HAL_ACMP_INPUT_PD10 = _ACMP_INPUTCTRL_POSSEL_PD10
SL_HAL_ACMP_INPUT_PD11 = _ACMP_INPUTCTRL_POSSEL_PD11
SL_HAL_ACMP_INPUT_PD12 = _ACMP_INPUTCTRL_POSSEL_PD12
SL_HAL_ACMP_INPUT_PD13 = _ACMP_INPUTCTRL_POSSEL_PD13
SL_HAL_ACMP_INPUT_PD14 = _ACMP_INPUTCTRL_POSSEL_PD14
SL_HAL_ACMP_INPUT_PD15 = _ACMP_INPUTCTRL_POSSEL_PD15
}

Input Selection.

Functions#

void
sl_hal_acmp_init(ACMP_TypeDef *acmp, const sl_hal_acmp_init_t *init)

Initialize ACMP.

void
sl_hal_acmp_reset(ACMP_TypeDef *acmp)

Reset ACMP to the state it is after a hardware reset.

void
sl_hal_acmp_setup_gpio_inversion(ACMP_TypeDef *acmp, bool invert)

Set up GPIO output inversion from the ACMP.

void
sl_hal_acmp_set_input(ACMP_TypeDef *acmp, sl_hal_acmp_input_t negative_input, sl_hal_acmp_input_t positive_input)

Set which channels are used in ACMP comparisons.

void
sl_hal_acmp_enable(ACMP_TypeDef *acmp)

Enable ACMP.

void
sl_hal_acmp_disable(ACMP_TypeDef *acmp)

Disable ACMP.

void
sl_hal_acmp_clear_interrupts(ACMP_TypeDef *acmp, uint32_t flags)

Clear one or more pending ACMP interrupts.

void
sl_hal_acmp_disable_interrupts(ACMP_TypeDef *acmp, uint32_t flags)

Disable one or more ACMP interrupts.

void
sl_hal_acmp_enable_interrupts(ACMP_TypeDef *acmp, uint32_t flags)

Enable one or more ACMP interrupts.

uint32_t

Get pending ACMP interrupt flags.

uint32_t

Get enabled and pending ACMP interrupt flags.

uint32_t

Get enabled ACMP interrupts.

void
sl_hal_acmp_set_interrupts(ACMP_TypeDef *acmp, uint32_t flags)

Set one or more pending ACMP interrupts from software.

sl_hal_acmp_gpio_to_input(uint32_t port, uint32_t pin)

Convert GPIO port/pin to ACMP input selection.

void
sl_hal_acmp_wait_sync(ACMP_TypeDef *acmp)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

void
sl_hal_acmp_wait_ready(ACMP_TypeDef *acmp)

Wait for disabling to finish.

uint32_t
sl_hal_acmp_get_status(ACMP_TypeDef *acmp)

Return the content of the status register.

Macros#

#define
SL_HAL_ACMP_REF_VALID (ref)

Validation of ACMP register block pointer reference for assert statements.

#define
PM5507_ACMP_CFG_BIAS_DEFAULT 0x00000004UL

Analog comparator CFG with initial bias value.

#define
PM5507_ACMP_CFG_RESETVALUE 0x00000004UL

Analog comparator reset value.

#define
SL_HAL_ACMP_INIT_DEFAULT undefined

Default configuration for ACMP regular initialization.

Enumeration Documentation#

sl_hal_acmp_hysteresis_t#

sl_hal_acmp_hysteresis_t

Hysteresis level.

Enumerator
SL_HAL_ACMP_HYSTERESIS_DISABLED

Mode DISABLED for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_SYM_10MV

Mode HYST10SYM for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_SYM_20MV

Mode HYST20SYM for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_SYM_30MV

Mode HYST30SYM for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_POS_10MV

Mode HYST10POS for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_POS_20MV

Mode HYST20POS for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_POS_30MV

Mode HYST30POS for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_NEG_10MV

Mode HYST10NEG for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_NEG_20MV

Mode HYST20NEG for ACMP_CFG.

SL_HAL_ACMP_HYSTERESIS_NEG_30MV

Mode HYST30NEG for ACMP_CFG.


sl_hal_acmp_input_range_t#

sl_hal_acmp_input_range_t

vcm/input range.

Enumerator
SL_HAL_ACMP_INPUT_RANGE_FULL

Input can be from 0 to VDD.

SL_HAL_ACMP_INPUT_RANGE_REDUCED

Input can be from 0 to VDD-0.7 V.


sl_hal_acmp_accuracy_t#

sl_hal_acmp_accuracy_t

Accuracy mode.

Enumerator
SL_HAL_ACMP_ACCURACY_LOW

Low-accuracy mode which consumes less current.

SL_HAL_ACMP_ACCURACY_HIGH

High-accuracy mode which consumes more current.


sl_hal_acmp_input_t#

sl_hal_acmp_input_t

Input Selection.

Enumerator
SL_HAL_ACMP_INPUT_VSS

Select VSS.

SL_HAL_ACMP_INPUT_VREFDIVAVDD

Select Divided AVDD.

SL_HAL_ACMP_INPUT_VREFDIVAVDDLP

Select Low-Power Divided AVDD.

SL_HAL_ACMP_INPUT_VREFDIV1V25

Select Divided 1V25 reference.

SL_HAL_ACMP_INPUT_VREFDIV1V25LP

Select Low-power Divided 1V25 reference.

SL_HAL_ACMP_INPUT_VREFDIV2V5

Select Divided 2V5 reference.

SL_HAL_ACMP_INPUT_VREFDIV2V5LP

Select Low-power Divided 2V5 reference.

SL_HAL_ACMP_INPUT_VSENSE01DIV4

Select VSENSE0 divided by 4.

SL_HAL_ACMP_INPUT_VSENSE01DIV4LP

Select Low-power VSENSE0 divided by 4.

SL_HAL_ACMP_INPUT_VSENSE11DIV4

Select VSENSE1 divided by 4.

SL_HAL_ACMP_INPUT_VSENSE11DIV4LP

Select Low-power VSENSE1 divided by 4.

SL_HAL_ACMP_INPUT_EXTPA

Select external interface, base is PA0.

SL_HAL_ACMP_INPUT_EXTPB

Select external interface, base is PB0.

SL_HAL_ACMP_INPUT_EXTPC

Select external interface, base is PC0.

SL_HAL_ACMP_INPUT_EXTPD

Select external interface, base is PD0.

SL_HAL_ACMP_INPUT_PA0

Select Port A Pin0.

SL_HAL_ACMP_INPUT_PA1

Select Port A Pin1.

SL_HAL_ACMP_INPUT_PA2

Select Port A Pin2.

SL_HAL_ACMP_INPUT_PA3

Select Port A Pin3.

SL_HAL_ACMP_INPUT_PA4

Select Port A Pin4.

SL_HAL_ACMP_INPUT_PA5

Select Port A Pin5.

SL_HAL_ACMP_INPUT_PA6

Select Port A Pin6.

SL_HAL_ACMP_INPUT_PA7

Select Port A Pin7.

SL_HAL_ACMP_INPUT_PA8

Select Port A Pin8.

SL_HAL_ACMP_INPUT_PA9

Select Port A Pin9.

SL_HAL_ACMP_INPUT_PA10

Select Port A Pin10.

SL_HAL_ACMP_INPUT_PA11

Select Port A Pin11.

SL_HAL_ACMP_INPUT_PA12

Select Port A Pin12.

SL_HAL_ACMP_INPUT_PA13

Select Port A Pin13.

SL_HAL_ACMP_INPUT_PA14

Select Port A Pin14.

SL_HAL_ACMP_INPUT_PA15

Select Port A Pin15.

SL_HAL_ACMP_INPUT_PB0

Select Port B Pin0.

SL_HAL_ACMP_INPUT_PB1

Select Port B Pin1.

SL_HAL_ACMP_INPUT_PB2

Select Port B Pin2.

SL_HAL_ACMP_INPUT_PB3

Select Port B Pin3.

SL_HAL_ACMP_INPUT_PB4

Select Port B Pin4.

SL_HAL_ACMP_INPUT_PB5

Select Port B Pin5.

SL_HAL_ACMP_INPUT_PB6

Select Port B Pin6.

SL_HAL_ACMP_INPUT_PB7

Select Port B Pin7.

SL_HAL_ACMP_INPUT_PB8

Select Port B Pin8.

SL_HAL_ACMP_INPUT_PB9

Select Port B Pin9.

SL_HAL_ACMP_INPUT_PB10

Select Port B Pin10.

SL_HAL_ACMP_INPUT_PB11

Select Port B Pin11.

SL_HAL_ACMP_INPUT_PB12

Select Port B Pin12.

SL_HAL_ACMP_INPUT_PB13

Select Port B Pin13.

SL_HAL_ACMP_INPUT_PB14

Select Port B Pin14.

SL_HAL_ACMP_INPUT_PB15

Select Port B Pin15.

SL_HAL_ACMP_INPUT_PC0

Select Port C Pin0.

SL_HAL_ACMP_INPUT_PC1

Select Port C Pin1.

SL_HAL_ACMP_INPUT_PC2

Select Port C Pin2.

SL_HAL_ACMP_INPUT_PC3

Select Port C Pin3.

SL_HAL_ACMP_INPUT_PC4

Select Port C Pin4.

SL_HAL_ACMP_INPUT_PC5

Select Port C Pin5.

SL_HAL_ACMP_INPUT_PC6

Select Port C Pin6.

SL_HAL_ACMP_INPUT_PC7

Select Port C Pin7.

SL_HAL_ACMP_INPUT_PC8

Select Port C Pin8.

SL_HAL_ACMP_INPUT_PC9

Select Port C Pin9.

SL_HAL_ACMP_INPUT_PC10

Select Port C Pin10.

SL_HAL_ACMP_INPUT_PC11

Select Port C Pin11.

SL_HAL_ACMP_INPUT_PC12

Select Port C Pin12.

SL_HAL_ACMP_INPUT_PC13

Select Port C Pin13.

SL_HAL_ACMP_INPUT_PC14

Select Port C Pin14.

SL_HAL_ACMP_INPUT_PC15

Select Port C Pin15.

SL_HAL_ACMP_INPUT_PD0

Select Port D Pin0.

SL_HAL_ACMP_INPUT_PD1

Select Port D Pin1.

SL_HAL_ACMP_INPUT_PD2

Select Port D Pin2.

SL_HAL_ACMP_INPUT_PD3

Select Port D Pin3.

SL_HAL_ACMP_INPUT_PD4

Select Port D Pin4.

SL_HAL_ACMP_INPUT_PD5

Select Port D Pin5.

SL_HAL_ACMP_INPUT_PD6

Select Port D Pin6.

SL_HAL_ACMP_INPUT_PD7

Select Port D Pin7.

SL_HAL_ACMP_INPUT_PD8

Select Port D Pin8.

SL_HAL_ACMP_INPUT_PD9

Select Port D Pin9.

SL_HAL_ACMP_INPUT_PD10

Select Port D Pin10.

SL_HAL_ACMP_INPUT_PD11

Select Port D Pin11.

SL_HAL_ACMP_INPUT_PD12

Select Port D Pin12.

SL_HAL_ACMP_INPUT_PD13

Select Port D Pin13.

SL_HAL_ACMP_INPUT_PD14

Select Port D Pin14.

SL_HAL_ACMP_INPUT_PD15

Select Port D Pin15.


Function Documentation#

sl_hal_acmp_init#

void sl_hal_acmp_init (ACMP_TypeDef * acmp, const sl_hal_acmp_init_t * init)

Initialize ACMP.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

const sl_hal_acmp_init_t *[in]init

A pointer to the initialization structure used to configure ACMP.

Note

  • A call to ACMP_Init can cause side effects since it can enable/disable the peripheral.


sl_hal_acmp_reset#

void sl_hal_acmp_reset (ACMP_TypeDef * acmp)

Reset ACMP to the state it is after a hardware reset.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

Note

  • The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.

  • The peripheral may be enabled and disabled during reset.


sl_hal_acmp_setup_gpio_inversion#

void sl_hal_acmp_setup_gpio_inversion (ACMP_TypeDef * acmp, bool invert)

Set up GPIO output inversion from the ACMP.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

Pointer to the ACMP peripheral register block.

bool[in]invert

true = GPIO output is inverted. false = GPIO output is not inverted.


sl_hal_acmp_set_input#

void sl_hal_acmp_set_input (ACMP_TypeDef * acmp, sl_hal_acmp_input_t negative_input, sl_hal_acmp_input_t positive_input)

Set which channels are used in ACMP comparisons.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

sl_hal_acmp_input_t[in]negative_input

ACMP channel for the negative input.

sl_hal_acmp_input_t[in]positive_input

ACMP channel for the positive input.

Note

  • Can only be called when the peripheral is enabled.

  • If GPIO is used for both posSel and negSel, they cannot both use even or odd pins.


sl_hal_acmp_enable#

void sl_hal_acmp_enable (ACMP_TypeDef * acmp)

Enable ACMP.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.


sl_hal_acmp_disable#

void sl_hal_acmp_disable (ACMP_TypeDef * acmp)

Disable ACMP.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.


sl_hal_acmp_clear_interrupts#

void sl_hal_acmp_clear_interrupts (ACMP_TypeDef * acmp, uint32_t flags)

Clear one or more pending ACMP interrupts.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

uint32_t[in]flags

Pending ACMP interrupt source to clear. Use one or more valid interrupt flags for the ACMP module (ACMP_IF_nnn) OR'ed together.


sl_hal_acmp_disable_interrupts#

void sl_hal_acmp_disable_interrupts (ACMP_TypeDef * acmp, uint32_t flags)

Disable one or more ACMP interrupts.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

uint32_t[in]flags

ACMP interrupt sources to disable. Use one or more valid interrupt flags for the ACMP module (ACMP_IF_nnn) OR'ed together.


sl_hal_acmp_enable_interrupts#

void sl_hal_acmp_enable_interrupts (ACMP_TypeDef * acmp, uint32_t flags)

Enable one or more ACMP interrupts.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

uint32_t[in]flags

ACMP interrupt sources to enable. Use one or more valid interrupt flags for the ACMP module (ACMP_IF_nnn) OR'ed together.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Use ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.


sl_hal_acmp_get_pending_interrupts#

uint32_t sl_hal_acmp_get_pending_interrupts (ACMP_TypeDef * acmp)

Get pending ACMP interrupt flags.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

Note

  • This function does not clear event bits.

Returns

  • Pending ACMP interrupt sources. Use one or more valid interrupt flags for the ACMP module (ACMP_IF_nnn) OR'ed together.


sl_hal_acmp_get_enabled_pending_interrupts#

uint32_t sl_hal_acmp_get_enabled_pending_interrupts (ACMP_TypeDef * acmp)

Get enabled and pending ACMP interrupt flags.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • This function does not clear interrupt flags.

Returns

  • Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).


sl_hal_acmp_get_enabled_interrupts#

uint32_t sl_hal_acmp_get_enabled_interrupts (ACMP_TypeDef * acmp)

Get enabled ACMP interrupts.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Enabled ACMP interrupt sources.


sl_hal_acmp_set_interrupts#

void sl_hal_acmp_set_interrupts (ACMP_TypeDef * acmp, uint32_t flags)

Set one or more pending ACMP interrupts from software.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

uint32_t[in]flags

ACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP.


sl_hal_acmp_gpio_to_input#

sl_hal_acmp_input_t sl_hal_acmp_gpio_to_input (uint32_t port, uint32_t pin)

Convert GPIO port/pin to ACMP input selection.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]port

GPIO port to convert.

uint32_t[in]pin

GPIO pin to convert.

Returns

  • ACMP input selection of the selected GPIO port and pin.


sl_hal_acmp_wait_sync#

void sl_hal_acmp_wait_sync (ACMP_TypeDef * acmp)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.


sl_hal_acmp_wait_ready#

void sl_hal_acmp_wait_ready (ACMP_TypeDef * acmp)

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.


sl_hal_acmp_get_status#

uint32_t sl_hal_acmp_get_status (ACMP_TypeDef * acmp)

Return the content of the status register.

Parameters
TypeDirectionArgument NameDescription
ACMP_TypeDef *[in]acmp

A pointer to the ACMP peripheral register block.

Returns

  • Status register.