PRS async channel configuration structure.
Public Attributes#
uint8_t
Channel number.
uint8_t
Channel to input to logic block.
Lookup function for configurable logic.
Peripheral signal.
Peripheral consumer. Used to select which signal to listen to.
Public Attribute Documentation#
logic#
sl_hal_prs_logic_t sl_hal_prs_async_channel_init_t::logic
Lookup function for configurable logic.
producer_signal#
sl_hal_prs_async_producer_signal_t sl_hal_prs_async_channel_init_t::producer_signal
Peripheral signal.
consumer_event#
sl_hal_prs_consumer_event_t sl_hal_prs_async_channel_init_t::consumer_event
Peripheral consumer. Used to select which signal to listen to.