Power Manager#
Power manager is a platform level software module that manages the system's energy modes. Its main purpose is to transition the system to a low energy mode when the processor has nothing to execute. The energy mode the system will transition to is determined each time the system goes to sleep using requirements. These requirements are set by the different software modules (drivers, stacks, application code, etc...). Power manager also ensures a strict control of some power hungry resources such as the high frequency external oscillator (normally called HFXO). Power manager also offers a notification mechanism through which any piece of software module can be notified of energy mode transitions through callbacks.
Note
Emlib EMU functions EMU_EnterEM1()/EMU_EnterEM2()/EMU_EnterEM3() must not be used when the Power Manager is present. The Power Manager module must be the one deciding at which EM level the device sleeps to ensure the application properly works. Using both at the same time could lead to undefined behavior in the application.
Initialization#
Power manager must be initialized prior to any call to power manager API. If sl_system or sl_main is used, the sl_power_manager_init() function will be part of the initilization sequence handled by those modules. Otherwise sl_power_manager_init() must be called manually. Note that power manager must be initialized after the clock(s), when initialized manually, as the power manager check which oscillators are used during the initialization phase.
Add and remove requirements#
The drivers should add and remove energy mode requirements, at runtime, on the lowest energy mode for them depending on their state. When calling sl_power_manager_sleep(), the lowest possible Energy mode will be automatically selected.
It is possible to add and remove requirements from ISR. If a specific energy mode is required in the ISR, but not required to generate the interrupt, a requirement on the energy mode can be added from the ISR. It is guaranteed that the associated clock will be active once sl_power_manager_add_em_requirement() returns. The EM requirement can be also be removed from an ISR.
Requirements should not be removed if it was not previously added.
Subscribe to events#
It possible to get notified when the system transition from a power level to another power level. This can allow to do some operations depending on which level the system goes, such as saving/restoring context.
Sleep#
When the software has no more operation and only need to wait for an event, the software must call sl_power_manager_sleep(). This is automatically done when a kernel is present, but it needs to be called from the super loop in a baremetal project.
Query callback functions#
Is OK to sleep#
Between the time sl_power_manager_sleep is called and the MCU is really put in a lower Energy mode, it is possible that an ISR occur and require the system to resume at that time instead of sleeping. So a callback is called in a critical section to validate that the MCU can go to sleep.
In case of an application that runs on an RTOS, the RTOS will take care of determining if it is ok to sleep. In case of a baremetal application, the function sl_power_manager_is_ok_to_sleep() will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to take a decision. The application can contribute to the decision by defining the function app_is_ok_to_sleep(). If any of the software modules (including the application via app_is_ok_to_sleep()) return false, the process of entering in sleep will be aborted.
Sleep on ISR exit#
When the system enters sleep, the only way to wake it up is via an interrupt or exception. By default, power manager will assume that when an interrupt occurs and the corresponding ISR has been executed, the system must not go back to sleep. However, in the case where all the processing related to this interrupt is performed in the ISR, it is possible to go back to sleep by using this hook.
In case of an application that runs on an RTOS, the RTOS will take care of determining if the system can go back to sleep on ISR exit. Power manager will ensure the system resumes its operations as soon as a task is resumed, posted or that its delay expires. In case of a baremetal application, the function sl_power_manager_sleep_on_isr_exit() will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to take a decision. The application can contribute to the decision by defining the function app_sleep_on_isr_exit(). The generated function will take a decision based on the value returned by the different software modules (including the application via app_sleep_on_isr_exit()):
SL_POWER_MANAGER_IGNORE: if the software module did not cause the system wakeup and/or doesn't want to contribute to the decision. SL_POWER_MANAGER_SLEEP: if the software module did cause the system wakeup, but the system should go back to sleep. SL_POWER_MANAGER_WAKEUP: if the software module did cause the system wakeup, and the system should not go back to sleep.
If any software module returned SL_POWER_MANAGER_SLEEP and none returned SL_POWER_MANAGER_WAKEUP, the system will go back to sleep. Any other combination will cause the system not to go back to sleep.
Debugging feature#
By setting the configuration define SL_POWER_MANAGER_DEBUG to 1, it is possible to record the requirements currently set and their owner. It is possible to print at any time a table that lists all the added requirements and their owner. This table can be printed by caling the function sl_power_manager_debug_print_em_requirements(). Make sure to add the following define
#define CURRENT_MODULE_NAME "<Module printable name here>"
to any application code source file that adds and removes requirements.
Usage Example#
#define EM_EVENT_MASK_ALL (SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM0 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM0 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM1 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM1 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM2 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM2)
sl_power_manager_em_transition_event_handle_t event_handle;
sl_power_manager_em_transition_event_info_t event_info = {
.event_mask = EM_EVENT_MASK_ALL,
.on_event = my_events_callback,
}
void main(void)
{
// Initialize power manager; not needed if sl_system_init() is used.
sl_power_manager_init();
// Limit sleep level to EM1.
sl_power_manager_add_em_requirement(SL_POWER_MANAGER_EM1);
// Subscribe to all event types; get notified for every power transition.
sl_power_manager_subscribe_em_transition_event(&event_handle, &event_info);
while (1) {
// Actions
[...]
if (completed) {
// Remove energy mode requirement, can go to EM2 or EM3 now, depending on the configuration.
sl_power_manager_remove_em_requirement(SL_POWER_MANAGER_EM1);
}
// Sleep to lowest possible energy mode; This call is not needed when using the kernel.
sl_power_manager_sleep();
// Will resume after an interrupt or exception.
}
}
void my_events_callback(sl_power_manager_em_t from,
sl_power_manager_em_t to)
{
printf("Event:%s-%s\r\n", string_lookup_table[from], string_lookup_table[to]);
}
EM4 Sleep#
The Power Manager module provides support for entering Energy Mode 4 (EM4), the lowest energy mode available.
To enter EM4, the sl_power_manager_enter_em4() function is used. This function ensures that the system transitions to EM4 safely and performs any necessary pre-sleep operations via the sl_power_manager_em4_presleep_hook() function, which can be overridden by the application if additional actions are required.
Additionally, the Power Manager provides support for EM4 pin retention. Use the SL_POWER_MANAGER_INIT_EMU_EM4_PIN_RETENTION_MODE configuration to set the pin retention mode in EM4. When enabled, pins retain their state through EM4 entry and wake-up. The retained pin state can be released after wake-up by calling the sl_power_manager_em4_unlatch_pin_retention() function.
Keep in mind that EM4 entry is irreversible, and waking up from this energy mode will result in a system reset. Careful consideration should be given to the conditions under which EM4 is entered.
Update Power Manager after runtime clock changes#
The slx_power_manager_update_clock_info() API is an advanced function used to update the Power Manager's internal information about the system's clock configuration. This is particularly important when the clock tree is modified during runtime, as the Power Manager relies on accurate clock data to evaluate energy mode transitions and wake-up times. It is essential to call this function after any clock changes to ensure the Power Manager operates correctly. Note that this function must be invoked when the system is fully restored and should not be called from ISRs or Power Manager notifications.
Execution Modes#
Power Manager has the Executions Modes feature which is specific to series 3 devices. It can be enabled by setting the configuration SL_POWER_MANAGER_EXECUTION_MODES_FEATURE_EN. When this feature is active, the system can dynamically switch between Standard and Performance modes during normal execution in EM0. Performance mode typically increases the system clock frequency, providing enhanced performance. The exact specifications and behavior of Standard and Performance modes are device-specific.
To manage these modes, use the following APIs:
sl_power_manager_add_performance_mode_requirement() : Add a requirement on the Performance mode. If no previous requirement were added, this will activate the Performance mode.
sl_power_manager_remove_performance_mode_requirement() : Remove a previously added requirement. If the last requirement is removed, this will deactivate the Performance mode and reverts to Standard mode.
Advanced Functionalities#
Update Power Manager after runtime clock changes#
The Power Manager initialization must occur after the clocks are initialized, as it relies on the clock configuration to determine which clocks to restore during wake-ups. Using sl_system or sl_main modules will automatically call the clock and power initialization functions in the right order as part of their initialization sequence. If any clock branches are modified at runtime, the Power Manager must be informed of these changes to ensure proper clock restoration after sleep.
To handle this, use the slx_power_manager_update_clock_info() API. This function captures the current clock configuration and must be called after any runtime changes to the clock tree. It ensures the Power Manager has accurate information for restoring clocks during wake-ups.
Important: Call slx_power_manager_update_clock_info() only when the system is fully restored, as it takes a snapshot of the current clock usage. Avoid invoking this function from ISRs or within Power Manager notifications.
Important: Modifying the clock tree at runtime is an advanced operation and should only be performed with a thorough understanding of its potential impact on other modules sharing the same clock branch and the overall system stability.
Additional Information#
For more information on the Power Manager module please refer to this Power Manager guide.
Modules#
sl_power_manager_em_transition_event_info_t
sl_power_manager_em_transition_event_handle_t
Enumerations#
Energy modes.
On ISR Exit Hook answer.
Typedefs#
Mask of all the event(s) to listen to.
Typedef for the user supplied callback function which is called when an energy mode transition occurs.
Functions#
Initialize Power Manager module.
Sleep at the lowest allowed energy mode.
Adds requirement on given energy mode.
Removes requirement on given energy mode.
Registers a callback to be called on given Energy Mode transition(s).
Unregisters an event callback handle on Energy mode transition.
Get configurable overhead value for early restore time in Sleeptimer ticks when a schedule wake-up is set.
Set configurable overhead value for early restore time in Sleeptimer ticks used for schedule wake-up.
Get configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
Set configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
Enable or disable fast wake-up in EM2 and EM3.
Determines if the HFXO interrupt was part of the last wake-up and/or if the HFXO early wakeup expired during the last ISR and if it was the only timer to expire in that period.
Enter energy mode 4 (EM4).
When EM4 pin retention is set to power_manager_pin_retention_latch, then pins are retained through EM4 entry and wakeup.
Energy mode 4 pre-sleep hook function.
Updates the clocks information used by the Power Manager to evaluate the EM2/3 wake-up time.
Adds requirement on performance execution mode.
Removes requirement on performance execution mode.
Print a table that describes the current requirements on each energy mode and their owner.
Macros#
current module name
sl power manager event transition entering em0
sl power manager event transition leaving em0
sl power manager event transition entering em1
sl power manager event transition leaving em1
sl power manager event transition entering em2
sl power manager event transition leaving em2
Enumeration Documentation#
sl_power_manager_em_t#
sl_power_manager_em_t
Energy modes.
| Enumerator | |
|---|---|
| SL_POWER_MANAGER_EM0 | Run Mode (Energy Mode 0) |
| SL_POWER_MANAGER_EM1 | Sleep Mode (Energy Mode 1) |
| SL_POWER_MANAGER_EM2 | Deep Sleep Mode (Energy Mode 2) |
| SL_POWER_MANAGER_EM3 | Stop Mode (Energy Mode 3) |
| SL_POWER_MANAGER_EM4 | Shutoff Mode (Energy Mode 4) |
sl_power_manager_on_isr_exit_t#
sl_power_manager_on_isr_exit_t
On ISR Exit Hook answer.
| Enumerator | |
|---|---|
| SL_POWER_MANAGER_IGNORE | The module did not trigger an ISR and it doesn't want to contribute to the decision. |
| SL_POWER_MANAGER_SLEEP | The module was the one that caused the system wakeup and the system SHOULD go back to sleep. |
| SL_POWER_MANAGER_WAKEUP | The module was the one that caused the system wakeup and the system MUST NOT go back to sleep. |
Typedef Documentation#
sl_power_manager_em_transition_event_t#
typedef uint32_t sl_power_manager_em_transition_event_t
Mask of all the event(s) to listen to.
sl_power_manager_em_transition_on_event_t#
typedef void(* sl_power_manager_em_transition_on_event_t) (sl_power_manager_em_t from, sl_power_manager_em_t to) )(sl_power_manager_em_t from, sl_power_manager_em_t to)
Typedef for the user supplied callback function which is called when an energy mode transition occurs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | from | Energy mode we are leaving. | |
| N/A | to | Energy mode we are entering. |
Function Documentation#
sl_power_manager_init#
sl_status_t sl_power_manager_init (void )
Initialize Power Manager module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code
sl_power_manager_sleep#
void sl_power_manager_sleep (void )
Sleep at the lowest allowed energy mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
Must not be called from ISR
This function will expect and call a callback with the following signature:
bool sl_power_manager_is_ok_to_sleep(void). This callback can be used to cancel a sleep action and handle the possible race condition where an ISR that would cause a wakeup is triggered right after the decision to call sl_power_manager_sleep() has been made.This function must NOT be called with interrupts disabled. This means both BASEPRI and PRIMASK MUST have a value of 0 when invoking this function.
Usage example:
void main(void)
{
sl_power_manager_init();
while (1) {
tick();
sl_power_manager_sleep();
}
}
sl_power_manager_add_em_requirement#
void sl_power_manager_add_em_requirement (sl_power_manager_em_t em)
Adds requirement on given energy mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_em_t | N/A | em | Energy mode to add the requirement to: |
sl_power_manager_remove_em_requirement#
void sl_power_manager_remove_em_requirement (sl_power_manager_em_t em)
Removes requirement on given energy mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_em_t | N/A | em | Energy mode to remove the requirement to: |
sl_power_manager_subscribe_em_transition_event#
void sl_power_manager_subscribe_em_transition_event (sl_power_manager_em_transition_event_handle_t * event_handle, const sl_power_manager_em_transition_event_info_t * event_info)
Registers a callback to be called on given Energy Mode transition(s).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_em_transition_event_handle_t * | N/A | event_handle | Event handle (no initialization needed). |
| const sl_power_manager_em_transition_event_info_t * | N/A | event_info | Event info structure that contains the event mask and the callback that must be called. |
Note
Adding and removing requirement(s) from a callback on a transition event is not supported.
The parameters passed must be persistent, meaning that they need to survive until the callback fires.
Usage example:
#define EM_EVENT_MASK_ALL ( SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM0 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM0 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM1 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM1 \
| SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM2 \
| SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM2)
sl_power_manager_em_transition_event_handle_t event_handle;
sl_power_manager_em_transition_event_info_t event_info = {
.event_mask = EM_EVENT_MASK_ALL,
.on_event = my_callback,
};
void my_callback(sl_power_manager_em_t from,
sl_power_manager_em_t to)
{
[...]
}
void main(void)
{
sl_power_manager_init();
sl_power_manager_subscribe_em_transition_event(&event_handle, &event_info);
}
sl_power_manager_unsubscribe_em_transition_event#
void sl_power_manager_unsubscribe_em_transition_event (sl_power_manager_em_transition_event_handle_t * event_handle)
Unregisters an event callback handle on Energy mode transition.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_power_manager_em_transition_event_handle_t * | N/A | event_handle | Event handle which must be unregistered (must have been registered previously). |
Note
An EFM_ASSERT is thrown if the handle is not found.
sl_power_manager_schedule_wakeup_get_restore_overhead_tick#
int32_t sl_power_manager_schedule_wakeup_get_restore_overhead_tick (void )
Get configurable overhead value for early restore time in Sleeptimer ticks when a schedule wake-up is set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current overhead value for early restore time.
Note
This function will do nothing when a project contains the power_manager_no_deepsleep component, which configures the lowest energy mode as EM1.
sl_power_manager_schedule_wakeup_set_restore_overhead_tick#
void sl_power_manager_schedule_wakeup_set_restore_overhead_tick (int32_t overhead_tick)
Set configurable overhead value for early restore time in Sleeptimer ticks used for schedule wake-up.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | N/A | overhead_tick | Overhead value to set for early restore time. |
Must be called after initialization else the value will be overwritten.
Note
The overhead value can also be negative to remove time from the restore process.
This function will do nothing when a project contains the power_manager_no_deepsleep component, which configures the lowest energy mode as EM1.
sl_power_manager_schedule_wakeup_get_minimum_offtime_tick#
uint32_t sl_power_manager_schedule_wakeup_get_minimum_offtime_tick (void )
Get configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current minimum off-time value for schedule wake-up.
Note
Turning on external high frequency clock, such as HFXO, requires more energy since we must supply higher current for the wake-up. Therefore, when an 'external high frequency clock enable' is scheduled in 'x' time, there is a threshold 'x' value where turning off the clock is not worthwhile since the energy consumed by taking into account the wake-up will be greater than if we just keep the clock on until the next scheduled clock enabled. This threshold value is what we refer as the minimum off-time.
This function will do nothing when a project contains the power_manager_no_deepsleep component, which configures the lowest energy mode as EM1.
sl_power_manager_schedule_wakeup_set_minimum_offtime_tick#
void sl_power_manager_schedule_wakeup_set_minimum_offtime_tick (uint32_t minimum_offtime_tick)
Set configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | minimum_offtime_tick | minimum off-time value to set for schedule wake-up. |
Note
Turning on external high frequency clock, such as HFXO, requires more energy since we must supply higher current for the wake-up. Therefore, when an 'external high frequency clock enable' is scheduled in 'x' time, there is a threshold 'x' value where turning off the clock is not worthwhile since the energy consumed by taking into account the wake-up will be greater than if we just keep the clock on until the next scheduled clock enabled. This threshold value is what we refer as the minimum off-time.
This function will do nothing when a project contains the power_manager_no_deepsleep component, which configures the lowest energy mode as EM1.
sl_power_manager_em23_voltage_scaling_enable_fast_wakeup#
void sl_power_manager_em23_voltage_scaling_enable_fast_wakeup (bool enable)
Enable or disable fast wake-up in EM2 and EM3.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | enable | True False variable act as a switch for this api |
Note
Will also update the wake up time from EM2 to EM0.
This function will do nothing when a project contains the power_manager_no_deepsleep component, which configures the lowest energy mode as EM1.
sl_power_manager_is_latest_wakeup_internal#
bool sl_power_manager_is_latest_wakeup_internal (void )
Determines if the HFXO interrupt was part of the last wake-up and/or if the HFXO early wakeup expired during the last ISR and if it was the only timer to expire in that period.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if power manager sleep can return to sleep, false otherwise.
Note
This function will always return false in case a requirement is added on SL_POWER_MANAGER_EM1, since we will never sleep at a lower level than EM1.
sl_power_manager_enter_em4#
void sl_power_manager_enter_em4 (void )
Enter energy mode 4 (EM4).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
You should not expect to return from this function. Once the device enters EM4, only a power on reset or external reset pin can wake the device.
On xG22 devices, this function re-configures the IADC if EM4 entry is possible.
sl_power_manager_em4_unlatch_pin_retention#
void sl_power_manager_em4_unlatch_pin_retention (void )
When EM4 pin retention is set to power_manager_pin_retention_latch, then pins are retained through EM4 entry and wakeup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The pin state is released by calling this function. The feature allows peripherals or GPIO to be re-initialized after EM4 exit (reset), and when initialization is done, this function can release pins and return control to the peripherals or GPIO.
Note
When the EM4 Pin Retention feature is not available on a device, calling this function will do nothing.
sl_power_manager_em4_presleep_hook#
void sl_power_manager_em4_presleep_hook (void )
Energy mode 4 pre-sleep hook function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
This function is called by sl_power_manager_enter_em4 just prior to the sequence of writes to put the device in EM4. The function implementation does not perform anything, but it is SL_WEAK so that it can be re-implemented in application code if actions are needed.
slx_power_manager_update_clock_info#
void slx_power_manager_update_clock_info (void )
Updates the clocks information used by the Power Manager to evaluate the EM2/3 wake-up time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
This function is an advanced function used in case the clock tree is changed during runtime. Call this function after the clock change so that the Power Manager module can update its internal information about the clocks.
This function must always be called when the system is fully restored since it's taking a snapshot of the current clock usage. Therefore, it must not be called from ISRs and Power Manager notifications.
sl_power_manager_add_performance_mode_requirement#
void sl_power_manager_add_performance_mode_requirement (void )
Adds requirement on performance execution mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_power_manager_remove_performance_mode_requirement#
void sl_power_manager_remove_performance_mode_requirement (void )
Removes requirement on performance execution mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_power_manager_debug_print_em_requirements#
void sl_power_manager_debug_print_em_requirements (void )
Print a table that describes the current requirements on each energy mode and their owner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |