LETIMER - Low Energy Timer#
Example#
The following example demonstrates how to configure and use the LETIMER for PWM generation with a configurable duty cycle.
// Global flag for COMP0 interrupt
volatile bool comp0_occurred = false;
// LETIMER0 IRQ Handler
void LETIMER0_IRQHandler(void)
{
// Get pending interrupts
uint32_t flags = sl_hal_letimer_get_pending_interrupts(LETIMER0);
// Check for COMP0 interrupt
if (flags & LETIMER_IF_COMP0) {
// Clear the interrupt flag
sl_hal_letimer_clear_interrupts(LETIMER0, LETIMER_IF_COMP0);
// Set our flag to indicate the event occurred
comp0_occurred = true;
// Additional processing can be done here
}
}
// Example of configuring LETIMER for PWM generation
void letimer_pwm_example(void)
{
// Enable bus clock for LETIMER0
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LETIMER0);
// Initialize with custom configuration for PWM generation
sl_hal_letimer_init_t init = SL_HAL_LETIMER_INIT_DEFAULT;
// Set prescaler to divide clock by 4
init.prescaler = SL_HAL_LETIMER_PRESCALER_DIV4;
// Free-running mode
init.repeat_mode = SL_HAL_LETIMER_REPEAT_MODE_FREE;
// Configure PWM on output 0
init.underflow_output0_action = SL_HAL_LETIMER_UNDERFLOW_OUTPUT_ACTION_PWM;
// Reload TOP on underflow
init.enable_top = true;
// Initialize LETIMER with our configuration
sl_hal_letimer_init(LETIMER0, &init);
// Enable LETIMER
sl_hal_letimer_enable(LETIMER0);
// Set TOP value for desired frequency
// For example, with 32.768 kHz clock, div4 prescaler, and TOP=1000:
// Frequency = 32768 / 4 / 1000 = 8.192 Hz
sl_hal_letimer_set_top(LETIMER0, 1000);
// Set compare values to control PWM duty cycle
// COMP0 = 0 (active at start of period)
sl_hal_letimer_set_compare(LETIMER0, 0, 0);
// COMP1 = 500 (50% duty cycle)
sl_hal_letimer_set_compare(LETIMER0, 1, 500);
// Clear any pending interrupts
sl_hal_letimer_clear_interrupts(LETIMER0, _LETIMER_IF_MASK);
// Enable COMP0 interrupt to trigger at the start of each period
sl_hal_letimer_enable_interrupts(LETIMER0, LETIMER_IEN_COMP0);
// Enable NVIC interrupt for LETIMER
sl_interrupt_manager_clear_irq_pending(LETIMER0_IRQn);
sl_interrupt_manager_enable_irq(LETIMER0_IRQn);
// Reset the event flag
comp0_occurred = false;
// Start LETIMER
sl_hal_letimer_start(LETIMER0);
// Wait for first COMP0 interrupt to occur
while (!comp0_occurred) {
// Could enter energy mode here to save power while waiting
}
// Change duty cycle to 25%
sl_hal_letimer_set_compare(LETIMER0, 1, 750); // 25% = (1000-750)/1000
// Application code would continue here
// ...
// When done, clean up
sl_hal_letimer_stop(LETIMER0);
sl_hal_letimer_disable_interrupts(LETIMER0, _LETIMER_IEN_MASK);
sl_interrupt_manager_disable_irq(LETIMER0_IRQn);
sl_hal_letimer_disable(LETIMER0);
sl_hal_letimer_wait_ready(LETIMER0);
}
Modules#
Enumerations#
Prescaler.
Repeat mode.
Underflow action on output.
Functions#
Initialize LETIMER.
Reset the LETIMER to the same state that it was in after a hardware reset.
Enable the LETIMER.
Disable LETIMER.
Wait for resetting and disabling to finish.
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
Get status values for the LETIMER.
Enable one or more LETIMER interrupts.
Disable one or more LETIMER interrupts.
Clear one or more pending LETIMER interrupts.
Set one or more pending LETIMER interrupts from SW.
Get pending LETIMER interrupt flags.
Get enabled and pending LETIMER interrupt flags.
Start LETIMER counter.
Stop LETIMER counter.
Set the LETIMER counter register value.
Get the LETIMER counter register value.
Set the LETIMER compare register value.
Get the LETIMER compare register value.
Set the LETIMER repeat register value.
Get the LETIMER repeat register value.
Set the LETIMER top register value.
Get the LETIMER top register value.
Set the LETIMER top register value buffer.
Get the LETIMER top register value buffer.
Macros#
Check if LETIMER module is valid.
Return LETIMER module max count.
Default configuration for LETIMER initialization structure.
Enumeration Documentation#
sl_hal_letimer_prescaler_t#
sl_hal_letimer_prescaler_t
Prescaler.
| Enumerator | |
|---|---|
| SL_HAL_LETIMER_PRESCALER_DIV1 | |
| SL_HAL_LETIMER_PRESCALER_DIV2 | Divide by 1. |
| SL_HAL_LETIMER_PRESCALER_DIV4 | Divide by 2. |
| SL_HAL_LETIMER_PRESCALER_DIV8 | Divide by 4. |
| SL_HAL_LETIMER_PRESCALER_DIV16 | Divide by 8. |
| SL_HAL_LETIMER_PRESCALER_DIV32 | Divide by 16. |
| SL_HAL_LETIMER_PRESCALER_DIV64 | Divide by 32. |
| SL_HAL_LETIMER_PRESCALER_DIV128 | Divide by 64. |
| SL_HAL_LETIMER_PRESCALER_DIV256 | Divide by 128. |
sl_hal_letimer_repeat_mode_t#
sl_hal_letimer_repeat_mode_t
Repeat mode.
| Enumerator | |
|---|---|
| SL_HAL_LETIMER_REPEAT_MODE_FREE | Count until stopped by SW. |
| SL_HAL_LETIMER_REPEAT_MODE_ONESHOT | Count REP0 times. |
| SL_HAL_LETIMER_REPEAT_MODE_BUFFERED | Count REP0 times, if REP1 has been written to, it is loaded into REP0 when REP0 is about to be decremented to 0. |
| SL_HAL_LETIMER_REPEAT_MODE_DOUBLE | Run as long as both REP0 and REP1 are not 0. |
sl_hal_letimer_underflow_output_action_t#
sl_hal_letimer_underflow_output_action_t
Underflow action on output.
| Enumerator | |
|---|---|
| SL_HAL_LETIMER_UNDERFLOW_OUTPUT_ACTION_NONE | No output action. |
| SL_HAL_LETIMER_UNDERFLOW_OUTPUT_ACTION_TOGGLE | Toggle output when counter underflows. |
| SL_HAL_LETIMER_UNDERFLOW_OUTPUT_ACTION_PULSE | Hold output one LETIMER clock cycle when counter underflows. |
| SL_HAL_LETIMER_UNDERFLOW_OUTPUT_ACTION_PWM | Set output idle when counter underflows, and active when matching COMP1. |
Function Documentation#
sl_hal_letimer_init#
void sl_hal_letimer_init (LETIMER_TypeDef * letimer, const sl_hal_letimer_init_t * init)
Initialize LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| const sl_hal_letimer_init_t * | [in] | init | A pointer to the LETIMER initialization structure. |
sl_hal_letimer_reset#
void sl_hal_letimer_reset (LETIMER_TypeDef * letimer)
Reset the LETIMER to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
sl_hal_letimer_enable#
void sl_hal_letimer_enable (LETIMER_TypeDef * letimer)
Enable the LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
sl_hal_letimer_disable#
void sl_hal_letimer_disable (LETIMER_TypeDef * letimer)
Disable LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
sl_hal_letimer_wait_ready#
void sl_hal_letimer_wait_ready (LETIMER_TypeDef * letimer)
Wait for resetting and disabling to finish.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
sl_hal_letimer_wait_sync#
void sl_hal_letimer_wait_sync (LETIMER_TypeDef * letimer)
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
sl_hal_letimer_get_status#
uint32_t sl_hal_letimer_get_status (LETIMER_TypeDef * letimer)
Get status values for the LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Returns
Current status values.
sl_hal_letimer_enable_interrupts#
void sl_hal_letimer_enable_interrupts (LETIMER_TypeDef * letimer, uint32_t flags)
Enable one or more LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt source(s) to enable. Use one or more valid interrupt flags for the LETIMER module (LETIMER_IF_nnn) OR'ed together. |
sl_hal_letimer_disable_interrupts#
void sl_hal_letimer_disable_interrupts (LETIMER_TypeDef * letimer, uint32_t flags)
Disable one or more LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt source(s) to disable. Use one or more valid interrupt flags for the LETIMER module (LETIMER_IF_nnn) OR'ed together. |
sl_hal_letimer_clear_interrupts#
void sl_hal_letimer_clear_interrupts (LETIMER_TypeDef * letimer, uint32_t flags)
Clear one or more pending LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | flags | Pending LETIMER interrupt source(s) to clear. Use one or more valid interrupt flags for the LETIMER module (LETIMER_IF_nnn) OR'ed together. |
sl_hal_letimer_set_interrupts#
void sl_hal_letimer_set_interrupts (LETIMER_TypeDef * letimer, uint32_t flags)
Set one or more pending LETIMER interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt source(s) to set to pending. Use one or more valid interrupt flags for the LETIMER module (LETIMER_IF_nnn) OR'ed together. |
sl_hal_letimer_get_pending_interrupts#
uint32_t sl_hal_letimer_get_pending_interrupts (LETIMER_TypeDef * letimer)
Get pending LETIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Note
Event bits are not cleared by this function.
Returns
LETIMER interrupt source(s) pending. Returns one or more valid interrupt flags for the LETIMER module (LETIMER_IF_nnn) OR'ed together.
sl_hal_letimer_get_enabled_pending_interrupts#
uint32_t sl_hal_letimer_get_enabled_pending_interrupts (LETIMER_TypeDef * letimer)
Get enabled and pending LETIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled LETIMER interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in LETIMERx_IEN_nnn register (LETIMERx_IEN_nnn) and
the OR combination of valid interrupt flags of the LETIMER module (LETIMERx_IF_nnn).
sl_hal_letimer_start#
void sl_hal_letimer_start (LETIMER_TypeDef * letimer)
Start LETIMER counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
This function will send a start command to the LETIMER peripheral. The LETIMER peripheral will use some LF clock ticks before the command is executed. The sl_hal_letimer_wait_sync() function can be used to wait for the start command to be executed.
sl_hal_letimer_stop#
void sl_hal_letimer_stop (LETIMER_TypeDef * letimer)
Stop LETIMER counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
This function will send a stop command to the LETIMER peripheral. The LETIMER peripheral will use some LF clock ticks before the command is executed. The sl_hal_letimer_wait_sync() function can be used to wait for the stop command to be executed.
sl_hal_letimer_set_counter#
void sl_hal_letimer_set_counter (LETIMER_TypeDef * letimer, uint32_t value)
Set the LETIMER counter register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | value | Value to set in counter register. |
sl_hal_letimer_get_counter#
uint32_t sl_hal_letimer_get_counter (LETIMER_TypeDef * letimer)
Get the LETIMER counter register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Returns
Current counter.
sl_hal_letimer_set_compare#
void sl_hal_letimer_set_compare (LETIMER_TypeDef * letimer, uint8_t channel, uint32_t value)
Set the LETIMER compare register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint8_t | [in] | channel | A compare register to set, either 0 or 1. |
| uint32_t | [in] | value | Value to set in the compare register. |
sl_hal_letimer_get_compare#
uint32_t sl_hal_letimer_get_compare (LETIMER_TypeDef * letimer, uint8_t channel)
Get the LETIMER compare register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| uint8_t | [in] | channel | A compare register to get, either 0 or 1. |
Returns
A compare register value, 0 if invalid register selected.
sl_hal_letimer_set_repeat#
void sl_hal_letimer_set_repeat (LETIMER_TypeDef * letimer, uint8_t channel, uint32_t value)
Set the LETIMER repeat register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint8_t | [in] | channel | A repeat register to set, either 0 or 1. |
| uint32_t | [in] | value | Value to set in the repeat register. |
sl_hal_letimer_get_repeat#
uint32_t sl_hal_letimer_get_repeat (LETIMER_TypeDef * letimer, uint8_t channel)
Get the LETIMER repeat register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| uint8_t | [in] | channel | A repeat register to get, either 0 or 1. |
Returns
A repeat register value, 0 if invalid register selected.
sl_hal_letimer_set_top#
void sl_hal_letimer_set_top (LETIMER_TypeDef * letimer, uint32_t value)
Set the LETIMER top register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | value | Value to set in top value register. |
The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value. The LETIMER needs to be configured with enable_top to use a top value.
sl_hal_letimer_get_top#
uint32_t sl_hal_letimer_get_top (LETIMER_TypeDef * letimer)
Get the LETIMER top register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Returns
Current top value.
sl_hal_letimer_set_top_buffer#
void sl_hal_letimer_set_top_buffer (LETIMER_TypeDef * letimer, uint32_t value)
Set the LETIMER top register value buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | value | Value to set in top value buffer register. |
When top value buffer register is updated, value is loaded into top value register the next time the counter reaches 0. This feature is useful to update top value safely when LETIMER is running. This won't happen if buffered_top is not configured to true and the mode is not SL_HAL_LETIMER_REPEAT_MODE_BUFFERED.
sl_hal_letimer_get_top_buffer#
uint32_t sl_hal_letimer_get_top_buffer (LETIMER_TypeDef * letimer)
Get the LETIMER top register value buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Returns
Current top value buffer.
Macro Definition Documentation#
SL_HAL_LETIMER_REF_VALID#
#define SL_HAL_LETIMER_REF_VALIDValue:
(letimer_ref)
Check if LETIMER module is valid.
SL_HAL_LETIMER_MAX_COUNT#
#define SL_HAL_LETIMER_MAX_COUNTValue:
(letimer_ref)
Return LETIMER module max count.
SL_HAL_LETIMER_INIT_DEFAULT#
#define SL_HAL_LETIMER_INIT_DEFAULTValue:
Default configuration for LETIMER initialization structure.