PDM - Pulse Density Modulation#

Pulse Density Modulation API.

Modules#

sl_hal_pdm_init_t

Enumerations#

enum
SL_HAL_PDM_CH_CLOCK_POLARITY_RISING_EDGE = _PDM_CFG0_CH0CLKPOL_NORMAL
SL_HAL_PDM_CH_CLOCK_POLARITY_FALLING_EDGE = _PDM_CFG0_CH0CLKPOL_INVERT
}

Configure channel clock polarity.

enum
SL_HAL_PDM_FIFO_VALID_WATERMARK_ONE = _PDM_CFG0_FIFODVL_ONE
SL_HAL_PDM_FIFO_VALID_WATERMARK_TWO = _PDM_CFG0_FIFODVL_TWO
SL_HAL_PDM_FIFO_VALID_WATERMARK_THREE = _PDM_CFG0_FIFODVL_THREE
SL_HAL_PDM_FIFO_VALID_WATERMARK_FOUR = _PDM_CFG0_FIFODVL_FOUR
}

Configure FIFO Data valid level water-mark.

enum
SL_HAL_PDM_DATA_FORMAT_RIGHT_16 = _PDM_CFG0_DATAFORMAT_RIGHT16
SL_HAL_PDM_DATA_FORMAT_DOUBLE_16 = _PDM_CFG0_DATAFORMAT_DOUBLE16
SL_HAL_PDM_DATA_FORMAT_RIGHT_24 = _PDM_CFG0_DATAFORMAT_RIGHT24
SL_HAL_PDM_DATA_FORMAT_FULL_32BIT = _PDM_CFG0_DATAFORMAT_FULL32BIT
SL_HAL_PDM_DATA_FORMAT_LEFT_16 = _PDM_CFG0_DATAFORMAT_LEFT16
SL_HAL_PDM_DATA_FORMAT_LEFT_24 = _PDM_CFG0_DATAFORMAT_LEFT24
SL_HAL_PDM_DATA_FORMAT_RAW_32BIT = _PDM_CFG0_DATAFORMAT_RAW32BIT
}

Configure PDM filter data output format.

enum
SL_HAL_PDM_NUMBER_OF_CHANNELS_ONE = _PDM_CFG0_NUMCH_ONE
SL_HAL_PDM_NUMBER_OF_CHANNELS_TWO = _PDM_CFG0_NUMCH_TWO
}

Configure number of PDM channels.

enum
SL_HAL_PDM_FILTER_ORDER_SECOND = _PDM_CFG0_FORDER_SECOND
SL_HAL_PDM_FILTER_ORDER_THIRD = _PDM_CFG0_FORDER_THIRD
SL_HAL_PDM_FILTER_ORDER_FOURTH = _PDM_CFG0_FORDER_FOURTH
SL_HAL_PDM_FILTER_ORDER_FIFTH = _PDM_CFG0_FORDER_FIFTH
}

Configure order of the PDM filter.

Variables#

bool

Enable stereo mode for channel pair CH0 and CH1.

PDM filter data output format.

uint32_t

PDM gain.

uint32_t

PDM down sampling rate.

uint32_t

PDM clock prescaler, resulting PDM clock is input clock / (prescaler + 1).

Functions#

void
sl_hal_pdm_init(PDM_TypeDef *pdm, const sl_hal_pdm_init_t *init)

Initialize the PDM peripheral.

void
sl_hal_pdm_deinit(PDM_TypeDef *pdm)

De-initialize the PDM peripheral.

void
sl_hal_pdm_reset(PDM_TypeDef *pdm)

Initialize PDM registers with reset values.

void
sl_hal_pdm_wait_sync(PDM_TypeDef *pdm)

Waits for the PDM to complete all synchronization of register changes and commands.

void
sl_hal_pdm_wait_ready(PDM_TypeDef *pdm)

Waits for the PDM to complete disabling procedure.

void
sl_hal_pdm_start(PDM_TypeDef *pdm)

Start the PDM operation (start the PDM filter).

void
sl_hal_pdm_stop(PDM_TypeDef *pdm)

Stop the PDM operation (stop the PDM filter).

void
sl_hal_pdm_enable(PDM_TypeDef *pdm)

Enable the PDM peripheral.

void
sl_hal_pdm_disable(PDM_TypeDef *pdm)

Disable the PDM peripheral.

void
sl_hal_pdm_clear(PDM_TypeDef *pdm)

Clear the PDM filter.

void
sl_hal_pdm_fifo_flush(PDM_TypeDef *pdm)

Flush the PDM sample FIFO.

uint32_t
sl_hal_pdm_rx(PDM_TypeDef *pdm)

Read one entry from the PDM FIFO.

uint32_t
sl_hal_pdm_get_status(PDM_TypeDef *pdm)

Get the PDM STATUS register.

void
sl_hal_pdm_clear_interrupts(PDM_TypeDef *pdm, uint32_t flags)

Clear one or more pending PDM interrupts.

void
sl_hal_pdm_set_interrupts(PDM_TypeDef *pdm, uint32_t flags)

Set one or more pending PDM interrupts.

void
sl_hal_pdm_enable_interrupts(PDM_TypeDef *pdm, uint32_t flags)

Enable one or more PDM interrupts.

void
sl_hal_pdm_disable_interrupts(PDM_TypeDef *pdm, uint32_t flags)

Disable one or more PDM interrupts.

uint32_t

Get pending PDM interrupt flags.

uint32_t

Get enabled and pending PDM interrupt flags.

Macros#

#define

Check if PDM instance is valid.

#define

Default PDM clock prescaler value, no prescaling.

#define

Default PDM down sampling rate, 32 times oversampling.

#define

Default PDM gain, 5 dB.

#define

Default configuration for PDM.

Enumeration Documentation#

sl_hal_pdm_ch_clock_polarity_t#

sl_hal_pdm_ch_clock_polarity_t

Configure channel clock polarity.

Enumerator
SL_HAL_PDM_CH_CLOCK_POLARITY_RISING_EDGE

Input data clocked on rising clock edge.

SL_HAL_PDM_CH_CLOCK_POLARITY_FALLING_EDGE

Input data clocked on falling clock edge.


sl_hal_pdm_fifo_valid_watermark_t#

sl_hal_pdm_fifo_valid_watermark_t

Configure FIFO Data valid level water-mark.

Enumerator
SL_HAL_PDM_FIFO_VALID_WATERMARK_ONE

At least one word.

SL_HAL_PDM_FIFO_VALID_WATERMARK_TWO

Two words.

SL_HAL_PDM_FIFO_VALID_WATERMARK_THREE

Three words.

SL_HAL_PDM_FIFO_VALID_WATERMARK_FOUR

Four words.


sl_hal_pdm_data_format_t#

sl_hal_pdm_data_format_t

Configure PDM filter data output format.

Enumerator
SL_HAL_PDM_DATA_FORMAT_RIGHT_16

Right aligned 16-bit, left bits are sign extended.

SL_HAL_PDM_DATA_FORMAT_DOUBLE_16

Pack two 16-bit samples into one 32-bit word.

SL_HAL_PDM_DATA_FORMAT_RIGHT_24

Right aligned 24bit, left bits are sign extended.

SL_HAL_PDM_DATA_FORMAT_FULL_32BIT

32 bit data.

SL_HAL_PDM_DATA_FORMAT_LEFT_16

Left aligned 16-bit, right bits are zeros.

SL_HAL_PDM_DATA_FORMAT_LEFT_24

Left aligned 24-bit, right bits are zeros.

SL_HAL_PDM_DATA_FORMAT_RAW_32BIT

RAW 32 bit data from integrator.


sl_hal_pdm_number_of_channels_t#

sl_hal_pdm_number_of_channels_t

Configure number of PDM channels.

Enumerator
SL_HAL_PDM_NUMBER_OF_CHANNELS_ONE

Only one Channel.

SL_HAL_PDM_NUMBER_OF_CHANNELS_TWO

Two Channels.


sl_hal_pdm_filter_order_t#

sl_hal_pdm_filter_order_t

Configure order of the PDM filter.

Enumerator
SL_HAL_PDM_FILTER_ORDER_SECOND

Second order filter.

SL_HAL_PDM_FILTER_ORDER_THIRD

Third order filter.

SL_HAL_PDM_FILTER_ORDER_FOURTH

Fourth order filter.

SL_HAL_PDM_FILTER_ORDER_FIFTH

Fifth order filter.


Variable Documentation#

ch0ch1_stereo_enable#

bool sl_hal_pdm_init_t::ch0ch1_stereo_enable

Enable stereo mode for channel pair CH0 and CH1.


filter_order#

sl_hal_pdm_filter_order_t sl_hal_pdm_init_t::filter_order

PDM filter order.


number_channels#

sl_hal_pdm_number_of_channels_t sl_hal_pdm_init_t::number_channels

Number of PDM channels.


data_format#

sl_hal_pdm_data_format_t sl_hal_pdm_init_t::data_format

PDM filter data output format.


fifo_valid_watermark#

sl_hal_pdm_fifo_valid_watermark_t sl_hal_pdm_init_t::fifo_valid_watermark

FIFO Data valid level water-mark.


ch0_clock_polarity#

sl_hal_pdm_ch_clock_polarity_t sl_hal_pdm_init_t::ch0_clock_polarity

Ch 0 clock polarity.


ch1_clock_polarity#

sl_hal_pdm_ch_clock_polarity_t sl_hal_pdm_init_t::ch1_clock_polarity

Ch 1 clock polarity.


gain#

uint32_t sl_hal_pdm_init_t::gain

PDM gain.


down_sampling_rate#

uint32_t sl_hal_pdm_init_t::down_sampling_rate

PDM down sampling rate.


clk_prescaler#

uint32_t sl_hal_pdm_init_t::clk_prescaler

PDM clock prescaler, resulting PDM clock is input clock / (prescaler + 1).


Function Documentation#

sl_hal_pdm_init#

void sl_hal_pdm_init (PDM_TypeDef * pdm, const sl_hal_pdm_init_t * init)

Initialize the PDM peripheral.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

const sl_hal_pdm_init_t *[in]init

A pointer to the initialization structure used to configure the PDM.

This function will configure basic settings in PDM according to values in the initialization data structure. Notice that enabling of PDM clock, setup of PDM pins and setup of PRS is not covered by this function.


sl_hal_pdm_deinit#

void sl_hal_pdm_deinit (PDM_TypeDef * pdm)

De-initialize the PDM peripheral.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

This function will stop the PDM filter and set PDM control registers to their reset values.


sl_hal_pdm_reset#

void sl_hal_pdm_reset (PDM_TypeDef * pdm)

Initialize PDM registers with reset values.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_wait_sync#

void sl_hal_pdm_wait_sync (PDM_TypeDef * pdm)

Waits for the PDM to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_wait_ready#

void sl_hal_pdm_wait_ready (PDM_TypeDef * pdm)

Waits for the PDM to complete disabling procedure.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

Note

  • This function is only needed if the PDM peripheral supports disabling bit in the EN register. If the PDM peripheral doesn't support, this function will do nothing.


sl_hal_pdm_start#

void sl_hal_pdm_start (PDM_TypeDef * pdm)

Start the PDM operation (start the PDM filter).

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_stop#

void sl_hal_pdm_stop (PDM_TypeDef * pdm)

Stop the PDM operation (stop the PDM filter).

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_enable#

void sl_hal_pdm_enable (PDM_TypeDef * pdm)

Enable the PDM peripheral.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_disable#

void sl_hal_pdm_disable (PDM_TypeDef * pdm)

Disable the PDM peripheral.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_clear#

void sl_hal_pdm_clear (PDM_TypeDef * pdm)

Clear the PDM filter.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_fifo_flush#

void sl_hal_pdm_fifo_flush (PDM_TypeDef * pdm)

Flush the PDM sample FIFO.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.


sl_hal_pdm_rx#

uint32_t sl_hal_pdm_rx (PDM_TypeDef * pdm)

Read one entry from the PDM FIFO.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

Returns

  • The entry read from the FIFO.

Note

  • This function will wait until a sample is available in the FIFO. Depending on PDM configuration, a FIFO entry can consist of one or two samples.


sl_hal_pdm_get_status#

uint32_t sl_hal_pdm_get_status (PDM_TypeDef * pdm)

Get the PDM STATUS register.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

Returns

  • STATUS register value.


sl_hal_pdm_clear_interrupts#

void sl_hal_pdm_clear_interrupts (PDM_TypeDef * pdm, uint32_t flags)

Clear one or more pending PDM interrupts.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

uint32_t[in]flags

Pending PDM interrupt sources to clear. Use one or more valid interrupt flags for the PDM module. The flags are PDM_IFC_DV, PDM_IFC_DVL, PDM_IFC_OF and PDM_IFC_UF.


sl_hal_pdm_set_interrupts#

void sl_hal_pdm_set_interrupts (PDM_TypeDef * pdm, uint32_t flags)

Set one or more pending PDM interrupts.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

uint32_t[in]flags

PDM interrupt sources to set to pending. Use one or more valid interrupt flags for the PDM module. The flags are PDM_IFS_DV, PDM_IFS_DVL, PDM_IFS_OF and PDM_IFS_UF.


sl_hal_pdm_enable_interrupts#

void sl_hal_pdm_enable_interrupts (PDM_TypeDef * pdm, uint32_t flags)

Enable one or more PDM interrupts.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

uint32_t[in]flags

PDM interrupt sources to enable. Use one or more valid interrupt flags for the PDM module. The flags are PDM_IEN_DV, PDM_IEN_DVL, PDM_IEN_OF and PDM_IEN_UF.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_pdm_clear_interrupts() prior to enabling the interrupt.


sl_hal_pdm_disable_interrupts#

void sl_hal_pdm_disable_interrupts (PDM_TypeDef * pdm, uint32_t flags)

Disable one or more PDM interrupts.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

uint32_t[in]flags

PDM interrupt sources to disable. Use one or more valid interrupt flags for the PDM module. The flags are PDM_IEN_DV, PDM_IEN_DVL, PDM_IEN_OF and PDM_IEN_UF.


sl_hal_pdm_get_pending_interrupts#

uint32_t sl_hal_pdm_get_pending_interrupts (PDM_TypeDef * pdm)

Get pending PDM interrupt flags.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

Returns

  • PDM interrupt sources pending. Returns one or more valid interrupt flags for PDM module. The flags are PDM_IF_DV, PDM_IF_DVL, PDM_IF_OF and PDM_IF_UF.

Note

  • Event bits are not cleared by the use of this function.


sl_hal_pdm_get_enabled_pending_interrupts#

uint32_t sl_hal_pdm_get_enabled_pending_interrupts (PDM_TypeDef * pdm)

Get enabled and pending PDM interrupt flags.

Parameters
TypeDirectionArgument NameDescription
PDM_TypeDef *[in]pdm

A pointer to the PDM peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled PDM interrupt sources Return value is the bitwise AND of

    • the enabled interrupt sources in PDM_IEN and

    • the pending interrupt flags PDM_IF

Note

  • Interrupt flags are not cleared by the use of this function.


Macro Definition Documentation#

SL_HAL_PDM_REF_VALID#

#define SL_HAL_PDM_REF_VALID
Value:
(pdm_ref)

Check if PDM instance is valid.


SL_HAL_PDM_CLOCK_PRESCALER#

#define SL_HAL_PDM_CLOCK_PRESCALER
Value:
0U

Default PDM clock prescaler value, no prescaling.


SL_HAL_PDM_DOWN_SAMPLING_RATE#

#define SL_HAL_PDM_DOWN_SAMPLING_RATE
Value:
32U

Default PDM down sampling rate, 32 times oversampling.


SL_HAL_PDM_GAIN#

#define SL_HAL_PDM_GAIN
Value:
5U

Default PDM gain, 5 dB.


SL_HAL_PDM_INIT_DEFAULT#

#define SL_HAL_PDM_INIT_DEFAULT
Value:
{ \
true, /* Enable stereo mode for channel pair CH0 and CH1. */ \
SL_HAL_PDM_FILTER_ORDER_FIFTH, /* Fifth order filter. */ \
SL_HAL_PDM_NUMBER_OF_CHANNELS_TWO, /* Two Channels. */ \
SL_HAL_PDM_DATA_FORMAT_DOUBLE_16, /* Two 16-bit samples per FIFO entry. */ \
SL_HAL_PDM_FIFO_VALID_WATERMARK_ONE, /* At least one word water-mark level. */ \
SL_HAL_PDM_CH_CLOCK_POLARITY_RISING_EDGE, /* Input data clocked on rising clock edge. */ \
SL_HAL_PDM_CH_CLOCK_POLARITY_FALLING_EDGE, /* Input data clocked on falling clock edge. */ \
SL_HAL_PDM_GAIN, /* PDM gain. */ \
SL_HAL_PDM_DOWN_SAMPLING_RATE, /* PDM down sampling rate. */ \
SL_HAL_PDM_CLOCK_PRESCALER /* No clock prescaling. */ \
}

Default configuration for PDM.

Stereo Ch0/1, 16bit samples, 44,100 Hz sampling rate, 32 times oversampling (requires 1,411,209 Hz PDM clock).