LESENSE - Low Energy Sensor Interface#

Low Energy Sensor Interface (LESENSE) Peripheral API.


This module contains functions to control the LESENSE peripheral of Silicon Labs 32-bit MCUs and SoCs. LESENSE is a low energy sensor interface which utilizes on-chip peripherals to perform measurement of a configurable set of sensors

Example#

This example demonstrates initialization, basic configuration, and usage of the LESENSE peripheral. It shows how to:

  • Initialize the LESENSE with default settings to sample a single channel. LESENSE uses ACMP to sample input state of a button 0 and will trigger an interrupt to toggle LED0.

#include "sl_hal_lesense.h"
#include "sl_hal_acmp.h"
#include "sl_hal_gpio.h"
#include "sl_clock_manager.h"

sl_gpio_t led0 = {LED0_PORT, LED0_PIN};
void init_gpio(void)
{
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);
  sl_hal_gpio_set_pin_mode(&led0, SL_GPIO_MODE_PUSH_PULL, 0);
}

void init_ACMP(void)
{
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_ACMP0);
  sl_hal_acmp_init_t amcp_init = SL_HAL_ACMP_INIT_DEFAULT;
  
  sl_hal_acmp_init(ACMP0, &amcp_init);
  if (BTN0_PIN % 2 == 0) {
     GPIO->BBUSALLOC_SET = GPIO_BBUSALLOC_BEVEN0_ACMP0;
  } else {
     GPIO->BBUSALLOC_SET = GPIO_BBUSALLOC_BODD0_ACMP0;
  }
  sl_hal_acmp_enable(ACMP0);
  // Set 1.25V internal as reference voltage for ACMP negative input and port B external interface override.
  sl_hal_acmp_set_input(ACMP0, SL_HAL_ACMP_INPUT_VREFDIV1V25, SL_HAL_ACMP_INPUT_EXTPB);
  // Wait for warm-up.
  while (!(ACMP0->STATUS & ACMP_IF_ACMPRDY));
}

void lesense_acmp_example(void)
{
  init_gpio();
  init_ACMP();
  // Initialize configuration structure with default settings
  sl_hal_lesense_init_t init = SL_HAL_LESENSE_INIT_DEFAULT;
  sl_hal_lesense_channel_descriptor_t lesense_channel = SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT;
  uint32_t reference_freq;

  // Enable clock.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LFRCO);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LESENSE);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_PRS);

  // Get the frequency of LFRCO for LESENSE reference.
  sl_clock_manager_get_oscillator_frequency(SL_OSCILLATOR_LFRCO, &reference_freq);

  // Do not store scan result and invert ACMP0 to accommodate PB0 pull-up.
  init.core_control.store_scanres = false;
  init.core_control.invert_acmp0 = true;
  // Enable LESENSE control of ACMP0 positive input mux.
  init.per_control.acmp0_mode = SL_HAL_LESENSE_ACMP_MODE_MUX;

  // Config lesense channel.
  lesense_channel.enable_scan = true;
  lesense_channel.enable_interrupt = true;
  lesense_channel.sample_mode = SL_HAL_LESENSE_SAMPLE_MODE_ACMP;
  lesense_channel.interrupt_mode = SL_HAL_LESENSE_SET_INTERRUPT_POSITIVE_EDGE;
  lesense_channel.offset = PB0_PIN; // push button pin number.

  // Initialize and enable LESENSE with default settings.
  sl_hal_lesense_init(&init);
  // Config channel 0.
  sl_hal_lesense_channel_config(&lesense_channel, 0);
  // Get 32 samples per second.
  sl_hal_lesense_disable();
  sl_hal_lesense_set_scan_frequency(reference_freq, 32);

  // Start LESENSE scanning.
  sl_hal_lesense_enable();
  sl_hal_lesense_start_scan();

  // Enable interrupt in NVIC.
  NVIC_ClearPendingIRQ(LESENSE_IRQn);
  NVIC_EnableIRQ(LESENSE_IRQn);
}

void LESENSE_IRQHandler(void)
{
  // Clear all LESENSE interrupt flag
  uint32_t flags = sl_hal_lesense_get_pending_interrupts();
  sl_hal_lesense_clear_interrupts(flags);
  // Toggle LED0.
  if (flags & LESENSE_IF_CH0) {
    sl_hal_gpio_toggle_pin(&led0);
  }
}

Modules#

sl_hal_lesense_core_descriptor_t

sl_hal_lesense_timing_descriptor_t

sl_hal_lesense_peripheral_descriptor_t

sl_hal_lesense_decoder_descriptor_t

sl_hal_lesense_init_t

sl_hal_lesense_channel_descriptor_t

sl_hal_lesense_channel_all_t

sl_hal_lesense_channel_alternate_excitation_t

sl_hal_lesense_transition_arc_t

sl_hal_lesense_all_transition_arcs_t

Enumerations#

enum
SL_HAL_LESENSE_CLOCK_DIV1 = 0
SL_HAL_LESENSE_CLOCK_DIV2 = 1
SL_HAL_LESENSE_CLOCK_DIV4 = 2
SL_HAL_LESENSE_CLOCK_DIV8 = 3
SL_HAL_LESENSE_CLOCK_DIV16 = 4
SL_HAL_LESENSE_CLOCK_DIV32 = 5
SL_HAL_LESENSE_CLOCK_DIV64 = 6
SL_HAL_LESENSE_CLOCK_DIV128 = 7
}

Clock divisors for controlling the prescaling factor of the period counter.

enum
SL_HAL_LESENSE_SCAN_START_PERIODIC = _LESENSE_CFG_SCANMODE_PERIODIC
SL_HAL_LESENSE_SCAN_START_ONESHOT = _LESENSE_CFG_SCANMODE_ONESHOT
SL_HAL_LESENSE_SCAN_START_PRS = _LESENSE_CFG_SCANMODE_PRS
}

Scan modes.

enum
SL_HAL_LESENSE_PRS_CHANNEL_0 = 0
SL_HAL_LESENSE_PRS_CHANNEL_1 = 1
SL_HAL_LESENSE_PRS_CHANNEL_2 = 2
SL_HAL_LESENSE_PRS_CHANNEL_3 = 3
SL_HAL_LESENSE_PRS_CHANNEL_4 = 4
SL_HAL_LESENSE_PRS_CHANNEL_5 = 5
SL_HAL_LESENSE_PRS_CHANNEL_6 = 6
SL_HAL_LESENSE_PRS_CHANNEL_7 = 7
SL_HAL_LESENSE_PRS_CHANNEL_8 = 8
SL_HAL_LESENSE_PRS_CHANNEL_9 = 9
SL_HAL_LESENSE_PRS_CHANNEL_10 = 10
SL_HAL_LESENSE_PRS_CHANNEL_11 = 11
}

PRS sources.

enum
SL_HAL_LESENSE_SCAN_CONFIG_DIRECTLY_MAP = _LESENSE_CFG_SCANCONF_DIRMAP
SL_HAL_LESENSE_SCAN_CONFIG_INV_MAP = _LESENSE_CFG_SCANCONF_INVMAP
SL_HAL_LESENSE_SCAN_CONFIG_TOGGLE = _LESENSE_CFG_SCANCONF_TOGGLE
SL_HAL_LESENSE_SCAN_CONFIG_DECODER_DEFINES = _LESENSE_CFG_SCANCONF_DECDEF
}

Scan configuration.

enum
SL_HAL_LESENSE_DAC_CH_DATA = _LESENSE_PERCTRL_DACCH0DATA_DACDATA
SL_HAL_LESENSE_DAC_THRES = _LESENSE_PERCTRL_DACCH0DATA_THRES
}

DAC CHx data control configuration.

enum
SL_HAL_LESENSE_ACMP_MODE_MUX = _LESENSE_PERCTRL_ACMP0MODE_MUX
SL_HAL_LESENSE_ACMP_MODE_MUXTHRES = _LESENSE_PERCTRL_ACMP0MODE_MUXTHRES
}

ACMPx control configuration.

enum
SL_HAL_LESENSE_SAMPLE_MODE_ACMP_COUNT = _LESENSE_CH_INTERACT_SAMPLE_ACMPCOUNT
SL_HAL_LESENSE_SAMPLE_MODE_ACMP = _LESENSE_CH_INTERACT_SAMPLE_ACMP
SL_HAL_LESENSE_SAMPLE_MODE_ADC = _LESENSE_CH_INTERACT_SAMPLE_ADC
SL_HAL_LESENSE_SAMPLE_MODE_ADC_DIFF = _LESENSE_CH_INTERACT_SAMPLE_ADCDIFF
}

Compare source selection for sensor sampling.

enum
SL_HAL_LESENSE_SET_INTERRUPT_NONE = _LESENSE_CH_INTERACT_SETIF_NONE
SL_HAL_LESENSE_SET_INTERRUPT_LEVEL = _LESENSE_CH_INTERACT_SETIF_LEVEL
SL_HAL_LESENSE_SET_INTERRUPT_POSITIVE_EDGE = _LESENSE_CH_INTERACT_SETIF_POSEDGE
SL_HAL_LESENSE_SET_INTERRUPT_NEGATIVE_EDGE = _LESENSE_CH_INTERACT_SETIF_NEGEDGE
SL_HAL_LESENSE_SET_INTERRUPT_BOTH_EDGE = _LESENSE_CH_INTERACT_SETIF_BOTHEDGES
}

Interrupt generation setup for CHx interrupt flag.

enum
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_DISABLE = _LESENSE_CH_INTERACT_EXMODE_DISABLE
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_HIGH = _LESENSE_CH_INTERACT_EXMODE_HIGH
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_LOW = _LESENSE_CH_INTERACT_EXMODE_LOW
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_DAC_OUTPUT = _LESENSE_CH_INTERACT_EXMODE_DACOUT
}

Channel pin mode for the excitation phase of the scan sequence.

enum
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_DISABLE = _LESENSE_IDLECONF_CHIDLE0_DISABLE
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_HIGH = _LESENSE_IDLECONF_CHIDLE0_HIGH
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_LOW = _LESENSE_IDLECONF_CHIDLE0_LOW
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_DAC = _LESENSE_IDLECONF_CHIDLE0_DAC
}

Channel pin mode for the idle phase of scan sequence.

enum
SL_HAL_LESENSE_EXCITATION_TIMING_LFACLK = _LESENSE_CH_INTERACT_EXCLK_LFACLK
SL_HAL_LESENSE_EXCITATION_TIMING_AUXHFRCO = _LESENSE_CH_INTERACT_EXCLK_AUXHFRCO
}

Clock used for excitation and sample delay timing.

enum
SL_HAL_LESENSE_COMPARE_MODE_LESS = _LESENSE_CH_EVALCFG_COMP_LESS
SL_HAL_LESENSE_COMPARE_MODE_GREATER_OR_EQUAL = _LESENSE_CH_EVALCFG_COMP_GE
}

Compare modes for counter comparison.

enum
SL_HAL_LESENSE_STORE_SAMPLE_DISABLE = _LESENSE_CH_EVALCFG_STRSAMPLE_DISABLE
SL_HAL_LESENSE_STORE_SAMPLE_DATA = _LESENSE_CH_EVALCFG_STRSAMPLE_DATA
SL_HAL_LESENSE_STORE_SAMPLE_DATA_SOURCE = _LESENSE_CH_EVALCFG_STRSAMPLE_DATASRC
}

Mode of Storing of Sensor Sample in Result Buffer.

enum
SL_HAL_LESENSE_EVALUATION_MODE_THRESHOLD = _LESENSE_CH_EVALCFG_MODE_THRES
SL_HAL_LESENSE_EVALUATION_MODE_SLIDING_WINDOW = _LESENSE_CH_EVALCFG_MODE_SLIDINGWIN
SL_HAL_LESENSE_EVALUATION_MODE_STEP_DETECTION = _LESENSE_CH_EVALCFG_MODE_STEPDET
}

Sensor evaluation modes.

enum
SL_HAL_LESENSE_TRANSITION_ACTION_NONE = _LESENSE_ST_ARC_PRSACT_NONE
SL_HAL_LESENSE_TRANSITION_ACTION_PRS0 = _LESENSE_ST_ARC_PRSACT_PRS0
SL_HAL_LESENSE_TRANSITION_ACTION_PRS1 = _LESENSE_ST_ARC_PRSACT_PRS1
SL_HAL_LESENSE_TRANSITION_ACTION_PRS01 = _LESENSE_ST_ARC_PRSACT_PRS01
SL_HAL_LESENSE_TRANSITION_ACTION_PRS2 = _LESENSE_ST_ARC_PRSACT_PRS2
SL_HAL_LESENSE_TRANSITION_ACTION_PRS02 = _LESENSE_ST_ARC_PRSACT_PRS02
SL_HAL_LESENSE_TRANSITION_ACTION_PRS12 = _LESENSE_ST_ARC_PRSACT_PRS12
SL_HAL_LESENSE_TRANSITION_ACTION_PRS012 = _LESENSE_ST_ARC_PRSACT_PRS012
SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_UP = _LESENSE_ST_ARC_PRSACT_UP
SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_DOWN = _LESENSE_ST_ARC_PRSACT_DOWN
SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_UP_PRS2 = _LESENSE_ST_ARC_PRSACT_UPANDPRS2
SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_DOWN_PRS2 = _LESENSE_ST_ARC_PRSACT_DOWNANDPRS2
}

Transition action modes.

Functions#

void
sl_hal_lesense_init(const sl_hal_lesense_init_t *init)

Initialize the LESENSE module.

uint32_t
sl_hal_lesense_set_scan_frequency(uint32_t reference_frequency, uint32_t scan_frequency)

Set the scan frequency for periodic scanning.

void
sl_hal_lesense_set_clock_division(sl_hal_lesense_excitation_clock_t clock, sl_hal_lesense_clock_prescale_t clock_divisor)

Set the clock division for LESENSE timers.

void
sl_hal_lesense_channel_config_all(const sl_hal_lesense_channel_all_t *config_all_channel)

Configure all (16) LESENSE sensor channels.

void
sl_hal_lesense_channel_config(const sl_hal_lesense_channel_descriptor_t *config_channel, uint32_t channel_index)

Configure a single LESENSE sensor channel.

void
sl_hal_lesense_channel_enable(uint8_t channel_index, bool enable_scan_channel, bool enable_pin)

Enable/disable LESENSE scan channel and the pin assigned to it.

void
sl_hal_lesense_channel_enable_mask(uint16_t channel_mask, uint16_t pin_mask)

Enable/disable LESENSE scan channel and the pin assigned to it.

void
sl_hal_lesense_channel_set_threshold(uint8_t channel_index, uint16_t acmp_threshold, uint16_t count_threshold)

Set LESENSE channel threshold parameters.

void
sl_hal_lesense_channel_config_sliding_window(uint8_t channel_index, uint32_t window_size, uint32_t init_value)

Configure a Sliding Window evaluation mode for a specific channel.

void
sl_hal_lesense_channel_config_step_detection(uint8_t channel_index, uint32_t step_size, uint32_t init_value)

Configure the step detection evaluation mode for a specific channel.

void
sl_hal_lesense_config_alternate_excitation(const sl_hal_lesense_channel_alternate_excitation_t *config_alternate_excitation)

Configure the LESENSE alternate excitation modes.

void
sl_hal_lesense_decoder_config_all_arcs(const sl_hal_lesense_all_transition_arcs_t *config_all_arcs)

Configure all LESENSE transition ARCs.

void

Enable the LESENSE module.

void

Wait for ongoing sync of register(s) to complete before writing to any other register.

void

Wait for disabling to finish.

void

Disable the LESENSE module.

void

Start the LESENSE decoder.

void

Stop LESENSE decoder.

void
sl_hal_lesense_set_scan_mode(sl_hal_lesense_scan_mode_t scan_mode)

Set scan mode of the LESENSE channels.

void

Start scanning sensors.

void

Stop scanning sensors.

void
sl_hal_lesense_set_start_delay(uint8_t start_delay)

Set the start delay of the sensor interaction on each channel.

void
sl_hal_lesense_set_window_size(uint32_t window_size)

Set the window size for all LESENSE channels.

void
sl_hal_lesense_set_step_size(uint32_t step_size)

Set the step size for all LESENSE channels.

void
sl_hal_lesense_decoder_config_arc(const sl_hal_lesense_transition_arc_t *config_arc, uint32_t arc_index)

Configure a single LESENSE transition ARC.

void
sl_hal_lesense_decoder_enable_prs_output(uint32_t decoder_mask, uint32_t decoder_compare)

Enable the PRS output from the LESENSE decoder.

void

Disable the PRS output from the LESENSE decoder.

uint32_t

Get the current status of LESENSE.

void
sl_hal_lesense_channel_set_timing(uint8_t channel_index, uint8_t excitation_time, uint8_t sample_delay, uint16_t measure_delay)

Set LESENSE channel timing parameters.

void

Wait until status of LESENSE is equal to what was requested.

uint32_t

Get the currently active channel index.

uint32_t

Get the latest scan comparison result (1 bit / channel).

uint32_t

Get the oldest unread data from the result buffer.

void

Clear the result buffer.

uint32_t

Get the current state of the LESENSE decoder.

uint32_t

Get the current state of the LESENSE sensor.

void

Reset the LESENSE module.

void

Clear one or more pending LESENSE interrupts.

void

Enable one or more LESENSE interrupts.

void

Disable one or more LESENSE interrupts.

void

Set one or more pending LESENSE interrupts from SW.

uint32_t

Get pending LESENSE interrupt flags.

uint32_t

Get enabled and pending LESENSE interrupt flags.

Macros#

#define
SL_HAL_LESENSE_NUM_ARCS (SLI_HAL_LESENSE_NUM_DECODER_STATES << 1)

Number of ARCs supported by current device. Number of ARCS is the number of states times 2.

#define

Number of LESENSE channels.

#define

Default value for the FIFO trigger level.

#define

Default configuration for sl_hal_lesense_core_descriptor_t structure.

#define
#define
#define
#define

Default configuration for sl_hal_lesense_init_t structure.

#define

Default configuration for the scan channel.

#define

Default configuration for all the sensor channels.

#define

Default configuration for all the alternate excitation channels.

#define

Default configuration for the decoder state condition.

#define

Default configuration for all decoder states.

Enumeration Documentation#

sl_hal_lesense_clock_prescale_t#

sl_hal_lesense_clock_prescale_t

Clock divisors for controlling the prescaling factor of the period counter.

Note

  • These enumeration values are used for different clock division related configuration parameters.

Enumerator
SL_HAL_LESENSE_CLOCK_DIV1

Divide clock by 1.

SL_HAL_LESENSE_CLOCK_DIV2

Divide clock by 2.

SL_HAL_LESENSE_CLOCK_DIV4

Divide clock by 4.

SL_HAL_LESENSE_CLOCK_DIV8

Divide clock by 8.

SL_HAL_LESENSE_CLOCK_DIV16

Divide clock by 16.

SL_HAL_LESENSE_CLOCK_DIV32

Divide clock by 32.

SL_HAL_LESENSE_CLOCK_DIV64

Divide clock by 64.

SL_HAL_LESENSE_CLOCK_DIV128

Divide clock by 128.


sl_hal_lesense_scan_mode_t#

sl_hal_lesense_scan_mode_t

Scan modes.

Enumerator
SL_HAL_LESENSE_SCAN_START_PERIODIC

New scan is started each time the period counter overflows.

SL_HAL_LESENSE_SCAN_START_ONESHOT

Single scan is performed when sl_hal_lesense_start_scan() is called.

SL_HAL_LESENSE_SCAN_START_PRS

New scan is triggered by pulse on PRS channel.


sl_hal_lesense_prs_source_t#

sl_hal_lesense_prs_source_t

PRS sources.

Note

  • These enumeration values are being used for different PRS related. configuration parameters.

Enumerator
SL_HAL_LESENSE_PRS_CHANNEL_0

PRS channel 0.

SL_HAL_LESENSE_PRS_CHANNEL_1

PRS channel 1.

SL_HAL_LESENSE_PRS_CHANNEL_2

PRS channel 2.

SL_HAL_LESENSE_PRS_CHANNEL_3

PRS channel 3.

SL_HAL_LESENSE_PRS_CHANNEL_4

PRS channel 4.

SL_HAL_LESENSE_PRS_CHANNEL_5

PRS channel 5.

SL_HAL_LESENSE_PRS_CHANNEL_6

PRS channel 6.

SL_HAL_LESENSE_PRS_CHANNEL_7

PRS channel 7.

SL_HAL_LESENSE_PRS_CHANNEL_8

PRS channel 8.

SL_HAL_LESENSE_PRS_CHANNEL_9

PRS channel 9.

SL_HAL_LESENSE_PRS_CHANNEL_10

PRS channel 10.

SL_HAL_LESENSE_PRS_CHANNEL_11

PRS channel 11.


sl_hal_lesense_scan_config_t#

sl_hal_lesense_scan_config_t

Scan configuration.

Enumerator
SL_HAL_LESENSE_SCAN_CONFIG_DIRECTLY_MAP

Channel configuration registers (CHx_CONF) used are directly mapped to the channel number.

SL_HAL_LESENSE_SCAN_CONFIG_INV_MAP

Channel configuration registers used are CHx+8_CONF for channels 0-7 and CHx-8_CONF for channels 8-15.

SL_HAL_LESENSE_SCAN_CONFIG_TOGGLE

Channel configuration registers used toggles between CHX_SCANCONF and CHX+8_SCANCONF when channel x triggers.

SL_HAL_LESENSE_SCAN_CONFIG_DECODER_DEFINES

Decoder state defines the channel configuration register (CHx_CONF) to be used.


sl_hal_lesense_control_dac_data_t#

sl_hal_lesense_control_dac_data_t

DAC CHx data control configuration.

Note

  • This value could be used for both DAC Ch0 and Ch1.

Enumerator
SL_HAL_LESENSE_DAC_CH_DATA

DAC channel x data is defined by the DAC_CH0DATA register.

SL_HAL_LESENSE_DAC_THRES

DAC channel x data is defined by the THRES in LESENSE_CHx_INTERACT.


sl_hal_lesense_control_acmp_t#

sl_hal_lesense_control_acmp_t

ACMPx control configuration.

Note

  • This value could be used for both ACMP0 and ACMP1.

Enumerator
SL_HAL_LESENSE_ACMP_MODE_MUX

ACMPx is controlled by LESENSE input mux.

SL_HAL_LESENSE_ACMP_MODE_MUXTHRES

ACMPx is controlled by LESENSE input mux and threshold value.


sl_hal_lesense_channel_sample_t#

sl_hal_lesense_channel_sample_t

Compare source selection for sensor sampling.

Enumerator
SL_HAL_LESENSE_SAMPLE_MODE_ACMP_COUNT

ACMP Counter output will be used in comparison.

SL_HAL_LESENSE_SAMPLE_MODE_ACMP

ACMP output will be used in comparison.

SL_HAL_LESENSE_SAMPLE_MODE_ADC

ADC output will be used in comparison.

SL_HAL_LESENSE_SAMPLE_MODE_ADC_DIFF

Differential ADC output will be used in comparison.


sl_hal_lesense_channel_interrupt_t#

sl_hal_lesense_channel_interrupt_t

Interrupt generation setup for CHx interrupt flag.

Enumerator
SL_HAL_LESENSE_SET_INTERRUPT_NONE

No interrupt is generated.

SL_HAL_LESENSE_SET_INTERRUPT_LEVEL

Set interrupt flag if the sensor triggers.

SL_HAL_LESENSE_SET_INTERRUPT_POSITIVE_EDGE

Set interrupt flag on positive edge of the sensor state.

SL_HAL_LESENSE_SET_INTERRUPT_NEGATIVE_EDGE

Set interrupt flag on negative edge of the sensor state.

SL_HAL_LESENSE_SET_INTERRUPT_BOTH_EDGE

Set interrupt flag on both edges of the sensor state.


sl_hal_lesense_pin_excitation_phase_t#

sl_hal_lesense_pin_excitation_phase_t

Channel pin mode for the excitation phase of the scan sequence.

Enumerator
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_DISABLE

Channel pin is disabled.

SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_HIGH

Channel pin is configured as push-pull, driven HIGH.

SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_LOW

Channel pin is configured as push-pull, driven LOW.

SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_DAC_OUTPUT

DAC output (only available on channel 0, 1, 2, 3, 12, 13, 14 and 15).


sl_hal_lesense_pin_idle_mode_t#

sl_hal_lesense_pin_idle_mode_t

Channel pin mode for the idle phase of scan sequence.

Note

  • This value could be used for all channels.

Enumerator
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_DISABLE

Channel pin is disabled in idle phase.

SL_HAL_LESENSE_CHANNEL_PIN_IDLE_HIGH

Channel pin is configured as push-pull, driven HIGH in idle phase.

SL_HAL_LESENSE_CHANNEL_PIN_IDLE_LOW

Channel pin is configured as push-pull, driven LOW in idle phase.

SL_HAL_LESENSE_CHANNEL_PIN_IDLE_DAC

Channel pin is connected to DAC output in idle phase.


sl_hal_lesense_excitation_clock_t#

sl_hal_lesense_excitation_clock_t

Clock used for excitation and sample delay timing.

Enumerator
SL_HAL_LESENSE_EXCITATION_TIMING_LFACLK

LFACLK (LF clock) is used.

SL_HAL_LESENSE_EXCITATION_TIMING_AUXHFRCO

AUXHFRCO (HF clock) is used.


sl_hal_lesense_compare_counter_t#

sl_hal_lesense_compare_counter_t

Compare modes for counter comparison.

Enumerator
SL_HAL_LESENSE_COMPARE_MODE_LESS

Evaluates to 1 if sensor data is less than counter threshold, or if ACMP output is 0.

SL_HAL_LESENSE_COMPARE_MODE_GREATER_OR_EQUAL

Evaluates to 1 if sensor data is greater than, or equal to counter threshold, or if the ACMP output is 1.


sl_hal_lesense_store_sample_data_t#

sl_hal_lesense_store_sample_data_t

Mode of Storing of Sensor Sample in Result Buffer.

Enumerator
SL_HAL_LESENSE_STORE_SAMPLE_DISABLE

Nothing will be stored in the result buffer.

SL_HAL_LESENSE_STORE_SAMPLE_DATA

The sensor sample data will be stored in the result buffer.

SL_HAL_LESENSE_STORE_SAMPLE_DATA_SOURCE

The data source (i.e. the channel) will be stored alongside the sensor sample data.


sl_hal_lesense_sensor_evaluation_t#

sl_hal_lesense_sensor_evaluation_t

Sensor evaluation modes.

Enumerator
SL_HAL_LESENSE_EVALUATION_MODE_THRESHOLD

Threshold comparison evaluation mode.

SL_HAL_LESENSE_EVALUATION_MODE_SLIDING_WINDOW

Sliding window evaluation mode.

SL_HAL_LESENSE_EVALUATION_MODE_STEP_DETECTION

Step detection evaluation mode.


sl_hal_lesense_transition_action_t#

sl_hal_lesense_transition_action_t

Transition action modes.

Enumerator
SL_HAL_LESENSE_TRANSITION_ACTION_NONE

No PRS pulses generated (if PRSCOUNT == 0). Do not count (if PRSCOUNT == 1).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS0

Generate pulse on LESPRS0 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS1

Generate pulse on LESPRS1 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS01

Generate pulse on LESPRS0 and LESPRS1 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS2

Generate pulse on LESPRS2 (for both PRSCOUNT == 0 and PRSCOUNT == 1).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS02

Generate pulse on LESPRS0 and LESPRS2 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS12

Generate pulse on LESPRS1 and LESPRS2 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_PRS012

Generate pulse on LESPRS0, LESPRS1, and LESPRS2 (if PRSCOUNT == 0).

SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_UP

Count up (if PRSCOUNT == 1).

SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_DOWN

Count down (if PRSCOUNT == 1).

SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_UP_PRS2

Count up and generate pulse on LESPRS2 (if PRSCOUNT == 1).

SL_HAL_LESENSE_TRANSITION_ACTION_COUNT_DOWN_PRS2

Count down and generate pulse on LESPRS2 (if PRSCOUNT == 1).


Function Documentation#

sl_hal_lesense_init#

void sl_hal_lesense_init (const sl_hal_lesense_init_t * init)

Initialize the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_init_t *[in]init

The LESENSE initialization structure.

This function configures the main parameters of the LESENSE interface. See the initialization parameter type definition (sl_hal_lesense_init_t) for more details.

Note

  • Function sl_hal_lesense_init() is designed to initialize LESENSE once in an operation cycle. Be aware of the effects of reconfiguration if using this function from multiple sources in your code. This function has not been designed to be re-entrant. Notice that GPIO pins used by the LESENSE module must be properly configured by the user explicitly for the LESENSE to work as intended. (When configuring pins, one should remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.) LESENSE needs to be disabled before configuring any register.


sl_hal_lesense_set_scan_frequency#

uint32_t sl_hal_lesense_set_scan_frequency (uint32_t reference_frequency, uint32_t scan_frequency)

Set the scan frequency for periodic scanning.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]reference_frequency

Select reference LFACLK clock frequency in Hz.

uint32_t[in]scan_frequency

Set the desired scan frequency in Hz.

This function only applies to LESENSE if a period counter is used as a trigger for scan start. The calculation is based on the following formula: Fscan = LFACLKles / ((1+PCTOP)*2^PCPRESC)

Note

  • Note that the calculation does not necessarily result in the requested scan frequency due to integer division. Check the return value for the resulted scan frequency. LESENSE needs to be disabled before configuring any register.

Returns

  • Frequency in Hz calculated and set by this function. Users can use this to compare the requested and set values.


sl_hal_lesense_set_clock_division#

void sl_hal_lesense_set_clock_division (sl_hal_lesense_excitation_clock_t clock, sl_hal_lesense_clock_prescale_t clock_divisor)

Set the clock division for LESENSE timers.

Parameters
TypeDirectionArgument NameDescription
sl_hal_lesense_excitation_clock_t[in]clock

Select the clock to prescale.

sl_hal_lesense_clock_prescale_t[in]clock_divisor

The clock divisor value. A valid range depends on the channel_id value.

Use this function to configure the clock division for the LESENSE timers used for excitation timing. The division setting is global but the clock source can be selected for each channel using sl_hal_lesense_channel_config() function. See documentation for more details.

Note

  • If AUXHFRCO is used for excitation timing, LFACLK can't exceed 500 kHz. LFACLK can't exceed 50 kHz if the ACMP threshold level (ACMPTHRES) is not equal for all channels. LESENSE needs to be disabled before configuring any register.

  • SL_HAL_LESENSE_EXCITATION_TIMING_AUXHFRCO - set AUXHFRCO clock divisor for HF timer.

  • SL_HAL_LESENSE_EXCITATION_TIMING_LFACLK - set LFACLKles clock divisor for LF timer.


sl_hal_lesense_channel_config_all#

void sl_hal_lesense_channel_config_all (const sl_hal_lesense_channel_all_t * config_all_channel)

Configure all (16) LESENSE sensor channels.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_channel_all_t *[in]config_all_channel

A configuration structure for all (16) LESENSE sensor channels.

This function configures all sensor channels of the LESENSE interface. See the configuration parameter type definition (sl_hal_lesense_channel_all_t) for more details.

Note

  • Channels can be configured individually using sl_hal_lesense_channel_config() function. Notice that pins used by the LESENSE module must be properly configured by the user explicitly for LESENSE to work as intended. (When configuring pins, consider the sequence of the configuration to avoid unintended pulses/glitches on output pins.)


sl_hal_lesense_channel_config#

void sl_hal_lesense_channel_config (const sl_hal_lesense_channel_descriptor_t * config_channel, uint32_t channel_index)

Configure a single LESENSE sensor channel.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_channel_descriptor_t *[in]config_channel

A configuration structure for a single LESENSE sensor channel.

uint32_t[in]channel_index

A channel index to configure (0-15).

This function configures a single sensor channel of the LESENSE interface. See the configuration parameter type definition (sl_hal_lesense_channel_descriptor_t) for more details.

Note

  • This function has been designed to minimize the effects of sensor channel reconfiguration while LESENSE is in operation. However, be aware of these effects and the right timing to call this function. Parameter pin_alternate_excite must be true in the channel configuration to use alternate excitation pins. LESENSE needs to be disabled before configuring any register.


sl_hal_lesense_channel_enable#

void sl_hal_lesense_channel_enable (uint8_t channel_index, bool enable_scan_channel, bool enable_pin)

Enable/disable LESENSE scan channel and the pin assigned to it.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_index

An identifier of the scan channel. A valid range: 0-15.

bool[in]enable_scan_channel

Enable/disable the selected scan channel by setting this parameter to true/false respectively.

bool[in]enable_pin

Enable/disable the pin assigned to the channel selected by channel_index.

Use this function to enable/disable a selected LESENSE scan channel and the pin assigned to it.

Note

  • Users can enable/disable scan channels and the channel pin with the sl_hal_lesense_channel_config() function, but only with a significant overhead. This simple function controls these parameters after the channel has been configured.


sl_hal_lesense_channel_enable_mask#

void sl_hal_lesense_channel_enable_mask (uint16_t channel_mask, uint16_t pin_mask)

Enable/disable LESENSE scan channel and the pin assigned to it.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]channel_mask

Set the corresponding bit to 1 to enable, 0 to disable the selected scan channel.

uint16_t[in]pin_mask

Set the corresponding bit to 1 to enable, 0 to disable the pin on selected channel.

Use this function to enable/disable LESENSE scan channels and the pins assigned to them using a mask.

Note

  • Users can enable/disable scan channels and channel pins by using the sl_hal_lesense_channel_config_all() function, but only with a significant overhead. This function controls these parameters after the channel has been configured.


sl_hal_lesense_channel_set_threshold#

void sl_hal_lesense_channel_set_threshold (uint8_t channel_index, uint16_t acmp_threshold, uint16_t count_threshold)

Set LESENSE channel threshold parameters.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_index

A decision threshold for counter comparison. A valid range is 0-65535 (16 bits).

uint16_t[in]acmp_threshold

ACMP threshold.

uint16_tN/Acount_threshold

Use this function to set threshold parameters on a selected LESENSE channel.

Note

  • Users can configure the channel threshold parameters with the sl_hal_lesense_channel_config() function, but only with a significant overhead. This function serves controls these parameters after the channel has been configured. LESENSE needs to be disabled before configuring INTERACT register and needs to be enabled when configuring EVALTHRES register.

  • If per_control.dac_channel0_data is set to SL_HAL_LESENSE_DAC_CH_DATA, acmp_threshold defines the 12-bit DAC data in the corresponding data register of the DAC interface (DACn_CH0DATA and DACn_CH1DATA). In this case, the valid range is 0-4095 (12 bits).


sl_hal_lesense_channel_config_sliding_window#

void sl_hal_lesense_channel_config_sliding_window (uint8_t channel_index, uint32_t window_size, uint32_t init_value)

Configure a Sliding Window evaluation mode for a specific channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_index

An identifier of the scan channel. A valid range is 0-15.

uint32_t[in]window_size

A window size to be used on all channels.

uint32_t[in]init_value

The initial sensor value for the channel.

This function will configure the evaluation mode, the initial sensor measurement (COMPTHRES), and the window size. For other channel-related configuration, see the sl_hal_lesense_channel_config() function.

Note

  • LESENSE needs to be disabled before configuring EVALCFG register and needs to be enabled when configuring EVALTHRES register.

Warnings

  • Note that the step size and window size configuration are global to all LESENSE channels and use the same register field in the hardware. This means that any window_size configuration passed to this function will apply for all channels and override all other step_size/window_size configurations.


sl_hal_lesense_channel_config_step_detection#

void sl_hal_lesense_channel_config_step_detection (uint8_t channel_index, uint32_t step_size, uint32_t init_value)

Configure the step detection evaluation mode for a specific channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_index

An identifier of the scan channel. A valid range is 0-15.

uint32_t[in]step_size

A step size to be used on all channels.

uint32_t[in]init_value

The initial sensor value for the channel.

This function will configure the evaluation mode, the initial sensor measurement (COMPTHRES) and the window size. For other channel-related configuration, see the sl_hal_lesense_channel_config() function.

Warnings

  • Note that the step size and window size configuration are global to all LESENSE channels and use the same register field in the hardware. This means that any step_size configuration passed to this function will apply for all channels and override all other step_size/window_size configurations. LESENSE needs to be disabled before configuring EVALCFG register and needs to be enabled when configuring EVALTHRES register.


sl_hal_lesense_config_alternate_excitation#

void sl_hal_lesense_config_alternate_excitation (const sl_hal_lesense_channel_alternate_excitation_t * config_alternate_excitation)

Configure the LESENSE alternate excitation modes.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_channel_alternate_excitation_t *[in]config_alternate_excitation

A configuration structure for LESENSE alternate excitation pins.

This function enable/disable the alternate excitation channels of the LESENSE interface. See the configuration parameter type definition (sl_hal_lesense_channel_alternate_excitation_t) for more details.

Note

  • The config_alternate_excitation parameter must be true in the channel configuration structure (sl_hal_lesense_channel_descriptor_t) to use alternate excitation pins on the channel.


sl_hal_lesense_decoder_config_all_arcs#

void sl_hal_lesense_decoder_config_all_arcs (const sl_hal_lesense_all_transition_arcs_t * config_all_arcs)

Configure all LESENSE transition ARCs.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_all_transition_arcs_t *[in]config_all_arcs

A configuration structure for all 64 LESENSE decoder arcs.

This function configures all the transition ARC of the LESENSE interface. See the configuration parameter type definition (sl_hal_lesense_all_transition_arcs_t) for more details.


sl_hal_lesense_enable#

void sl_hal_lesense_enable (void )

Enable the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_lesense_wait_sync#

void sl_hal_lesense_wait_sync (void )

Wait for ongoing sync of register(s) to complete before writing to any other register.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_lesense_wait_ready#

void sl_hal_lesense_wait_ready (void )

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_lesense_disable#

void sl_hal_lesense_disable (void )

Disable the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_lesense_decoder_start#

void sl_hal_lesense_decoder_start (void )

Start the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


sl_hal_lesense_decoder_stop#

void sl_hal_lesense_decoder_stop (void )

Stop LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Disables LESENSE decoder by setting the command to LESENSE_DECCTRL register.


sl_hal_lesense_set_scan_mode#

void sl_hal_lesense_set_scan_mode (sl_hal_lesense_scan_mode_t scan_mode)

Set scan mode of the LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
sl_hal_lesense_scan_mode_t[in]scan_mode

Select the location to map LESENSE alternate excitation channels.

This function configures how the scan start is triggered. It can be used for re-configuring the scan mode while running the application but it is also used by sl_hal_lesense_init() for initialization.

Note

  • Users can configure the scan mode by sl_hal_lesense_init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Be aware of the effects of the non-atomic Read-Modify-Write cycle. LESENSE needs to be disabled before configuring any register.

  • SL_HAL_LESENSE_SCAN_START_PERIODIC - A new scan is started each time the period counter overflows.

  • SL_HAL_LESENSE_SCAN_START_ONESHOT - A single scan is performed when sl_hal_lesense_start_scan() function is called.

  • SL_HAL_LESENSE_SCAN_START_PRS - A new scan is triggered by pulse on the PRS channel.


sl_hal_lesense_start_scan#

void sl_hal_lesense_start_scan (void )

Start scanning sensors.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


sl_hal_lesense_stop_scan#

void sl_hal_lesense_stop_scan (void )

Stop scanning sensors.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application. If issued during a scan, the command takes effect after scan completion.


sl_hal_lesense_set_start_delay#

void sl_hal_lesense_set_start_delay (uint8_t start_delay)

Set the start delay of the sensor interaction on each channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]start_delay

A number of LFACLK cycles to delay. A valid range: 0-3 (2 bit).

This function sets the start delay of the sensor interaction on each channel. It can be used for adjusting the start delay while running the application but it is also used by sl_hal_lesense_init() for initialization.

Note

  • Users can configure the start delay by sl_hal_lesense_init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Be aware of the effects of the non-atomic Read-Modify-Write cycle. LESENSE needs to be disabled before configuring any register.


sl_hal_lesense_set_window_size#

void sl_hal_lesense_set_window_size (uint32_t window_size)

Set the window size for all LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]window_size

The window size to use for all channels.

The window size is used by all channels that are configured as SL_HAL_LESENSE_EVALUATION_MODE_SLIDING_WINDOW.

Note

  • LESENSE needs to be disabled before configuring EVALCTRL register.

Warnings

  • The window size configuration is using the same register field as the step detection size. As a result, the window size configuration will have an effect on channels configured with the SL_HAL_LESENSE_EVALUATION_MODE_STEP_DETECTION evaluation mode as well.


sl_hal_lesense_set_step_size#

void sl_hal_lesense_set_step_size (uint32_t step_size)

Set the step size for all LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]step_size

The step size to use for all channels.

The step size is configured using the same register field as used to configure window size. Therefore, calling this function will overwrite any previously configured window size as done by the sl_hal_lesense_set_window_size() function.


sl_hal_lesense_decoder_config_arc#

void sl_hal_lesense_decoder_config_arc (const sl_hal_lesense_transition_arc_t * config_arc, uint32_t arc_index)

Configure a single LESENSE transition ARC.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_lesense_transition_arc_t *[in]config_arc

A configuration structure for a single LESENSE transition ARC.

uint32_t[in]arc_index

An ARC index to configure.

This function configures a transition ARC of the LESENSE interface. See the configuration parameter type definition sl_hal_lesense_transition_arc_t for more details.

Note

  • LESENSE needs to be disabled before configuring STx_ARC register.


sl_hal_lesense_decoder_enable_prs_output#

void sl_hal_lesense_decoder_enable_prs_output (uint32_t decoder_mask, uint32_t decoder_compare)

Enable the PRS output from the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]decoder_mask

A decoder state compare value mask.

uint32_t[in]decoder_compare

A decoder state comparison value.


sl_hal_lesense_decoder_disable_prs_output#

void sl_hal_lesense_decoder_disable_prs_output (void )

Disable the PRS output from the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_lesense_get_status#

uint32_t sl_hal_lesense_get_status (void )

Get the current status of LESENSE.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_STATUS register that contains the OR combination of the following status bits for EFR series 2:

    • LESENSE_STATUS_RESFIFOV - Result Fifo valid. Set when data is available in result Fifo. Cleared when Fifo is empty.

    • LESENSE_STATUS_RESFIFOFULL - Result Fifo full. Set when result Fifo is full.

    • LESENSE_STATUS_RUNNING - LESENSE is active.

    • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

    • LESENSE_STATUS_FLUSHING - Fifo flushing

    • LESENSE_STATUS_READBUSY - Fifo Read busy


sl_hal_lesense_channel_set_timing#

void sl_hal_lesense_channel_set_timing (uint8_t channel_index, uint8_t excitation_time, uint8_t sample_delay, uint16_t measure_delay)

Set LESENSE channel timing parameters.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_index

An identifier of the scan channel. A valid range is 0-15.

uint8_t[in]excitation_time

An excitation time on channel_index. The excitation will last excitation_time+1 excitation clock cycles. A valid range is 0-63 (6 bits).

uint8_t[in]sample_delay

Sample delay on channel_index. Sampling will occur after sample_delay+1 sample clock cycles. A valid range is 0-127 (7 bits).

uint16_t[in]measure_delay

A measure delay on channel_index. Sensor measuring is delayed for measure_delay+1 excitation clock cycles. A valid range is 0-127 (7 bits).

Use this function to set timing parameters on a selected LESENSE channel.

Note

  • Users can configure the channel timing parameters with the sl_hal_lesense_channel_config() function, but only with a significant overhead. This function controls these parameters after the channel has been configured. LESENSE needs to be disabled before configuring any register.


sl_hal_lesense_wait_status#

void sl_hal_lesense_wait_status (uint32_t flag)

Wait until status of LESENSE is equal to what was requested.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flag

The OR combination of the following status bits for EFR series 2:

  • LESENSE_STATUS_RESFIFOV - Result FIFO valid. Set when data is available in result FIFO. Cleared when FIFO is empty.

  • LESENSE_STATUS_RESFIFOFULL - Result FIFO full. Set when result FIFO is full.

  • LESENSE_STATUS_RUNNING - LESENSE is active.

  • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

  • LESENSE_STATUS_FLUSHING - FIFO flushing

  • LESENSE_STATUS_READBUSY - FIFO Read busy

Polls LESENSE_STATUS register and waits until requested combination of flags are set.


sl_hal_lesense_channel_get_active#

uint32_t sl_hal_lesense_channel_get_active (void )

Get the currently active channel index.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_CHINDEX register that contains the index of currently active channel (0-15).


sl_hal_lesense_get_scan_result#

uint32_t sl_hal_lesense_get_scan_result (void )

Get the latest scan comparison result (1 bit / channel).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_SCANRES register that contains the comparison result of last scan on all channels. Bit x is set if a comparison triggered on channel x, which means that LESENSE counter met the comparison criteria set in LESENSE_CHx_EVAL by COMPMODE and CNTTHRES.


sl_hal_lesense_get_scan_result_data#

uint32_t sl_hal_lesense_get_scan_result_data (void )

Get the oldest unread data from the result buffer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Make sure that the STORERES bit is set in LESENSE_CHx_EVAL, or the STRSCANRES bit is set in LESENSE_CTRL; otherwise, returns the undefined value.

Returns

  • Returns the value of LESENSE_RESDATA register that contains the oldest unread counter result from result buffer.


sl_hal_lesense_clear_result_buffer#

void sl_hal_lesense_clear_result_buffer (void )

Clear the result buffer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


sl_hal_lesense_decoder_get_state#

uint32_t sl_hal_lesense_decoder_get_state (void )

Get the current state of the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • This function returns the value of the LESENSE_DECSTATE register that represents the current state of the LESENSE decoder.


sl_hal_lesense_get_sensor_state#

uint32_t sl_hal_lesense_get_sensor_state (void )

Get the current state of the LESENSE sensor.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of LESENSE_SENSORSTATE register that represents the current state of the LESENSE sensor.


sl_hal_lesense_reset#

void sl_hal_lesense_reset (void )

Reset the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to reset LESENSE registers.

Note

  • Resetting LESENSE registers is required in each reset or power-on cycle to configure the default values of the RAM mapped LESENSE registers. sl_hal_lesense_reset() can be called on initialization by setting the req_reset parameter to true in sl_hal_lesense_init(). Starting from Series 2 Config 3 (xG23 and higher), this function leaves LESENSE in the disabled state.


sl_hal_lesense_clear_interrupts#

void sl_hal_lesense_clear_interrupts (uint32_t flags)

Clear one or more pending LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Pending LESENSE interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


sl_hal_lesense_enable_interrupts#

void sl_hal_lesense_enable_interrupts (uint32_t flags)

Enable one or more LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to enable. Use a set of interrupt flags OR-ed together to enable multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


sl_hal_lesense_disable_interrupts#

void sl_hal_lesense_disable_interrupts (uint32_t flags)

Disable one or more LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


sl_hal_lesense_set_interrupts#

void sl_hal_lesense_set_interrupts (uint32_t flags)

Set one or more pending LESENSE interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources of LESENSE module (LESENSE_IFS_nnn).


sl_hal_lesense_get_pending_interrupts#

uint32_t sl_hal_lesense_get_pending_interrupts (void )

Get pending LESENSE interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Event bits are not cleared by the use of this function.

Returns

  • Pending LESENSE interrupt sources. The OR combination of valid interrupt flags of the LESENSE module (LESENSE_IF_nnn).


sl_hal_lesense_get_enabled_pending_interrupts#

uint32_t sl_hal_lesense_get_enabled_pending_interrupts (void )

Get enabled and pending LESENSE interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Event bits are not cleared by the use of this function.

Returns

  • Pending and enabled LESENSE interrupt sources. Return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in LESENSE_IEN_nnn register (LESENSE_IEN_nnn).

    • the OR combination of valid interrupt flags of LESENSE module (LESENSE_IF_nnn).


Macro Definition Documentation#

SL_HAL_LESENSE_NUM_ARCS#

#define SL_HAL_LESENSE_NUM_ARCS
Value:
(SLI_HAL_LESENSE_NUM_DECODER_STATES << 1)

Number of ARCs supported by current device. Number of ARCS is the number of states times 2.


SL_HAL_LESENSE_NUM_CHANNELS#

#define SL_HAL_LESENSE_NUM_CHANNELS
Value:
16

Number of LESENSE channels.


SL_HAL_LESENSE_DEFAULT_TRIGGER_LEVEL#

#define SL_HAL_LESENSE_DEFAULT_TRIGGER_LEVEL
Value:
15

Default value for the FIFO trigger level.


SL_HAL_LESENSE_CORE_DESCRIPTOR_DEFAULT#

#define SL_HAL_LESENSE_CORE_DESCRIPTOR_DEFAULT
Value:
{ \
SL_HAL_LESENSE_SCAN_START_PERIODIC, /* Start new scan each time the period counter overflows. */ \
SL_HAL_LESENSE_PRS_CHANNEL_0, /* Default PRS channel is selected. */ \
SL_HAL_LESENSE_SCAN_CONFIG_DIRECTLY_MAP, /* Direct mapping SCANCONF register usage strategy. */ \
false, /* Do not invert ACMP0 output. */ \
false, /* Do not invert ACMP1 output. */ \
false, /* Disable dual sampling. */ \
true, /* Store scan result after each scan. */ \
SL_HAL_LESENSE_DEFAULT_TRIGGER_LEVEL, /* Default value for the FIFO trigger level */ \
false, /* Do not wake up on DMA from EM2. */ \
true /* Keep LESENSE running in debug mode. */ \
}

Default configuration for sl_hal_lesense_core_descriptor_t structure.


SL_HAL_LESENSE_PERIPHERAL_DESCRIPTOR_DEFAULT#

#define SL_HAL_LESENSE_PERIPHERAL_DESCRIPTOR_DEFAULT
Value:
{ \
SL_HAL_LESENSE_DAC_CH_DATA, /* DAC channel 0 data is defined by DAC_CH0DATA register. */ \
SL_HAL_LESENSE_ACMP_MODE_MUXTHRES, /* LESENSE controls input mux and threshold value of ACMP0. */ \
SL_HAL_LESENSE_ACMP_MODE_MUXTHRES, /* LESENSE controls input mux and threshold value of ACMP1. */ \
false, /* DAC is enabled for before every channel measurement. */ \
false /* DAC is enabled a full clock cycle before sensor interaction. */ \
}

Default configuration for sl_hal_lesense_peripheral_descriptor_t structure.


SL_HAL_LESENSE_TIMING_DESCRIPTOR_DEFAULT#

#define SL_HAL_LESENSE_TIMING_DESCRIPTOR_DEFAULT
Value:
{ \
0U, /* No sensor interaction delay. */ \
false /* Do not delay the AUXHFRCO startup. */ \
}

Default configuration for sl_hal_lesense_timing_descriptor_t structure.


SL_HAL_LESENSE_DECODER_DESCRIPTOR_DEFAULT#

#define SL_HAL_LESENSE_DECODER_DESCRIPTOR_DEFAULT
Value:
{ \
false, /* Disable check of current state. */ \
true, /* Enable channel x % 16 interrupt on state x change. */ \
true, /* Enable decoder hysteresis on PRS0 output. */ \
true, /* Enable decoder hysteresis on PRS1 output. */ \
true, /* Enable decoder hysteresis on PRS2 output. */ \
true, /* Enable decoder hysteresis on interrupt requests. */ \
false /* Disable count mode on decoder PRS channels 0 and 1.*/ \
}

Default configuration for sl_hal_lesense_decoder_descriptor_t structure.


SL_HAL_LESENSE_INIT_DEFAULT#

#define SL_HAL_LESENSE_INIT_DEFAULT
Value:
{ \
SL_HAL_LESENSE_CORE_DESCRIPTOR_DEFAULT, /* Default core control parameters. */ \
SL_HAL_LESENSE_TIMING_DESCRIPTOR_DEFAULT, /* Default time control parameters. */ \
SL_HAL_LESENSE_PERIPHERAL_DESCRIPTOR_DEFAULT, /* Default peripheral control parameters. */ \
SL_HAL_LESENSE_DECODER_DESCRIPTOR_DEFAULT /* Default decoder control parameters. */ \
}

Default configuration for sl_hal_lesense_init_t structure.


SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT#

#define SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT
Value:
{ \
false, /* Disable scan channel. */ \
false, /* Disable assigned pin on scan channel. */ \
false, /* Disable interrupts on channel. */ \
SL_HAL_LESENSE_CHANNEL_PIN_EXCITATION_DISABLE, /* Channel pin is disabled during excitation period. */ \
SL_HAL_LESENSE_CHANNEL_PIN_IDLE_DISABLE, /* Channel pin is disabled during idle period. */ \
false, /* Do not use alternate excitation pins for excitation. */ \
false, /* Disabled to shift results from this channel to decoder register.*/ \
false, /* Disabled to invert scan result bit. */ \
SL_HAL_LESENSE_STORE_SAMPLE_DISABLE, /* Disabled to store counter value in result buffer. */ \
SL_HAL_LESENSE_EXCITATION_TIMING_LFACLK, /* Use LF clock for excitation timing. */ \
SL_HAL_LESENSE_EXCITATION_TIMING_LFACLK, /* Use LF clock for sample timing. */ \
0x00U, /* Excitation time is set to 0(+1) excitation clock cycles. */ \
0x00U, /* Sample delay is set to 0(+1) sample clock cycles. */ \
0x00U, /* Measure delay is set to 0 excitation clock cycles.*/ \
0x00U, /* ACMP threshold has been set to 0. */ \
SL_HAL_LESENSE_SAMPLE_MODE_ACMP, /* ACMP output will be used in comparison. */ \
SL_HAL_LESENSE_SET_INTERRUPT_NONE, /* No interrupt is generated by the channel. */ \
0x00U, /* Counter threshold has been set to 0x00. */ \
SL_HAL_LESENSE_COMPARE_MODE_LESS, /* Compare mode has been set to trigger interrupt on "less". */ \
SL_HAL_LESENSE_EVALUATION_MODE_THRESHOLD, /* Evaluation mode has been set to trigger interrupt on threshold. */ \
0x00U /* No offset for IADC or ACMP interaction. */ \
}

Default configuration for the scan channel.


SL_HAL_LESENSE_SCAN_CONFIG_DEFAULT#

#define SL_HAL_LESENSE_SCAN_CONFIG_DEFAULT
Value:
{ \
{ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 0. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 1. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 2. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 3. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 4. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 5. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 6. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 7. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 8. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 9. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 10. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 11. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 12. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 13. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 14. */ \
SL_HAL_LESENSE_CHANNEL_CONFIG_DEFAULT, /* Scan channel 15. */ \
} \
}

Default configuration for all the sensor channels.


SL_HAL_LESENSE_ALTERNATE_EXCITATION_CONFIG_DEFAULT#

#define SL_HAL_LESENSE_ALTERNATE_EXCITATION_CONFIG_DEFAULT
Value:
{ \
{ \
false, /* Alternate excitation channel 0 disabled. */ \
false, /* Alternate excitation channel 1 disabled. */ \
false, /* Alternate excitation channel 2 disabled. */ \
false, /* Alternate excitation channel 3 disabled. */ \
false, /* Alternate excitation channel 4 disabled. */ \
false, /* Alternate excitation channel 5 disabled. */ \
false, /* Alternate excitation channel 6 disabled. */ \
false, /* Alternate excitation channel 7 disabled. */ \
false, /* Alternate excitation channel 8 disabled. */ \
false, /* Alternate excitation channel 9 disabled. */ \
false, /* Alternate excitation channel 10 disabled. */ \
false, /* Alternate excitation channel 11 disabled. */ \
false, /* Alternate excitation channel 12 disabled. */ \
false, /* Alternate excitation channel 13 disabled. */ \
false, /* Alternate excitation channel 14 disabled. */ \
false /* Alternate excitation channel 15 disabled. */ \
} \
}

Default configuration for all the alternate excitation channels.


SL_HAL_LESENSE_STATE_CONFIG_DEFAULT#

#define SL_HAL_LESENSE_STATE_CONFIG_DEFAULT
Value:
{ \
0x0FU, /* Compare value set to 0x0F. */ \
0x00U, /* All decoder inputs masked. */ \
0U, /* Current state must be state 0. */ \
0U, /* Next state is state 0. */ \
SL_HAL_LESENSE_TRANSITION_ACTION_NONE, /* No PRS action performed on compare match. */ \
false /* No interrupt triggered on compare match. */ \
}

Default configuration for the decoder state condition.


SL_HAL_LESENSE_DECODER_CONFIG_DEFAULT#

#define SL_HAL_LESENSE_DECODER_CONFIG_DEFAULT

Default configuration for all decoder states.