DCDC Initialization#
Initialize the DC-DC converter.
Configures the DC-DC converter. If the DC-DC converter is not to be used, the configuration option SL_DEVICE_INIT_DCDC_ENABLE can be disabled, and the converter will be powered off. On Series 1 devices, this option should only be used when DVDD is externally powered.
To enable the bypass switch and short the DC-DC converter input to the DC-DC output, set the configuration option SL_DEVICE_INIT_DCDC_BYPASS.
See AN0948 Power Configurations and DC-DC for further details about DC-DC converter configuration and operation.
Functions#
sl_status_t
sl_device_init_dcdc(void)
Initialize DCDC.
Macros#
#define
SL_DEVICE_INIT_DCDC_TYPE_BUCK 0
DC/DC Converter Type.
#define
SL_DEVICE_INIT_DCDC_TYPE_BOOST 1
Boost Type.
Function Documentation#
sl_device_init_dcdc#
sl_status_t sl_device_init_dcdc (void )
Initialize DCDC.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Configure and start the DCDC
Returns
Status code
Return values
SL_STATUS_OK: DC-DC converter initialized successfully