I/O Stream#

I/O Stream can be used to read/write different formats of data to various streams.

The source files for I/O Stream platform software module are present under platform/services/iostream.

Overview#

I/O Stream is a platform module software that provides Input/Output functionalities by creating streams. Streams are abstractions allowing a uniform way to read/write data regardless of the physical communication interface.

I/O Stream offers many interfaces, see submodules for a list of all types available and their specificities.You can load multiple streams in the project and you can select the interface that must be used at runtime.Some interface type can also be instantiated, meaning that you can have multiple instances of an interface type which will be normally bound to a hardware peripheral.

Initialization#

The I/O Stream core doesn't require any initialization. Instead each stream type has their own initialization and their own configuration. See I/O Stream specific type to know more about how to initialize a stream.

Note that most stream will set itself as the default stream during their initialization. Thus the initial default stream will be the last stream initialized.

Default system-wide stream#

Multiple streams can be initialized in your application and you can configure a default stream that must be used when no stream is specified. Also note that the default stream will be used when calling printf and you can change the default stream at runtime. The following defines should be used for the default stream:

SL_IOSTREAM_STDIN SL_IOSTREAM_STDOUT SL_IOSTREAM_STDERR

RTOS - Task's default stream#

In the case of an RTOS environment, each task can set its own stream. By default, the task stream will be set to the system_wide default stream. From your task, you can change the default stream assigned to your task without affecting the other tasks' stream.

Printf#

I/O Stream provides third-party printf integrations. It can work with toolchain implementation or with the tiny printf implementation for embedded system. The printf API doesn't have an argument for specifying the stream to be used, so I/O Stream provides a printf API that takes a stream as an argument and calls the configured third-party implementation of printf.

Modules#

sl_iostream_t

sl_iostream_instance_info_t

I/O Stream EUSART

I/O Stream RTT

I/O Stream STDLIB Configuration

I/O Stream SWO

I/O Stream UART

I/O Stream VUART

Enumerations#

enum
SL_IOSTREAM_TYPE_SWO = 0
SL_IOSTREAM_TYPE_RTT = 1
SL_IOSTREAM_TYPE_UART = 2
SL_IOSTREAM_TYPE_VUART = 3
SL_IOSTREAM_TYPE_DEBUG_OUTPUT = 4
SL_IOSTREAM_TYPE_LOOPBACK = 5
SL_IOSTREAM_TYPE_UNDEFINED = 6
}

Enumeration representing the possible types of iostream instances.

Functions#

sl_status_t
sl_iostream_set_default(sl_iostream_t *stream)

Set the stream as default I/O Stream.

Get the default I/O Stream configured.

sl_status_t
sl_iostream_set_system_default(sl_iostream_t *stream)

Configure the systemwide default stream.

sl_status_t
sl_iostream_write(sl_iostream_t *stream, const void *buffer, size_t buffer_length)

Output data on a stream.

sl_status_t
sl_iostream_read(sl_iostream_t *stream, void *buffer, size_t buffer_length, size_t *bytes_read)

Get data from a stream.

sl_status_t
sl_iostream_putchar(sl_iostream_t *stream, char c)

Print a character on stream.

sl_status_t
sl_iostream_getchar(sl_iostream_t *stream, char *c)

Print a character on stream.

sl_status_t
sl_iostream_vprintf(sl_iostream_t *stream, const char *format, va_list argp)

Print a formated string on stream.

sl_status_t
sl_iostream_printf(sl_iostream_t *stream, const char *format,...)

Print a formated string on stream.

Enumeration Documentation#

sl_iostream_type_t#

sl_iostream_type_t

Enumeration representing the possible types of iostream instances.

Enumerator
SL_IOSTREAM_TYPE_SWO

SWO Instance.

SL_IOSTREAM_TYPE_RTT

RTT Instance.

SL_IOSTREAM_TYPE_UART

USART Instance.

SL_IOSTREAM_TYPE_VUART

Vuart.

SL_IOSTREAM_TYPE_DEBUG_OUTPUT

Backchannel output Instance Type.

SL_IOSTREAM_TYPE_LOOPBACK

Loopback Instance.

SL_IOSTREAM_TYPE_UNDEFINED

Undefined Instance Type.


Function Documentation#

sl_iostream_set_default#

sl_status_t sl_iostream_set_default (sl_iostream_t * stream)

Set the stream as default I/O Stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to set as default.

Returns

  • Status result


sl_iostream_get_default#

sl_iostream_t * sl_iostream_get_default (void )

Get the default I/O Stream configured.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status result


sl_iostream_set_system_default#

sl_status_t sl_iostream_set_system_default (sl_iostream_t * stream)

Configure the systemwide default stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used.

Returns

  • Status result


sl_iostream_write#

sl_status_t sl_iostream_write (sl_iostream_t * stream, const void * buffer, size_t buffer_length)

Output data on a stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used. SL_IOSTREAM_STDOUT; Default output stream will be used. Pointer to specific stream; Specific stream will be used.

const void *[in]buffer

Buffer that contains the data to output.

size_t[in]buffer_length

Data length contained in the buffer.

Returns

  • Status result


sl_iostream_read#

sl_status_t sl_iostream_read (sl_iostream_t * stream, void * buffer, size_t buffer_length, size_t * bytes_read)

Get data from a stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used. SL_IOSTREAM_STDIN; Default input stream will be used. Pointer to specific stream; Specific stream will be used.

void *[out]buffer

Buffer that contains the data to output.

size_t[in]buffer_length

Data length contained in the buffer.

size_t *[out]bytes_read

Data length copied to the buffer.

Returns

  • Status result


sl_iostream_putchar#

sl_status_t sl_iostream_putchar (sl_iostream_t * stream, char c)

Print a character on stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used: SL_IOSTREAM_STDOUT; Default output stream will be used. SL_IOSTREAM_STDERR; Default error output stream will be used. Pointer to specific stream; Specific stream will be used.

char[in]c

Character to print

Returns

  • Status result


sl_iostream_getchar#

sl_status_t sl_iostream_getchar (sl_iostream_t * stream, char * c)

Print a character on stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used. SL_IOSTREAM_STDIN; Default input stream will be used. Pointer to specific stream; Specific stream will be used.

char *[out]c

Pointer to variable that will receive the character.

Returns

  • Status result


sl_iostream_vprintf#

sl_status_t sl_iostream_vprintf (sl_iostream_t * stream, const char * format, va_list argp)

Print a formated string on stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used: SL_IOSTREAM_STDOUT; Default output stream will be used. SL_IOSTREAM_STDERR; Default error output stream will be used. Pointer to specific stream; Specific stream will be used.

const char *[in]format

String that contains the text to be written.

va_list[in]argp

A value identifying a variable arguments list.

Returns

  • Status result


sl_iostream_printf#

sl_status_t sl_iostream_printf (sl_iostream_t * stream, const char * format, ... )

Print a formated string on stream.

Parameters
TypeDirectionArgument NameDescription
sl_iostream_t *[in]stream

I/O Stream to be used: SL_IOSTREAM_STDOUT; Default output stream will be used. SL_IOSTREAM_STDERR; Default error output stream will be used. Pointer to specific stream; Specific stream will be used.

const char *[in]format

String that contains the text to be written.

...[in]

Additional arguments.

Returns

  • Status result