I/O Stream UART#
I/O Stream UART.
Overview#
UART layer provides a set of standard APIs that can be used with all type of UART interface.
Initialization#
Each UART stream type provides its initalization with parameters specific to them. Note
Each UART stream requires a dedicated (L)DMA channel through DMADRV.
Configuration#
RX Buffer Size#
The SL_IOSTREAM_<Peripheral>_<Instance>_RX_BUFFER_SIZE parameter should be chosen based on the time it takes for the MCU to consume the RX buffer, otherwise flow control will have to be asserted to avoid data loss. If hardware flow control is unavailable, data will be dropped.
Let's assume that the MCU is able to call the IOStream Read function with a maximum delay of 1ms. We have:
(1) MaximumDelay = RXBufferSize * TimePerDatum
Where TimePerDatum is defined by (#startBits + #dataBits + #parityBits + #stopBits)/BaudRate.
With default settings, we have 1 start & stop bit, 8 data bits and no parity.
Rewriting (1), we have:
(2) MaximumDelay = RXBufferSize * 10/BaudRate <=> RXBufferSize = MaximumDelay*Baudrate/10
With a baudrate of 921,600 and a maximum consumption delay of 1ms, we have
a recommended RXBufferSize of:
(3) RXBufferSize = 0.001*921600/10 = 93Bytes
This should ensure that flow control does not have to be asserted, slowing down the bus and if unavailable, that no data will be dropped.
Baudrate#
IOStream UART leverages the DMA in order consume data from the UART peripheral. When user reads data from IOStream, the internal reception buffer gets more room for receiving new data. However, this update process pauses the DMA, meaning that any new data coming from the bus will remain in the UART peripheral's FIFO. If too much data is received before the update can complete, hardware flow control will have be enforces, or data will be dropped if unavailable.
Measurements show that the DMA update executes in ~23.7us with -O3 optimization (-Os gives slightly worst performance of ~32.7us). With these, the following equations can be followed to understand the maximum baudrate supported by the current design, when no flow control is available:
The number of bytes received during the ring buffer update is given by:
(1) UpdateTime = FIFOSize * TimePerDatum
Where TimePerDatum is defined by (#startBits + #dataBits + #parityBits + #stopBits)/BaudRate.
With default settings, we have 1 start & stop bit, 8 data bits and no parity.
Rewriting (1), we have:
(2) UpdateTime = FIFOSize * 10/Baudrate
For USART, we have a FIFO of size 2. This means that for an update time of
23.7us, we have a max baudrate of:
(3) 23.7 = 2 * 10/Baudrate <=> Baudrate = 2*10/23.7 = 843,881Baud.
The maximum "real" baudrate is then 460,800 Baud, otherwise hardware flow control will have to be asserted, or data will be dropped.
To achieve higher throughput without flow control assertion, users can use the EUSART peripheral, which boasts a 16Bytes FIFO, allow for baudrate of upwards of 921600 without data loss with no hardware flow control.
Modules#
sl_iostream_uart_rx_subscriber_t
Typedefs#
I/O Stream UART new data callback.
Functions#
UART Stream De-init.
Configure Automatic line conversion.
Get Automatic line conversion.
Set next byte detect IRQ.
Restore the UART for normal operation after wakeup.
Add or remove energy mode restriction to enable/disable reception when the system goes to sleep.
Get reception energy mode restriction configuration.
Configure Read blocking mode.
Get read API block configuration.
Macros#
uart flow control none
uart flow control software
uartx on
uartx off
Typedef Documentation#
sl_iostream_uart_new_data_callback_t#
typedef void() sl_iostream_uart_new_data_callback_t(void *data) (void *data)
I/O Stream UART new data callback.
Function Documentation#
sl_iostream_uart_deinit#
sl_status_t sl_iostream_uart_deinit (sl_iostream_uart_t * iostream_uart)
UART Stream De-init.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART stream object. |
Returns
Status result
sl_iostream_uart_set_auto_cr_lf#
void sl_iostream_uart_set_auto_cr_lf (sl_iostream_uart_t * iostream_uart, bool on)
Configure Automatic line conversion.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART stream object. |
| bool | [in] | on | If true, automatic LF to CRLF conversion will be enabled. |
sl_iostream_uart_get_auto_cr_lf#
bool sl_iostream_uart_get_auto_cr_lf (sl_iostream_uart_t * iostream_uart)
Get Automatic line conversion.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART stream object. |
Returns
Auto-conversion mode.
sl_iostream_uart_prepare_for_sleep#
void sl_iostream_uart_prepare_for_sleep (sl_iostream_uart_t * iostream_uart)
Set next byte detect IRQ.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART stream object. |
sl_iostream_uart_wakeup#
void sl_iostream_uart_wakeup (sl_iostream_uart_t * iostream_uart)
Restore the UART for normal operation after wakeup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART stream object. |
sl_iostream_uart_set_rx_energy_mode_restriction#
void sl_iostream_uart_set_rx_energy_mode_restriction (sl_iostream_uart_t * iostream_uart, bool on)
Add or remove energy mode restriction to enable/disable reception when the system goes to sleep.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART context. |
| bool | [in] | on | If true, will be able to receive data when sleeping. i.e it affects the lowest power level that the system can go. Otherwise, it might not be possible to receive data when sleeping. |
sl_iostream_uart_get_rx_energy_mode_restriction#
bool sl_iostream_uart_get_rx_energy_mode_restriction (sl_iostream_uart_t * iostream_uart)
Get reception energy mode restriction configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART context. |
Returns
Sleep configuration.
sl_iostream_uart_set_read_block#
void sl_iostream_uart_set_read_block (sl_iostream_uart_t * iostream_uart, bool on)
Configure Read blocking mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART context. |
| bool | [in] | on | If false, the read API will be non-blocking. Otherwise the read API will block until data is received. |
sl_iostream_uart_get_read_block#
bool sl_iostream_uart_get_read_block (sl_iostream_uart_t * iostream_uart)
Get read API block configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_iostream_uart_t * | [in] | iostream_uart | UART context. |
Returns
Block mode.