Tamper Response#
In CPMS, the default tamper configuration will be automatically displayed for HSE SVH (Secure Vault High) parts, customization is available for each of these configurations for Secure Vault High parts only. The anti-tamper protection feature is only available on SVH devices. Each tamper configuration can be set to one of five different tamper response levels, ranging from ignore the tamper event to erase OTP of the affected device. CPMS will require a public command key to be uploaded when tamper is configured on a HSE-SVH device. For more information on anti-tamper protection, refer to AN1247: Anti-Tamper Protection Configuration and Use.