Building in VS Code#

This section covers creating a new sample application from an existing application, which is optional for Building , Flashing and Debugging the target Matter Accessory Devices.

Linux/Mac#

Step 1:#

Use the shortcut (Ctrl + Shift + P) to trigger the command pallet.

Step 2:#

Search for "Run Task" and select the "Copy Sample Application" option.

Step 3:#

On the drop-down menu, select "Copy Sample Application".

Step 4:#

On the next menu select an EFR32 example to copy.

Step 5:#

Select the appropriate target board.

Create EFR32 ExampleCreate EFR32 Example

Step 6:#

Provide a name for the sample application target directory in the Matter workspace.

Windows#

Copying a sample application is not supported for Windows at this time.