Using the Mattertool (chip-tool)#

The following commands show how to commission a 917 SoC Matter End Device (Matter Accessory Device), and then send the on/off commands with the mattertool automated script. The mattertool script provides an interface into various chip-tool commands used to create and interact with a Matter network.

Prerequistes#

  • Download the raspi image and flash the image onto pi using with default 'ubuntu' username and enable ssh in the options.

https://www.silabs.com/documents/public/software/SilabsMatterPi_2.3.0-1.3.zip

  • Erase 917 SoC (brd4338a) and Flash the lighting app on 917 SoC and flash the connectivity firmware image.

  • command for commission using mattertool :

  mattertool bleWifi -s <SSID> -p <passcode>

Basic Mattertool Commands#

Context

Command

Usage

Commissioning

mattertool bleWifi

Starts commissioning of a Matter Accessory Device using the chip-tool

Commissioning

mattertool pairing code

Commission a Matter end device which is already in the IPv6 local network

Commissioning

<node_id> <pairing code>

using it's pairing code

Multi-fabric

mattertool pairing open-commissioning-window

Open a commissioning window for a Matter end device

Multi-fabric

<node_id> <option> <window_timeout> <iteration> <discriminator>

so that it can join another fabric

Device interaction

mattertool on

Sends the on command to the Matter Accessory Device using the chip-tool

Device interaction

mattertool off

Sends the off command to the Matter Accessory Device using the chip-tool

Device interaction

mattertool onoff

Control the OnOff cluster of a specific Endpoint of a specific device

You can also use the full chip-tool command set (still using mattertool):

$ mattertool levelcontrol read current-level 106 1

Command

Description

help

Prints help options

bleWifi

For Matter Bluetooth LE Wi-FI commissioning with 917 SoC device

buildCT

Clean build of the chip-tool

cleanVars

Erase every Set variable used in the script. They will be set back to default or randomized value

off

Turn off the Light on the already-commissioned 917 SoC device

on

Turn on the Light on the already-commissioned 917 SoC device

toggle

Toggle the Light on the already-commissioned 917 SoC device

parsePayload

Parse the given Payload (QrCode string)

rebuildCT

Rebuild the chip-tool

vars

Print the Variables in use by the script

Some options/arguments can be added to the command to update the values of the variables used by the script.

Available commands:

Command

Description

-h, --help

Prints help options

-n, --nodeId DIGIT

Specify the Nodeid you are trying to reach

-e, --endpoint DIGIT

Specify an endpoint for the desired cluster

-s, --ssid STRING

Wi-Fi AP SSID that the end devices need to connect to

-p, --password STRING

Wi-Fi AP password

These configurations are held until overwritten, cleared with cleanVars or when Raspberry Pi reboots.

Active variables used by mattertool:

Variable

Value

MATTER_ROOT

/home/ubuntu/connectedhomeip

CHIPTOOL_PATH

/home/ubuntu/connectedhomeip/out/standalone/chip-tool

NODE_ID

31354

PINCODE

20202021

DISCRIMINATOR

3840

SSID

<your_SSID>

lastNodeId

0

You can preset them with export X=Y before running the script or use some available options to change some of them.

In most cases, MATTER_ROOT, CHIPTOOL_PATH, PINCODE, and DISCRIMINATOR should remain at the default set value.

For commissioning commands ( bleWifi), NODE_ID will be randomized if it is the same as the last pairing.

Scripts Alias#

The commands presented above are linked to scripts. You can edit .bashrc and rename the following alias to your liking.

$ alias mattertool=‘source $HOME/scripts/matterTool.sh’