Common header for bootloader tables.

Public Attributes#

uint32_t

Type of image.

uint32_t

Version number of the bootloader/application table.

uint32_t

Version number of the image.

Public Attribute Documentation#

type#

uint32_t BootloaderHeader_t::type

Type of image.


Definition at line 127 of file platform/bootloader/api/btl_interface.h

layout#

uint32_t BootloaderHeader_t::layout

Version number of the bootloader/application table.


Definition at line 129 of file platform/bootloader/api/btl_interface.h

version#

uint32_t BootloaderHeader_t::version

Version number of the image.


Definition at line 131 of file platform/bootloader/api/btl_interface.h