Reset Information#

Passing information when resetting into and out of the bootloader.

To signal the bootloader to run, the application needs to write the BootloaderResetCause_t structure to the first address of RAM, setting BootloaderResetCause_t::reason to BOOTLOADER_RESET_REASON_BOOTLOAD.

The reset cause is only valid if BootloaderResetCause_t::signature is set to BOOTLOADER_RESET_SIGNATURE_VALID.

BootloaderResetCause_t resetCause = {
  .reason = BOOTLOADER_RESET_REASON_BOOTLOAD,
  .signature = BOOTLOADER_RESET_SIGNATURE_VALID
} 

When the bootloader reboots back into the app, it sets the reset reason to BOOTLOADER_RESET_REASON_GO if the bootload succeeded, or BOOTLOADER_RESET_REASON_BADIMAGE if the bootload failed due to errors when parsing the upgrade image.

Note

Modules#

BootloaderResetCause_t

Macros#

#define
BOOTLOADER_RESET_REASON_UNKNOWN 0x0200u

Unknown bootloader cause (should never occur)

#define
BOOTLOADER_RESET_REASON_GO 0x0201u

Bootloader caused reset telling app to run.

#define
BOOTLOADER_RESET_REASON_BOOTLOAD 0x0202u

Application requested that bootloader runs.

#define
BOOTLOADER_RESET_REASON_BADIMAGE 0x0203u

Bootloader detected bad external upgrade image.

#define
BOOTLOADER_RESET_REASON_FATAL 0x0204u

Fatal Error or assert in bootloader.

#define
BOOTLOADER_RESET_REASON_FORCE 0x0205u

Forced bootloader activation.

#define
BOOTLOADER_RESET_REASON_OTAVALID 0x0206u

OTA Bootloader mode activation.

#define
BOOTLOADER_RESET_REASON_DEEPSLEEP 0x0207u

Bootloader initiated deep sleep.

#define
BOOTLOADER_RESET_REASON_BADAPP 0x0208u

Application verification failed.

#define
BOOTLOADER_RESET_REASON_UPGRADE 0x0209u

Bootloader requested that first stage upgrades main bootloader.

#define
BOOTLOADER_RESET_REASON_TIMEOUT 0x020Au

Bootloader timed out waiting for upgrade image.

#define
BOOTLOADER_RESET_REASON_FAULT 0x020Bu

Soft-reset was forced to handle a fault.

#define
BOOTLOADER_RESET_REASON_TZ_FAULT 0x020Cu

Soft-reset was forced to handle a security fault.

#define
BOOTLOADER_RESET_SIGNATURE_VALID 0xF00Fu

Reset signature is valid.

#define
BOOTLOADER_RESET_SIGNATURE_INVALID 0xC33Cu

Reset signature is invalid.