Compression Error Codes#
Bootloader error codes returned by the decompressor.
Offset from BOOTLOADER_ERROR_COMPRESSION_BASE
Macros#
#define
BOOTLOADER_ERROR_COMPRESSION_INIT (BOOTLOADER_ERROR_COMPRESSION_BASE | 0x01)
Could not initialize decompressor.
#define
BOOTLOADER_ERROR_COMPRESSION_STATE (BOOTLOADER_ERROR_COMPRESSION_BASE | 0x02)
Invalid decompressor state – possible invalid input.
#define
BOOTLOADER_ERROR_COMPRESSION_DATA (BOOTLOADER_ERROR_COMPRESSION_BASE | 0x03)
Data error.
#define
BOOTLOADER_ERROR_COMPRESSION_DATALEN (BOOTLOADER_ERROR_COMPRESSION_BASE | 0x04)
Data length error.
#define
BOOTLOADER_ERROR_COMPRESSION_MEM (BOOTLOADER_ERROR_COMPRESSION_BASE | 0x05)
Memory error.
Macro Definition Documentation#
BOOTLOADER_ERROR_COMPRESSION_INIT#
#define BOOTLOADER_ERROR_COMPRESSION_INITValue:
(BOOTLOADER_ERROR_COMPRESSION_BASE | 0x01)
Could not initialize decompressor.
Definition at line
363
of file platform/bootloader/api/btl_errorcode.h
BOOTLOADER_ERROR_COMPRESSION_STATE#
#define BOOTLOADER_ERROR_COMPRESSION_STATEValue:
(BOOTLOADER_ERROR_COMPRESSION_BASE | 0x02)
Invalid decompressor state – possible invalid input.
Definition at line
366
of file platform/bootloader/api/btl_errorcode.h
BOOTLOADER_ERROR_COMPRESSION_DATA#
#define BOOTLOADER_ERROR_COMPRESSION_DATAValue:
(BOOTLOADER_ERROR_COMPRESSION_BASE | 0x03)
Data error.
Definition at line
369
of file platform/bootloader/api/btl_errorcode.h
BOOTLOADER_ERROR_COMPRESSION_DATALEN#
#define BOOTLOADER_ERROR_COMPRESSION_DATALENValue:
(BOOTLOADER_ERROR_COMPRESSION_BASE | 0x04)
Data length error.
Definition at line
372
of file platform/bootloader/api/btl_errorcode.h
BOOTLOADER_ERROR_COMPRESSION_MEM#
#define BOOTLOADER_ERROR_COMPRESSION_MEMValue:
(BOOTLOADER_ERROR_COMPRESSION_BASE | 0x05)
Memory error.
Definition at line
375
of file platform/bootloader/api/btl_errorcode.h