UART Driver Error Codes#

Bootloader error codes returned by the UART driver.

Offset from BOOTLOADER_ERROR_UART_BASE

Macros#

#define
BOOTLOADER_ERROR_UART_UNINIT (BOOTLOADER_ERROR_UART_BASE | 0x01)

Operation not allowed because hardware has not been initialized.

#define
BOOTLOADER_ERROR_UART_INIT (BOOTLOADER_ERROR_UART_BASE | 0x02)

Hardware fail during initialization.

#define
BOOTLOADER_ERROR_UART_ARGUMENT (BOOTLOADER_ERROR_UART_BASE | 0x03)

Invalid argument.

#define
BOOTLOADER_ERROR_UART_TIMEOUT (BOOTLOADER_ERROR_UART_BASE | 0x04)

Operation timed out.

#define
BOOTLOADER_ERROR_UART_OVERFLOW (BOOTLOADER_ERROR_UART_BASE | 0x05)

Buffer overflow condition.

#define
BOOTLOADER_ERROR_UART_BUSY (BOOTLOADER_ERROR_UART_BASE | 0x06)

Busy condition.

Macro Definition Documentation#

BOOTLOADER_ERROR_UART_UNINIT#

#define BOOTLOADER_ERROR_UART_UNINIT
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x01)

Operation not allowed because hardware has not been initialized.


Definition at line 341 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_UART_INIT#

#define BOOTLOADER_ERROR_UART_INIT
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x02)

Hardware fail during initialization.


Definition at line 343 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_UART_ARGUMENT#

#define BOOTLOADER_ERROR_UART_ARGUMENT
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x03)

Invalid argument.


Definition at line 345 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_UART_TIMEOUT#

#define BOOTLOADER_ERROR_UART_TIMEOUT
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x04)

Operation timed out.


Definition at line 347 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_UART_OVERFLOW#

#define BOOTLOADER_ERROR_UART_OVERFLOW
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x05)

Buffer overflow condition.


Definition at line 349 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_UART_BUSY#

#define BOOTLOADER_ERROR_UART_BUSY
Value:
(BOOTLOADER_ERROR_UART_BASE | 0x06)

Busy condition.


Definition at line 351 of file platform/bootloader/api/btl_errorcode.h