Storage API accessible from the application.
Public Attributes#
Version of this struct.
Get information about the storage – capabilities, layout, configuration.
Get information about storage slot – size, location.
Read bytes from slot into buffer.
Write bytes from buffer into slot.
Get application minimum version.
Mark a list of slots for bootload.
Mark a list of slots for bootload.
Append a slot to bootload list.
Start image parsing.
Continue image verification.
Get app and bootloader upgrade information from storage slot.
Check whether the bootloader storage is busy.
Read raw bytes from storage.
Write bytes to raw storage.
Erase storage.
Get configured DMA channel.
Erase an entire slot.
Public Attribute Documentation#
getInfo#
void(* BootloaderStorageFunctions_t::getInfo)(BootloaderStorageInformation_t *info)
Get information about the storage – capabilities, layout, configuration.
getSlotInfo#
int32_t(* BootloaderStorageFunctions_t::getSlotInfo)(uint32_t slotId, BootloaderStorageSlot_t *slot)
Get information about storage slot – size, location.
read#
int32_t(* BootloaderStorageFunctions_t::read)(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length)
Read bytes from slot into buffer.
write#
int32_t(* BootloaderStorageFunctions_t::write)(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length)
Write bytes from buffer into slot.
getAppMinVersion#
void(* BootloaderStorageFunctions_t::getAppMinVersion) (uint32_t *version)
Get application minimum version.
setImagesToBootload#
int32_t(* BootloaderStorageFunctions_t::setImagesToBootload)(int32_t *slotIds, size_t length)
Mark a list of slots for bootload.
getImagesToBootload#
int32_t(* BootloaderStorageFunctions_t::getImagesToBootload)(int32_t *slotIds, size_t length)
Mark a list of slots for bootload.
appendImageToBootloadList#
int32_t(* BootloaderStorageFunctions_t::appendImageToBootloadList)(int32_t slotId)
Append a slot to bootload list.
initParseImage#
int32_t(* BootloaderStorageFunctions_t::initParseImage)(uint32_t slotId, BootloaderParserContext_t *context, size_t contextSize)
Start image parsing.
verifyImage#
int32_t(* BootloaderStorageFunctions_t::verifyImage)(BootloaderParserContext_t *context, BootloaderParserCallback_t metadataCallback)
Continue image verification.
getImageInfo#
int32_t(* BootloaderStorageFunctions_t::getImageInfo)(BootloaderParserContext_t *context, ApplicationData_t *appInfo, uint32_t *bootloaderVersion)
Get app and bootloader upgrade information from storage slot.
isBusy#
bool(* BootloaderStorageFunctions_t::isBusy)(void)
Check whether the bootloader storage is busy.
readRaw#
int32_t(* BootloaderStorageFunctions_t::readRaw)(uint32_t address, uint8_t *buffer, size_t length)
Read raw bytes from storage.
writeRaw#
int32_t(* BootloaderStorageFunctions_t::writeRaw)(uint32_t address, uint8_t *buffer, size_t length)
Write bytes to raw storage.
eraseRaw#
int32_t(* BootloaderStorageFunctions_t::eraseRaw)(uint32_t address, size_t length)
Erase storage.
getDMAchannel#
int32_t(* BootloaderStorageFunctions_t::getDMAchannel)(void)
Get configured DMA channel.