display.h File Reference
Display device interface.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file display.h
.
#include <stdbool.h>
#include <stdint.h>
#include "emstatus.h
"
#include "displayconfigall.h
"
Data Structures | |
struct | DISPLAY_Device_t |
struct | DISPLAY_Geometry_t |
Macros | |
#define | DISPLAY_EMSTATUS_INVALID_PARAMETER (DISPLAY_EMSTATUS_BASE | 3) |
#define | DISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY (DISPLAY_EMSTATUS_BASE | 1) |
#define | DISPLAY_EMSTATUS_NOT_INITIALIZED (DISPLAY_EMSTATUS_BASE | 5) |
#define | DISPLAY_EMSTATUS_NOT_SUPPORTED (DISPLAY_EMSTATUS_BASE | 4) |
#define | DISPLAY_EMSTATUS_OK (0) |
#define | DISPLAY_EMSTATUS_OUT_OF_RANGE (DISPLAY_EMSTATUS_BASE | 2) |
Typedefs | |
typedef enum DISPLAY_AddressMode_t | DISPLAY_AddressMode_t |
typedef enum DISPLAY_ColourMode_t | DISPLAY_ColourMode_t |
typedef struct DISPLAY_Device_t | DISPLAY_Device_t |
typedef struct DISPLAY_Geometry_t | DISPLAY_Geometry_t |
typedef void * | DISPLAY_PixelMatrix_t |
typedef EMSTATUS(* | pDisplayDeviceDriverInitFunction_t) (void) |
Functions | |
EMSTATUS | DISPLAY_DeviceGet (int displayDeviceNo, DISPLAY_Device_t *device) |
Get the display device data structure corresponding to the device number. | |
EMSTATUS | DISPLAY_DriverRefresh (void) |
Refresh all DISPLAY devices. | |
EMSTATUS | DISPLAY_Init (void) |
Initialize the DISPLAY module. | |