CANEMLIB
Detailed Description
Controller Area Network API.
The Controller Area Network Interface Bus (CAN) implements a multi-master serial bus for connecting microcontrollers and devices, also known as nodes, to communicate with each other in applications without a host computer. CAN is a message-based protocol, designed originally for automotive applications, but also used in many other scenarios. The complexity of a node can range from a simple I/O device up to an embedded computer with a CAN interface and sophisticated software. The node may also be a gateway allowing a standard computer to communicate over a USB or Ethernet port to the devices on a CAN network. Devices are connected to the bus through a host processor, a CAN controller, and a CAN transceiver.
Data Structures |
|
| struct | CAN_Init_TypeDef |
| struct | CAN_MessageObject_TypeDef |
Macros |
|
| #define | CAN_INIT_DEFAULT |
Enumerations |
|
| enum |
CAN_ErrorCode_TypeDef
{
canErrorNoError = CAN_STATUS_LEC_NONE, canErrorStuff = CAN_STATUS_LEC_STUFF, canErrorForm = CAN_STATUS_LEC_FORM, canErrorAck = CAN_STATUS_LEC_ACK, canErrorBit1 = CAN_STATUS_LEC_BIT1, canErrorBit0 = CAN_STATUS_LEC_BIT0, canErrorCrc = CAN_STATUS_LEC_CRC, canErrorUnused = CAN_STATUS_LEC_UNUSED } |
| enum |
CAN_Mode_TypeDef
{
canModeNormal , canModeBasic , canModeLoopBack , canModeSilentLoopBack , canModeSilent } |
Functions |
|
| void | CAN_AbortSendMessage ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Abort sending a message.
|
|
| void | CAN_ConfigureMessageObject ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool valid, bool tx, bool remoteTransfer, bool endOfBuffer, bool wait) |
|
Configure valid, TX/RX, remoteTransfer for a specific Message Object.
|
|
| __STATIC_INLINE void | CAN_Enable ( CAN_TypeDef *can, bool enable) |
|
Enable the Host Controller to send messages.
|
|
| uint32_t | CAN_GetClockFrequency ( CAN_TypeDef *can) |
|
Get the CAN module frequency.
|
|
| __STATIC_INLINE uint32_t | CAN_GetErrorCount ( CAN_TypeDef *can) |
|
Get the error count.
|
|
| __STATIC_INLINE CAN_ErrorCode_TypeDef | CAN_GetLastErrorCode ( CAN_TypeDef *can) |
|
Get the last error code and clear its register.
|
|
| __STATIC_INLINE uint32_t | CAN_HasNewdata ( CAN_TypeDef *can) |
|
Indicates which message objects have received new data.
|
|
| void | CAN_Init ( CAN_TypeDef *can, const CAN_Init_TypeDef *init) |
|
Initialize CAN.
|
|
| __STATIC_INLINE bool | CAN_IsEnabled ( CAN_TypeDef *can) |
|
Give the communication capabilities state.
|
|
| __STATIC_INLINE void | CAN_MessageIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN message interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGet ( CAN_TypeDef *can) |
|
Get pending CAN message interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGetEnabled ( CAN_TypeDef *can) |
|
Get CAN message interrupt flags that are pending and enabled.
|
|
| __STATIC_INLINE void | CAN_MessageIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN message interrupts.
|
|
| bool | CAN_MessageLost ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum) |
|
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
|
|
| void | CAN_ReadMessage ( CAN_TypeDef *can, uint8_t interface, CAN_MessageObject_TypeDef *message) |
|
Read data from a Message Object in RAM and store it in a message.
|
|
| __STATIC_INLINE void | CAN_ReadyWait ( CAN_TypeDef *can, uint8_t interface) |
|
Waiting function.
|
|
| void | CAN_Reset ( CAN_TypeDef *can) |
|
Set all CAN registers to RESETVALUE. Leave the CAN device disabled.
|
|
| void | CAN_ResetMessages ( CAN_TypeDef *can, uint8_t interface) |
|
Reset all Message Objects and set their data to 0.
|
|
| void | CAN_SendMessage ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Send data from the Message Object message.
|
|
| void | CAN_SendRequest ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Send a request for writing or reading RAM of the Message Object msgNum.
|
|
| void | CAN_SetBitTiming ( CAN_TypeDef *can, uint32_t bitrate, uint16_t propagationTimeSegment, uint16_t phaseBufferSegment1, uint16_t phaseBufferSegment2, uint16_t synchronisationJumpWidth) |
|
Set the bitrate and its parameters.
|
|
| void | CAN_SetIdAndFilter ( CAN_TypeDef *can, uint8_t interface, bool useMask, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Set the ID and the filter for a specific Message Object.
|
|
| void | CAN_SetMode ( CAN_TypeDef *can, CAN_Mode_TypeDef mode) |
|
Set the CAN operation mode.
|
|
| void | CAN_SetRoute ( CAN_TypeDef *can, bool active, uint16_t pinRxLoc, uint16_t pinTxLoc) |
|
Set the ROUTE registers.
|
|
| __STATIC_INLINE void | CAN_StatusClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear CAN status.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusGet ( CAN_TypeDef *can) |
|
Get CAN status.
|
|
| __STATIC_INLINE void | CAN_StatusIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN status interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGet ( CAN_TypeDef *can) |
|
Get pending CAN status interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGetEnabled ( CAN_TypeDef *can) |
|
Get pending and enabled CAN status interrupt flags.
|
|
| __STATIC_INLINE void | CAN_StatusIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN status interrupts.
|
|
| void | CAN_WriteData ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message) |
|
Write data from a message to the MIRx registers.
|
|
Macro Definition Documentation
| #define CAN_INIT_DEFAULT |
Default initialization of CAN_Init_TypeDef . The total duration of a bit with these default parameters is 10 tq (time quantum : tq = brp/fsys, brp being the baudrate prescaler and being set according to the wanted bitrate, fsys beeing the CAN device frequency).
Definition at line
185
of file
em_can.h
.
Enumeration Type Documentation
CAN Status codes.
Definition at line
65
of file
em_can.h
.
| enum CAN_Mode_TypeDef |
CAN peripheral mode.
Definition at line
95
of file
em_can.h
.
Function Documentation
| void CAN_AbortSendMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
wait
|
||
| ) |
Abort sending a message.
Set the TXRQST of the CTRL register to 0. Doesn't touch data or the other parameters. The user can call CAN_SendMessage() to send the object after using CAN_AbortSendMessage() .
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumA message number of this Message Object, [1 - 32]. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
733
of file
em_can.c
.
References _CAN_MIR_CTRL_TXRQST_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , and CAN_TypeDef::MIR .
| void CAN_ConfigureMessageObject | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
valid,
|
||
| bool |
tx,
|
||
| bool |
remoteTransfer,
|
||
| bool |
endOfBuffer,
|
||
| bool |
wait
|
||
| ) |
Configure valid, TX/RX, remoteTransfer for a specific Message Object.
The initialization bit has to be 0 to use this function.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumA message number of this Message Object, [1 - 32]. [in] validTrue if the Message Object is valid, false otherwise. [in] txTrue if the Message Object is used for transmission, false if used for reception. [in] remoteTransferTrue if the Message Object is used for remote transmission, false otherwise. [in] endOfBufferTrue if it is for a single Message Object or the end of a FIFO buffer, false if the Message Object is part of a FIFO buffer and not the last. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
505
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_SHIFT , _CAN_MIR_ARB_MSGVAL_MASK , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_EOB_SHIFT , _CAN_MIR_CTRL_RMTEN_SHIFT , _CAN_MIR_CTRL_RXIE_MASK , _CAN_MIR_CTRL_TXIE_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
| __STATIC_INLINE void CAN_Enable | ( | CAN_TypeDef * |
can,
|
| bool |
enable
|
||
| ) |
Enable the Host Controller to send messages.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] enableTrue to enable CAN device, false to disable it. If the CAN device is enabled, it goes to normal mode (the default working mode).
Definition at line
273
of file
em_can.h
.
References _CAN_CTRL_INIT_SHIFT , BUS_RegBitWrite() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() , and CAN_Reset() .
| uint32_t CAN_GetClockFrequency | ( | CAN_TypeDef * |
can
|
) |
Get the CAN module frequency.
An internal prescaler of 2 is inside the CAN module.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- A clock value.
Definition at line
133
of file
em_can.c
.
References CAN0 , CMU_ClockFreqGet() , and cmuClock_CAN0 .
Referenced by CAN_SetBitTiming() .
| __STATIC_INLINE uint32_t CAN_GetErrorCount | ( | CAN_TypeDef * |
can
|
) |
Get the error count.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- Error count.
Definition at line
484
of file
em_can.h
.
References CAN_TypeDef::ERRCNT .
| __STATIC_INLINE CAN_ErrorCode_TypeDef CAN_GetLastErrorCode | ( | CAN_TypeDef * |
can
|
) |
Get the last error code and clear its register.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- return Last error code.
Definition at line
321
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
| __STATIC_INLINE uint32_t CAN_HasNewdata | ( | CAN_TypeDef * |
can
|
) |
Indicates which message objects have received new data.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- State of MESSAGEDATA register indicating which message objects have received new data.
Definition at line
340
of file
em_can.h
.
References CAN_TypeDef::MESSAGEDATA .
| void CAN_Init | ( | CAN_TypeDef * |
can,
|
| const CAN_Init_TypeDef * |
init
|
||
| ) |
Initialize CAN.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] initA pointer to the CAN initialization structure.
Definition at line
100
of file
em_can.c
.
References _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_Init_TypeDef::bitrate , CAN_CTRL_INIT , CAN_Enable() , CAN_ResetMessages() , CAN_SetBitTiming() , CAN_TypeDef::CTRL , CAN_Init_TypeDef::enable , CAN_Init_TypeDef::phaseBufferSegment1 , CAN_Init_TypeDef::phaseBufferSegment2 , CAN_Init_TypeDef::propagationTimeSegment , CAN_Init_TypeDef::resetMessages , CAN_Init_TypeDef::synchronisationJumpWidth , and CAN_TypeDef::TEST .
| __STATIC_INLINE bool CAN_IsEnabled | ( | CAN_TypeDef * |
can
|
) |
Give the communication capabilities state.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- True if the Host Controller can send messages, false otherwise.
Definition at line
288
of file
em_can.h
.
References _CAN_CTRL_INIT_MASK , and CAN_TypeDef::CTRL .
Referenced by CAN_SetBitTiming() .
| __STATIC_INLINE void CAN_MessageIntClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending CAN message interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsPending CAN message interrupt source(s) to clear.
Definition at line
499
of file
em_can.h
.
References CAN_TypeDef::IF0IFC .
| __STATIC_INLINE void CAN_MessageIntDisable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Disable CAN message interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN message interrupt source(s) to disable.
Definition at line
514
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
| __STATIC_INLINE void CAN_MessageIntEnable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Enable CAN message interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN message interrupt source(s) to enable.
Definition at line
529
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
| __STATIC_INLINE uint32_t CAN_MessageIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN message interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending.
Definition at line
547
of file
em_can.h
.
References CAN_TypeDef::IF0IF .
| __STATIC_INLINE uint32_t CAN_MessageIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get CAN message interrupt flags that are pending and enabled.
- Note
- This function does not clear event bits.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending and enabled.
Definition at line
565
of file
em_can.h
.
References CAN_TypeDef::IF0IEN , and CAN_TypeDef::IF0IF .
| __STATIC_INLINE void CAN_MessageIntSet | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Set one or more CAN message interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN message interrupt source(s) to set as pending.
Definition at line
583
of file
em_can.h
.
References CAN_TypeDef::IF0IFS .
| bool CAN_MessageLost | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum
|
||
| ) |
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumA message number of the Message Object, [1 - 32].
- Returns
- True if a message was lost, false otherwise.
Definition at line
167
of file
em_can.c
.
References _CAN_MIR_CTRL_MESSAGEOF_MASK , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
| void CAN_ReadMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| CAN_MessageObject_TypeDef * |
message
|
||
| ) |
Read data from a Message Object in RAM and store it in a message.
Read the information from RAM on this Message Object : data but also the configuration of the other registers.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageA Message Object.
Definition at line
663
of file
em_can.c
.
References _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_DLC_SHIFT , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_TXRQSTNEWDAT , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and SL_MIN .
| __STATIC_INLINE void CAN_ReadyWait | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface
|
||
| ) |
Waiting function.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use.
Definition at line
304
of file
em_can.h
.
References _CAN_MIR_CMDREQ_BUSY_MASK , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , CAN_SendRequest() , CAN_SetIdAndFilter() , and CAN_WriteData() .
| void CAN_Reset | ( | CAN_TypeDef * |
can
|
) |
Set all CAN registers to RESETVALUE. Leave the CAN device disabled.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
Definition at line
797
of file
em_can.c
.
References _CAN_BITTIMING_RESETVALUE , _CAN_BRPE_RESETVALUE , _CAN_CONFIG_RESETVALUE , _CAN_CTRL_CCE_MASK , _CAN_CTRL_TEST_MASK , _CAN_IF0IEN_RESETVALUE , _CAN_IF0IFC_RESETVALUE , _CAN_IF0IFS_RESETVALUE , _CAN_IF1IEN_RESETVALUE , _CAN_IF1IF_RESETVALUE , _CAN_IF1IFC_RESETVALUE , _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CMDMASK_RESETVALUE , _CAN_MIR_CMDREQ_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_DATAH_RESETVALUE , _CAN_MIR_DATAL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , _CAN_ROUTE_RESETVALUE , _CAN_STATUS_RESETVALUE , _CAN_TEST_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_Enable() , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CMDREQ , CAN_TypeDef::CONFIG , CAN_TypeDef::CTRL , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_TypeDef::IF0IEN , CAN_TypeDef::IF0IFC , CAN_TypeDef::IF0IFS , CAN_TypeDef::IF1IEN , CAN_TypeDef::IF1IFC , CAN_TypeDef::IF1IFS , CAN_MIR_TypeDef::MASK , CAN_TypeDef::MIR , CAN_TypeDef::ROUTE , CAN_TypeDef::STATUS , and CAN_TypeDef::TEST .
| void CAN_ResetMessages | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface
|
||
| ) |
Reset all Message Objects and set their data to 0.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use.
Definition at line
765
of file
em_can.c
.
References _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MIR_TypeDef::MASK , and CAN_TypeDef::MIR .
Referenced by CAN_Init() .
| void CAN_SendMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| const CAN_MessageObject_TypeDef * |
message,
|
||
| bool |
wait
|
||
| ) |
Send data from the Message Object message.
If the message is configured as TX and remoteTransfer = 0, calling this function will send the data of this Message Object if its parameters are correct. If the message is TX and remoteTransfer = 1, this function will set the data of message to RAM and exit. Data will be automatically sent after reception of a remote frame. If the message is RX and remoteTransfer = 1, this function will send a remote frame to the corresponding ID. If the message is RX and remoteTransfer = 0, the user shouldn't call this function. It will also send a remote frame.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageA Message Object. [in] waitIf true, wait for the end of the transfer between the MIRx registers and RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
576
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_RX , _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_ARB_XTD_MASK , _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_RMTEN_MASK , _CAN_STATUS_LEC_MASK , CAN_MIR_TypeDef::ARB , BUS_RegMaskedWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_MIR_CTRL_DATAVALID , CAN_MIR_CTRL_TXRQST , CAN_ReadyWait() , CAN_SendRequest() , CAN_WriteData() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::dlc , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::id , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and CAN_TypeDef::STATUS .
| void CAN_SendRequest | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
wait
|
||
| ) |
Send a request for writing or reading RAM of the Message Object msgNum.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumA message number of the Message Object, [1 - 32]. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
893
of file
em_can.c
.
References _CAN_MIR_CMDREQ_MSGNUM_SHIFT , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| void CAN_SetBitTiming | ( | CAN_TypeDef * |
can,
|
| uint32_t |
bitrate,
|
||
| uint16_t |
propagationTimeSegment,
|
||
| uint16_t |
phaseBufferSegment1,
|
||
| uint16_t |
phaseBufferSegment2,
|
||
| uint16_t |
synchronisationJumpWidth
|
||
| ) |
Set the bitrate and its parameters.
Multiple parameters need to be properly configured. See the reference manual for a detailed description. Careful : the BRP (Baud Rate Prescaler) is calculated by: 'brp = freq / (period * bitrate);'. freq is the frequency of the CAN device, period the time of transmission of a bit. The result is an uint32_t. Hence it's truncated, causing an approximation error. This error is non negligible when the period is high, the bitrate is high, and frequency is low.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] bitrateA wanted bitrate on the CAN bus. [in] propagationTimeSegmentA value for the Propagation Time Segment. [in] phaseBufferSegment1A value for the Phase Buffer Segment 1. [in] phaseBufferSegment2A value for the Phase Buffer Segment 2. [in] synchronisationJumpWidthA value for the Synchronization Jump Width.
Definition at line
264
of file
em_can.c
.
References _CAN_BITTIMING_BRP_SHIFT , _CAN_BITTIMING_SJW_SHIFT , _CAN_BITTIMING_TSEG1_SHIFT , _CAN_BITTIMING_TSEG2_SHIFT , _CAN_CTRL_CCE_MASK , _CAN_CTRL_INIT_MASK , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_CTRL_CCE , CAN_CTRL_INIT , CAN_GetClockFrequency() , CAN_IsEnabled() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() .
| void CAN_SetIdAndFilter | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| bool |
useMask,
|
||
| const CAN_MessageObject_TypeDef * |
message,
|
||
| bool |
wait
|
||
| ) |
Set the ID and the filter for a specific Message Object.
The initialization bit has to be 0 to use this function.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] useMaskA boolean to choose whether or not to use the masks. [in] messageA Message Object. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
410
of file
em_can.c
.
References _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_UMASK_SHIFT , _CAN_MIR_MASK_MASK_SHIFT , _CAN_MIR_MASK_MDIR_SHIFT , _CAN_MIR_MASK_MXTD_SHIFT , CAN_MIR_TypeDef::ARB , BUS_RegBitWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::directionMask , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::extendedMask , CAN_MessageObject_TypeDef::id , CAN_MIR_TypeDef::MASK , CAN_MessageObject_TypeDef::mask , CAN_TypeDef::MIR , and CAN_MessageObject_TypeDef::msgNum .
| void CAN_SetMode | ( | CAN_TypeDef * |
can,
|
| CAN_Mode_TypeDef |
mode
|
||
| ) |
Set the CAN operation mode.
In initialization mode, the CAN module is deactivated. Reset the messages in all other modes to be sure that there is no leftover data that needs to be configured before use.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] modeMode of operation : Init, Normal, Loopback, SilentLoopback, Silent, Basic.
Definition at line
336
of file
em_can.c
.
References _CAN_CTRL_EIE_MASK , _CAN_CTRL_IE_MASK , _CAN_CTRL_SIE_MASK , _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_CTRL_TEST , CAN_TEST_BASIC , CAN_TEST_LBACK , CAN_TEST_SILENT , canModeBasic , canModeLoopBack , canModeNormal , canModeSilent , canModeSilentLoopBack , CAN_TypeDef::CTRL , and CAN_TypeDef::TEST .
| void CAN_SetRoute | ( | CAN_TypeDef * |
can,
|
| bool |
active,
|
||
| uint16_t |
pinRxLoc,
|
||
| uint16_t |
pinTxLoc
|
||
| ) |
Set the ROUTE registers.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] activeA boolean indicating whether or not to activate the ROUTE registers. [in] pinRxLocA location of the RX pin. [in] pinTxLocA location of the TX pin.
Definition at line
217
of file
em_can.c
.
References _CAN_ROUTE_RXLOC_SHIFT , _CAN_ROUTE_TXLOC_SHIFT , CAN_ROUTE_TXPEN , and CAN_TypeDef::ROUTE .
| __STATIC_INLINE void CAN_StatusClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear CAN status.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN status bits to clear.
Definition at line
469
of file
em_can.h
.
References CAN_TypeDef::STATUS .
| __STATIC_INLINE uint32_t CAN_StatusGet | ( | CAN_TypeDef * |
can
|
) |
Get CAN status.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- A value of CAN register STATUS.
Definition at line
454
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
| __STATIC_INLINE void CAN_StatusIntClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending CAN status interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsPending CAN status interrupt source(s) to clear.
Definition at line
355
of file
em_can.h
.
References CAN_TypeDef::IF1IFC .
| __STATIC_INLINE void CAN_StatusIntDisable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Disable CAN status interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN status interrupt source(s) to disable.
Definition at line
370
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
| __STATIC_INLINE void CAN_StatusIntEnable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Enable CAN status interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN status interrupt source(s) to enable.
Definition at line
385
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
| __STATIC_INLINE uint32_t CAN_StatusIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN status interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending.
Definition at line
403
of file
em_can.h
.
References CAN_TypeDef::IF1IF .
| __STATIC_INLINE uint32_t CAN_StatusIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get pending and enabled CAN status interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] canA pointer to the CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending and enabled.
Definition at line
421
of file
em_can.h
.
References CAN_TypeDef::IF1IEN , and CAN_TypeDef::IF1IF .
| __STATIC_INLINE void CAN_StatusIntSet | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Set one or more CAN status interrupts.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] flagsCAN status interrupt source(s) to set to pending.
Definition at line
439
of file
em_can.h
.
References CAN_TypeDef::IF1IFS .
| void CAN_WriteData | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| const CAN_MessageObject_TypeDef * |
message
|
||
| ) |
Write data from a message to the MIRx registers.
- Parameters
-
[in] canA pointer to the CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageA Message Object.
Definition at line
847
of file
em_can.c
.
References CAN_ReadyWait() , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , and SL_MIN .
Referenced by CAN_SendMessage() .