MTB_TypeDef Struct ReferenceDevices > MTB
MTB Register Declaration
Definition at line
49
of file
efm32tg11b_mtb.h
.
#include <
efm32tg11b_mtb.h
>
Data Fields |
|
| __IOM uint32_t | BASE |
| __IOM uint32_t | FLOW |
| __IOM uint32_t | MASTER |
| __IOM uint32_t | POSITION |
Field Documentation
| __IOM uint32_t MTB_TypeDef::BASE |
MTB Trace Base Register
Definition at line
53
of file
efm32tg11b_mtb.h
.
| __IOM uint32_t MTB_TypeDef::FLOW |
MTB Trace Flow Register
Definition at line
52
of file
efm32tg11b_mtb.h
.
| __IOM uint32_t MTB_TypeDef::MASTER |
MTB Trace Control Register
Definition at line
51
of file
efm32tg11b_mtb.h
.
| __IOM uint32_t MTB_TypeDef::POSITION |
MTB Trace Position Register.
Definition at line
50
of file
efm32tg11b_mtb.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_mtb.h