gpiointerrupt.h File Reference
GPIOINT API definition.
- Version
- 5.5.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file gpiointerrupt.h
.
#include "em_device.h
"
Typedefs | |
typedef void(* | GPIOINT_IrqCallbackPtr_t) (uint8_t pin) |
GPIO interrupt callback function pointer. | |
Functions | |
void | GPIOINT_CallbackRegister (uint8_t pin, GPIOINT_IrqCallbackPtr_t callbackPtr) |
Registers user callback for given pin number. | |
static __INLINE void | GPIOINT_CallbackUnRegister (uint8_t pin) |
Unregisters user callback for given pin number. | |
void | GPIOINT_Init (void) |
Initialization of GPIOINT module. | |