MSC_ExecConfig_TypeDef Struct ReferenceEMLIB > MSC
Code execution configuration.
Definition at line 152 of file em_msc.h.
#include <em_msc.h>
Data Fields | |
| bool | aiDis |
| bool | iccDis |
| bool | ifcDis |
| bool | prefetchEn |
| bool | scbtEn |
| bool | useHprot |
Field Documentation
| bool MSC_ExecConfig_TypeDef::aiDis |
Disable automatic cache invalidation on write or erase.
Definition at line 156 of file em_msc.h.
Referenced by MSC_ExecConfigSet().
| bool MSC_ExecConfig_TypeDef::iccDis |
Disable automatic caching of fetches in interrupt context.
Definition at line 157 of file em_msc.h.
Referenced by MSC_ExecConfigSet().
| bool MSC_ExecConfig_TypeDef::ifcDis |
Disable instruction cache.
Definition at line 155 of file em_msc.h.
Referenced by MSC_ExecConfigSet().
| bool MSC_ExecConfig_TypeDef::prefetchEn |
| bool MSC_ExecConfig_TypeDef::scbtEn |
Enable Suppressed Conditional Branch Target Prefetch.
Definition at line 153 of file em_msc.h.
Referenced by MSC_ExecConfigSet().
| bool MSC_ExecConfig_TypeDef::useHprot |
Use ahb_hprot to determine if the instruction is cacheable or not.
Definition at line 158 of file em_msc.h.
Referenced by MSC_ExecConfigSet().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_msc.h