API_LayerEMDRV > EZRADIODRV

Detailed Description

EzRadio API Layer


     

.

Enumerations

enum EZRADIO_ConfigRet_t {
EZRADIO_CONFIG_SUCCESS ,
EZRADIO_CONFIG_NO_PATCH ,
EZRADIO_CONFIG_CTS_TIMEOUT ,
EZRADIO_CONFIG_PATCH_FAIL ,
EZRADIO_CONFIG_COMMAND_ERROR
}

Functions

void ezradio_change_state (uint8_t next_state1)
EZRADIO_ConfigRet_t ezradio_configuration_init (const uint8_t *pSetPropCmd)
void ezradio_ezconfig_check (uint16_t checksum, ezradio_cmd_reply_t *ezradioReply)
void ezradio_fifo_info (uint8_t fifo, ezradio_cmd_reply_t *ezradioReply)
void ezradio_fifo_info_fast_read (ezradio_cmd_reply_t *ezradioReply)
void ezradio_fifo_info_fast_reset (uint8_t fifo)
void ezradio_frr_a_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
void ezradio_frr_b_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
void ezradio_frr_c_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
void ezradio_frr_d_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
void ezradio_func_info (ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_adc_reading (uint8_t adc_en, uint8_t adc_cfg, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_chip_status (uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_chip_status_fast_clear (void)
void ezradio_get_chip_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_int_status (uint8_t ph_clr_pend, uint8_t modem_clr_pend, uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_int_status_fast_clear (void)
void ezradio_get_int_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_modem_status (uint8_t modem_clr_pend, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_modem_status_fast_clear (void)
void ezradio_get_modem_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_packet_info (uint8_t field_number_mask, uint16_t len, int16_t diff_len, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_ph_status (uint8_t ph_clr_pend, ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_ph_status_fast_clear (void)
void ezradio_get_ph_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
void ezradio_get_property (uint8_t group, uint8_t num_props, uint8_t start_prop, ezradio_cmd_reply_t *ezradioReply)
void ezradio_gpio_pin_cfg (uint8_t gpio0, uint8_t gpio1, uint8_t gpio2, uint8_t gpio3, uint8_t nirq, uint8_t sdo, uint8_t gen_config, ezradio_cmd_reply_t *ezradioReply)
void ezradio_gpio_pin_cfg_fast (ezradio_cmd_reply_t *ezradioReply)
void ezradio_ircal (uint8_t searching_step_size, uint8_t searching_rssi_avg, uint8_t rx_chain_setting1, uint8_t rx_chain_setting2)
void ezradio_ircal_manual (uint8_t ircal_amp, uint8_t ircal_ph, ezradio_cmd_reply_t *ezradioReply)
void ezradio_nop (void)
void ezradio_part_info (ezradio_cmd_reply_t *ezradioReply)
void ezradio_power_up (uint8_t boot_options, uint8_t xtal_options, uint32_t xo_freq)
void ezradio_read_cmd_buff (ezradio_cmd_reply_t *ezradioReply)
void ezradio_read_rx_fifo (uint8_t numbytes, uint8_t *prxdata)
void ezradio_request_device_state (ezradio_cmd_reply_t *ezradioReply)
void ezradio_reset (void)
void ezradio_rx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0)
void ezradio_set_property (uint8_t group, uint8_t num_props, uint8_t start_prop,...)
void ezradio_start_rx (uint8_t channel, uint8_t condition, uint16_t rx_len, uint8_t next_state1, uint8_t next_state2, uint8_t next_state3)
void ezradio_start_rx_fast (void)
void ezradio_start_tx (uint8_t channel, uint8_t condition, uint16_t tx_len)
void ezradio_start_tx_fast (void)
void ezradio_tx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0, uint8_t pll_settle_time1, uint8_t pll_settle_time0)
void ezradio_write_ezconfig_array (uint8_t numBytes, uint8_t *pEzConfigArray)
void ezradio_write_tx_fifo (uint8_t numbytes, uint8_t *pdata)

Enumeration Type Documentation

EZRadio device configuration return values

Enumerator
EZRADIO_CONFIG_SUCCESS

Configuration succeded.

EZRADIO_CONFIG_NO_PATCH

No patch is given.

EZRADIO_CONFIG_CTS_TIMEOUT

CTS timeout error during configuration.

EZRADIO_CONFIG_PATCH_FAIL

Patching is failed.

EZRADIO_CONFIG_COMMAND_ERROR

Command error during configuration.

Definition at line 65 of file ezradio_api_lib.h .

Function Documentation

void ezradio_change_state ( uint8_t next_state1 )

Issue a change state command to the radio.

Parameters
[in] next_state1 Next state.

Definition at line 298 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

Referenced by ezradioStopDirectReceive() , ezradioStopDirectTransmit() , ezradioStopPn9() , and ezradioStopUnmodulatedCarrier() .

EZRADIO_ConfigRet_t ezradio_configuration_init ( const uint8_t * pSetPropCmd )

This function is used to load all properties and commands with a list of NULL terminated commands. Before this function ezradio_reset should be called.

Parameters
[in] pSetPropCmd Pointer to the configuration array.

Definition at line 53 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmdGetResp() , EZRADIO_CONFIG_COMMAND_ERROR , EZRADIO_CONFIG_CTS_TIMEOUT , EZRADIO_CONFIG_SUCCESS , ezradio_get_int_status() , ezradio_hal_NirqLevel() , and ezradio_write_ezconfig_array() .

Referenced by ezradioInit() .

void ezradio_ezconfig_check ( uint16_t checksum,
ezradio_cmd_reply_t * ezradioReply
)

Validates the EZConfig array was written correctly.

Parameters
[in] checksum Checksum value
[out] ezradioReply Reply structure of the command.

Definition at line 143 of file ezradio_api_lib_add.c .

References ezradio_comm_CtsWentHigh , and ezradio_comm_SendCmdGetResp() .

void ezradio_fifo_info ( uint8_t fifo,
ezradio_cmd_reply_t * ezradioReply
)

Send the FIFO_INFO command to the radio. Optionally resets the TX/RX FIFO. Reads the radio response back into ezradioReply.

Parameters
[in] fifo RX/TX FIFO reset flags.
[out] ezradioReply Reply structure of the command.

Definition at line 332 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

Referenced by ezradioResetTRxFifo() .

void ezradio_fifo_info_fast_read ( ezradio_cmd_reply_t * ezradioReply )

Reads RX/TX FIFO count space. Does NOT reset RX/TX FIFO

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 962 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_fifo_info_fast_reset ( uint8_t fifo )

Resets the RX/TX FIFO. Does not read back anything from TX/RX FIFO

Parameters
[in] fifo FIFO to be reset.

Definition at line 946 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_frr_a_read ( uint8_t respByteCount,
ezradio_cmd_reply_t * ezradioReply
)

Reads the Fast Response Registers starting with A register into ezradioReply union.

Parameters
[in] respByteCount Number of Fast Response Registers to be read.
[out] ezradioReply Reply structure of the command.

Definition at line 452 of file ezradio_api_lib.c .

References ezradio_comm_ReadData() .

void ezradio_frr_b_read ( uint8_t respByteCount,
ezradio_cmd_reply_t * ezradioReply
)

Reads the Fast Response Registers starting with B register into ezradioReply union.

Parameters
[in] respByteCount Number of Fast Response Registers to be read.
[out] ezradioReply Reply structure of the command.

Definition at line 476 of file ezradio_api_lib.c .

References ezradio_comm_ReadData() .

void ezradio_frr_c_read ( uint8_t respByteCount,
ezradio_cmd_reply_t * ezradioReply
)

Reads the Fast Response Registers starting with C register into ezradioReply union.

Parameters
[in] respByteCount Number of Fast Response Registers to be read.
[out] ezradioReply Reply structure of the command.

Definition at line 500 of file ezradio_api_lib.c .

References ezradio_comm_ReadData() .

void ezradio_frr_d_read ( uint8_t respByteCount,
ezradio_cmd_reply_t * ezradioReply
)

Reads the Fast Response Registers starting with D register into ezradioReply union.

Parameters
[in] respByteCount Number of Fast Response Registers to be read.
[out] ezradioReply Reply structure of the command.

Definition at line 524 of file ezradio_api_lib.c .

References ezradio_comm_ReadData() .

void ezradio_func_info ( ezradio_cmd_reply_t * ezradioReply )

Sends the FUNC_INFO command to the radio, then reads the resonse into ezradioReply union.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 426 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_adc_reading ( uint8_t adc_en,
uint8_t adc_cfg,
ezradio_cmd_reply_t * ezradioReply
)

Reads the ADC values from the radio into ezradioReply union.

Parameters
[in] adc_en ADC enable parameter.
[in] adc_cfg ADC configuration parameter.
[out] ezradioReply Reply structure of the command.

Definition at line 178 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_chip_status ( uint8_t chip_clr_pend,
ezradio_cmd_reply_t * ezradioReply
)

Gets the Chip status flags. Optionally clears them.

Parameters
[in] chip_clr_pend Flags to clear.
[out] ezradioReply Reply structure of the command.

Definition at line 664 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_chip_status_fast_clear ( void )

Clear all Chip status flags. Does NOT read back interrupt flags

Definition at line 906 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_get_chip_status_fast_clear_read ( ezradio_cmd_reply_t * ezradioReply )

Clear and read all Chip status flags.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 922 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_int_status ( uint8_t ph_clr_pend,
uint8_t modem_clr_pend,
uint8_t chip_clr_pend,
ezradio_cmd_reply_t * ezradioReply
)

Get the Interrupt status/pending flags form the radio and clear flags if requested.

Parameters
[in] ph_clr_pend Packet Handler pending flags clear.
[in] modem_clr_pend Modem Status pending flags clear.
[in] chip_clr_pend Chip State pending flags clear.
[out] ezradioReply Reply structure of the command.

Definition at line 185 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

Referenced by ezradio_configuration_init() , ezradioInit() , ezradioPluginManager() , ezradioStartDirectReceive() , ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .

void ezradio_get_int_status_fast_clear ( void )

Clear all Interrupt status/pending flags. Does NOT read back interrupt flags

Definition at line 753 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_get_int_status_fast_clear_read ( ezradio_cmd_reply_t * ezradioReply )

Clear and read all Interrupt status/pending flags

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 768 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_modem_status ( uint8_t modem_clr_pend,
ezradio_cmd_reply_t * ezradioReply
)

Gets the Modem status flags. Optionally clears them.

Parameters
[in] modem_clr_pend Flags to clear.
[out] ezradioReply Reply structure of the command.

Definition at line 633 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_modem_status_fast_clear ( void )

Clear all Modem status flags. Does NOT read back interrupt flags

Definition at line 862 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_get_modem_status_fast_clear_read ( ezradio_cmd_reply_t * ezradioReply )

Clear and read all Modem status flags.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 878 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_packet_info ( uint8_t field_number_mask,
uint16_t len,
int16_t diff_len,
ezradio_cmd_reply_t * ezradioReply
)

Receives information from the radio of the current packet. Optionally can be used to modify the Packet Handler properties during packet reception.

Parameters
[in] field_number_mask Packet Field number mask value.
[in] len Length value.
[in] diff_len Difference length.
[out] ezradioReply Reply structure of the command.

Definition at line 693 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_ph_status ( uint8_t ph_clr_pend,
ezradio_cmd_reply_t * ezradioReply
)

Gets the Packet Handler status flags. Optionally clears them.

Parameters
[in] ph_clr_pend Flags to clear.
[out] ezradioReply Reply structure of the command.

Definition at line 608 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_ph_status_fast_clear ( void )

Clear all Packet Handler status flags. Does NOT read back interrupt flags

Definition at line 824 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_get_ph_status_fast_clear_read ( ezradio_cmd_reply_t * ezradioReply )

Clear and read all Packet Handler status flags.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 840 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_get_property ( uint8_t group,
uint8_t num_props,
uint8_t start_prop,
ezradio_cmd_reply_t * ezradioReply
)

Get property values from the radio. Reads them into ezradioReply union.

Parameters
[in] group Property group number.
[in] num_props Number of properties to be read.
[in] start_prop Starting sub-property number.
[out] ezradioReply Reply structure of the command.

Definition at line 382 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_gpio_pin_cfg ( uint8_t gpio0,
uint8_t gpio1,
uint8_t gpio2,
uint8_t gpio3,
uint8_t nirq,
uint8_t sdo,
uint8_t gen_config,
ezradio_cmd_reply_t * ezradioReply
)

Send GPIO pin config command to the radio and reads the answer into ezradioReply union.

Parameters
[in] gpio0 GPIO0 configuration.
[in] gpio1 GPIO1 configuration.
[in] gpio2 GPIO2 configuration.
[in] gpio3 GPIO3 configuration.
[in] nirq NIRQ configuration.
[in] sdo SDO configuration.
[in] gen_config General pin configuration.
[out] ezradioReply Reply structure of the command.

Definition at line 226 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_gpio_pin_cfg_fast ( ezradio_cmd_reply_t * ezradioReply )

Reads back current GPIO pin configuration. Does NOT configure GPIO pins

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 797 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_ircal ( uint8_t searching_step_size,
uint8_t searching_rssi_avg,
uint8_t rx_chain_setting1,
uint8_t rx_chain_setting2
)

Performs image rejection calibration. Completion can be monitored by polling CTS or waiting for CHIP_READY interrupt source.

Parameters
[in] searching_step_size
[in] searching_rssi_avg
[in] rx_chain_setting1
[in] rx_chain_setting2

Definition at line 144 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmd() .

void ezradio_ircal_manual ( uint8_t ircal_amp,
uint8_t ircal_ph,
ezradio_cmd_reply_t * ezradioReply
)

Image rejection calibration. Forces a specific value for IR calibration, and reads back calibration values from previous calibrations

Parameters
[in] ircal_amp
[in] ircal_ph
[out] ezradioReply Reply structure of the command.

Definition at line 165 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_nop ( void )

Sends NOP command to the radio. Can be used to maintain SPI communication.

Definition at line 315 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_part_info ( ezradio_cmd_reply_t * ezradioReply )

This function sends the PART_INFO command to the radio and receives the answer into ezradioReply union.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 101 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_power_up ( uint8_t boot_options,
uint8_t xtal_options,
uint32_t xo_freq
)

This function is used to initialize after power-up the radio chip. Before this function ezradio_reset should be called.

Parameters
[in] boot_options Boot options input to the power up command.
[in] xtal_options XTAL options input to the power up command.
[in] xo_freq XO frequency input to the power up command.

Definition at line 80 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_read_cmd_buff ( ezradio_cmd_reply_t * ezradioReply )

Reads the command buffer

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 570 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

void ezradio_read_rx_fifo ( uint8_t numBytes,
uint8_t * pRxData
)

Reads the RX FIFO content from the radio.

Parameters
[in] numBytes Data length to be read.
[in] pRxData Pointer to the buffer location.

Definition at line 369 of file ezradio_api_lib.c .

References ezradio_comm_ReadData() .

void ezradio_request_device_state ( ezradio_cmd_reply_t * ezradioReply )

Requests the current state of the device and lists pending TX and RX requests.

Parameters
[out] ezradioReply Reply structure of the command.

Definition at line 547 of file ezradio_api_lib.c .

References ezradio_comm_SendCmdGetResp() .

Referenced by ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .

void ezradio_reset ( void )

This functions is used to reset the EZRadio device by applying shutdown and releasing it. After this function ezradio_power_up or ezradio_configuration_init should be called. The user can check if POR has completed by waiting 4 ms or by polling radio GPIO 0, 2, or 3. When these GPIOs are high, it is safe to call the above mentioned functions.

Definition at line 54 of file ezradio_api_lib.c .

References ezradio_comm_ClearCTS() , ezradio_hal_AssertShutdown() , ezradio_hal_DeassertShutdown() , USTIMER_DeInit() , USTIMER_Delay() , and USTIMER_Init() .

void ezradio_rx_hop ( uint8_t inte,
uint8_t frac2,
uint8_t frac1,
uint8_t frac0,
uint8_t vco_cnt1,
uint8_t vco_cnt0
)

While in RX state this will hop to the frequency specified by the parameters and start searching for a preamble.

Parameters
[in] inte new inte register value.
[in] frac2 new frac2 register value.
[in] frac1 new frac1 register value.
[in] frac0 new frac0 register value.
[in] vco_cnt1 new vco_cnt1 register value.
[in] vco_cnt0 new vco_cnt0 register value.

Definition at line 225 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmd() .

void ezradio_set_property ( uint8_t group,
uint8_t num_props,
uint8_t start_prop,
...
)

Send SET_PROPERTY command to the radio.

Parameters
[in] group Property group.
[in] num_props Number of property to be set. The properties must be in ascending order in their sub-property aspect. Max. 12 properties can be set in one command.
[in] start_prop Start sub-property address.
[in] ... Variable number of properties to be set.

Definition at line 269 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_start_rx ( uint8_t channel,
uint8_t condition,
uint16_t rx_len,
uint8_t next_state1,
uint8_t next_state2,
uint8_t next_state3
)

Sends START_RX command to the radio.

Parameters
[in] channel Channel number.
[in] condition Start RX condition.
[in] rx_len Payload length (exclude the PH generated CRC).
[in] next_state1 Next state when Preamble Timeout occurs.
[in] next_state2 Next state when a valid packet received.
[in] next_state3 Next state when invalid packet received (e.g. CRC error).

Definition at line 160 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

Referenced by ezradioStartDirectReceive() , and ezradioStartRx() .

void ezradio_start_rx_fast ( void )

Sends START_RX command ID to the radio with no input parameters

Definition at line 739 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_start_tx ( uint8_t channel,
uint8_t condition,
uint16_t tx_len
)

Sends START_TX command to the radio.

Parameters
[in] channel Channel number.
[in] condition Start TX condition.
[in] tx_len Payload length (exclude the PH generated CRC).

Definition at line 131 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

Referenced by ezradioStartDirectTransmit() , ezradioStartPn9() , and ezradioStartUnmodulatedCarrier() .

void ezradio_start_tx_fast ( void )

Sends START_TX command ID to the radio with no input parameters

Definition at line 725 of file ezradio_api_lib.c .

References ezradio_comm_SendCmd() .

void ezradio_tx_hop ( uint8_t inte,
uint8_t frac2,
uint8_t frac1,
uint8_t frac0,
uint8_t vco_cnt1,
uint8_t vco_cnt0,
uint8_t pll_settle_time1,
uint8_t pll_settle_time0
)

While in TX state this will hop to the frequency specified by the parameters

Parameters
[in] inte new inte register value.
[in] frac2 new frac2 register value.
[in] frac1 new frac1 register value.
[in] frac0 new frac0 register value.
[in] vco_cnt1 new vco_cnt1 register value.
[in] vco_cnt0 new vco_cnt0 register value.
[in] pll_settle_time1 new pll_settle_time1 register value.
[in] pll_settle_time0 new pll_settle_time0 register value.

Definition at line 197 of file ezradio_api_lib_add.c .

References ezradio_comm_SendCmd() .

void ezradio_write_ezconfig_array ( uint8_t numBytes,
uint8_t * pEzConfigArray
)

Writes data byte(s) to the EZConfig array.

Parameters
[in] numBytes number of bytes to send
[in] pEzConfigArray pointer to the EZConfig configuration array

Definition at line 132 of file ezradio_api_lib_add.c .

References ezradio_comm_WriteData() .

Referenced by ezradio_configuration_init() .

void ezradio_write_tx_fifo ( uint8_t numBytes,
uint8_t * pTxData
)

The function can be used to load data into TX FIFO.

Parameters
[in] numBytes Data length to be load.
[in] pTxData Pointer to the data (uint8_t*).

Definition at line 358 of file ezradio_api_lib.c .

References ezradio_comm_WriteData() .