MSDBOT_CBW_TypeDef Struct ReferenceKit Drivers > Msd
Bulk Only Transport (BOT) Command Block Wrapper (CBW) typedef.
       Definition at line
       
        51
       
       of file
       
        msdbot.h
       
       .
      
      
       #include <
       
     
        msdbot.h
       
       >
      
| Data Fields | |
| union { | |
| struct { | |
| uint8_t CBLength : 5 | |
| uint8_t Reserved3 : 3 | |
| } | |
| uint8_t bCBWCBLength | |
| }; | |
| union { | |
| struct { | |
| uint8_t Direction : 1 | |
| uint8_t Obsolete : 1 | |
| uint8_t Reserved1 : 6 | |
| } | |
| uint8_t bmCBWFlags | |
| }; | |
| union { | |
| struct { | |
| uint8_t Lun : 4 | |
| uint8_t Reserved2 : 4 | |
| } | |
| uint8_t bCBWLUN | |
| }; | |
| uint8_t | CBWCB [16] | 
| uint32_t | dCBWDataTransferLength | 
| uint32_t | dCBWSignature | 
| uint32_t | dCBWTag | 
Field Documentation
| uint8_t MSDBOT_CBW_TypeDef::bCBWCBLength | 
SCSI CDB length.
        Definition at line
        
         75
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::bmCBWFlags | 
CBW Flags.
        Definition at line
        
         61
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::CBLength | 
SCSI CDB length.
        Definition at line
        
         72
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::CBWCB[16] | 
| uint32_t MSDBOT_CBW_TypeDef::dCBWDataTransferLength | 
| uint32_t MSDBOT_CBW_TypeDef::dCBWSignature | 
The CBW signature (ascii USBC).
        Definition at line
        
         52
        
        of file
        
         msdbot.h
        
        .
       
| uint32_t MSDBOT_CBW_TypeDef::dCBWTag | 
The CBW tag.
        Definition at line
        
         53
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::Direction | 
BOT transfer directon, 1=BOT IN
        Definition at line
        
         59
        
        of file
        
         msdbot.h
        
        .
       
Referenced by MSDBOT_Xfer() .
| uint8_t MSDBOT_CBW_TypeDef::Lun | 
Device Logical Unit Number.
        Definition at line
        
         65
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::Obsolete | 
Obsolete, expect 0.
        Definition at line
        
         58
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::Reserved1 | 
Reserved, expect 0.
        Definition at line
        
         57
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::Reserved2 | 
Reserved, expect 0.
        Definition at line
        
         66
        
        of file
        
         msdbot.h
        
        .
       
| uint8_t MSDBOT_CBW_TypeDef::Reserved3 | 
Reserved, expect 0.
        Definition at line
        
         73
        
        of file
        
         msdbot.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       msdbot.h