LESENSE_CH_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_CH LESENSE CH Register

.

Definition at line 47 of file efr32fg13p_lesense_ch.h.

#include <efr32fg13p_lesense_ch.h>

Data Fields

__IOM uint32_t EVAL
 
__IOM uint32_t INTERACT
 
uint32_t RESERVED0 [1]
 
__IOM uint32_t TIMING
 

Field Documentation

__IOM uint32_t LESENSE_CH_TypeDef::EVAL

Scan Configuration

Definition at line 50 of file efr32fg13p_lesense_ch.h.

Referenced by LESENSE_ChannelSlidingWindow(), and LESENSE_ChannelStepDetection().

__IOM uint32_t LESENSE_CH_TypeDef::INTERACT

Scan Configuration

Definition at line 49 of file efr32fg13p_lesense_ch.h.

uint32_t LESENSE_CH_TypeDef::RESERVED0[1]

Reserved future

Definition at line 51 of file efr32fg13p_lesense_ch.h.

__IOM uint32_t LESENSE_CH_TypeDef::TIMING

Scan Configuration

Definition at line 48 of file efr32fg13p_lesense_ch.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG13P/Include/efr32fg13p_lesense_ch.h