EMU_DCDCInit_TypeDef Struct ReferenceEMLIB > EMU
DCDC initialization structure.
       Definition at line
       
        572
       
       of file
       
        em_emu.h
       
       .
      
      
       #include <
       
     
        em_emu.h
       
       >
      
Field Documentation
| EMU_DcdcAnaPeripheralPower_TypeDef EMU_DCDCInit_TypeDef::anaPeripheralPower | 
Select analog peripheral power in DCDC-to-DVDD mode.
        Definition at line
        
         589
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| EMU_DcdcLnCompCtrl_TypeDef EMU_DCDCInit_TypeDef::dcdcLnCompCtrl | 
DCDC Low-noise mode compensator control.
        Definition at line
        
         596
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::dcdcMode | 
DCDC regulator operating mode in EM0/1.
        Definition at line
        
         575
        
        of file
        
         em_emu.h
        
        .
       
Referenced by BSP_initDcdc() , and EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::em01LoadCurrent_mA | 
Estimated average load current in EM0/1. (mA). This estimate is also used for EM1 optimization; if EM1 current is expected to be higher than EM0, then this parameter should hold the higher EM1 current.
        Definition at line
        
         577
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::em234LoadCurrent_uA | 
Estimated average load current in EM2 (uA). This estimate is also used for EM3 and 4 optimization; if EM3 or 4 current is expected to be higher than EM2, then this parameter should hold the higher EM3 or 4 current.
        Definition at line
        
         581
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::maxCurrent_mA | 
Maximum average DCDC output current (mA). This can be set to the maximum for the power source, for example the maximum for a battery.
        Definition at line
        
         585
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::mVout | 
Target output voltage (mV).
        Definition at line
        
         576
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| EMU_PowerConfig_TypeDef EMU_DCDCInit_TypeDef::powerConfig | 
Device external power configuration. emuPowerConfig_DcdcToDvdd is currently the only supported mode.
        Definition at line
        
         573
        
        of file
        
         em_emu.h
        
        .
       
| EMU_DcdcLnReverseCurrentControl_TypeDef EMU_DCDCInit_TypeDef::reverseCurrentControl | 
Low-noise reverse current control. NOTE: this parameter uses special encoding: >= 0 is forced CCM mode where the parameter is used as the reverse current threshold in mA. -1 is encoded as emuDcdcLnHighEfficiencyMode (EFM32 only).
        Definition at line
        
         591
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_emu.h