HALL - Hall Effect SensorBSP > Thunderboard Sense BSP
Detailed Description
Driver for Hall effect sensor.
| Modules | |
| Si7210 - Hall Effect Sensor | |
| Driver for the Silicon Labs Si7210 Hall effect sensor. | |
| Data Structures | |
| struct | __HALL_Config | 
| Structure to configure the Hall effect sensor device. | |
| Typedefs | |
| typedef struct __HALL_Config | HALL_Config | 
| Structure to configure the Hall effect sensor device. | |
| typedef void(* | HALL_IntCallback ) (bool pinHigh) | 
| Functions | |
| uint32_t | HALL_configure ( HALL_Config *config) | 
| Configures the Si7210 chip. | |
| void | HALL_deInit (void) | 
| De-initializes the Hall sensor. Disables the sensor power domain. | |
| uint32_t | HALL_deInitDevice (void) | 
| Does device-specific de-initializaiton for the Si7210 chip. | |
| float | HALL_getTamperLevel (void) | 
| Returns the tamper level configured in the chip. | |
| uint32_t | HALL_init (void) | 
| Initializes the Hall sensor. | |
| uint32_t | HALL_initDevice (void) | 
| Does device-specific initializaiton for the Si7210 chip. | |
| uint32_t | HALL_measure (uint32_t scale, float *result) | 
| Performs a measurement. | |
| void | HALL_registerCallback ( HALL_IntCallback callback) | 
| Register GPIO interrupt callback function. This function will be called when the ALERT pin of the Hall sensor changes state and the interrupt functions are enabled. | |
| Error Codes | |
| #define | HALL_OK 0x0000 | 
| #define | HALL_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
| #define | HALL_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
| #define | HALL_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
| Configuration values | |
| #define | HALL_CONFIG_POLARITY_OMNIPOLAR 0x00 | 
| #define | HALL_CONFIG_POLARITY_NEGATIVE 0x01 | 
| #define | HALL_CONFIG_POLARITY_POSITIVE 0x02 | 
Macro Definition Documentation
| #define HALL_CONFIG_POLARITY_NEGATIVE 0x01 | 
Negative field polarity
        Definition at line
        
         44
        
        of file
        
         hall.h
        
        .
       
| #define HALL_CONFIG_POLARITY_OMNIPOLAR 0x00 | 
Omnipolar field polarity
        Definition at line
        
         43
        
        of file
        
         hall.h
        
        .
       
| #define HALL_CONFIG_POLARITY_POSITIVE 0x02 | 
Positive field polarity
        Definition at line
        
         45
        
        of file
        
         hall.h
        
        .
       
| #define HALL_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
The device ID does not match the expected value
        Definition at line
        
         36
        
        of file
        
         hall.h
        
        .
       
Referenced by HALL_initDevice() .
| #define HALL_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
The driver is not initialized
        Definition at line
        
         34
        
        of file
        
         hall.h
        
        .
       
| #define HALL_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
I2C transaction failed
        Definition at line
        
         35
        
        of file
        
         hall.h
        
        .
       
Referenced by SI7210_registerRead() , SI7210_registerWrite() , and SI7210_wakeUp() .
| #define HALL_OK 0x0000 | 
No errors
        Definition at line
        
         33
        
        of file
        
         hall.h
        
        .
       
Referenced by HALL_configure() , HALL_initDevice() , SI7210_loadCoeffsFromOtp() , SI7210_regClearBits() , SI7210_registerRead() , SI7210_registerWrite() , SI7210_regReadOTP() , SI7210_regSetBits() , and SI7210_wakeUp() .
Typedef Documentation
| typedef void(* HALL_IntCallback) (bool pinHigh) | 
Interrupt callback function
        Definition at line
        
         59
        
        of file
        
         hall.h
        
        .
       
Function Documentation
| uint32_t HALL_configure | ( | HALL_Config * | 
            config
            | ) | 
Configures the Si7210 chip.
- Parameters
- 
         [in] configThe structure, which contains the configuration parameters. If all fields are set to zero, the chip will revert to use default values. 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         105
        
        of file
        
         hall_si7210.c
        
        .
       
References HALL_OK , __HALL_Config::hysteresis , __HALL_Config::outputInvert , __HALL_Config::polarity , SI7210_calculateSWHYST() , SI7210_calculateSWOP() , SI7210_REG_ADDR_CTRL1 , SI7210_REG_ADDR_CTRL2 , SI7210_REG_ADDR_CTRL3 , SI7210_REG_ADDR_POWER_CTRL , SI7210_REG_CTRL1_SW_LOW4FIELD_MASK , SI7210_REG_CTRL1_SW_LOW4FIELD_SHIFT , SI7210_REG_CTRL1_SW_OP_MASK , SI7210_REG_CTRL1_SW_OP_SHIFT , SI7210_REG_CTRL2_SW_FIELDPOLSEL_MASK , SI7210_REG_CTRL2_SW_FIELDPOLSEL_SHIFT , SI7210_REG_CTRL2_SW_HYST_MASK , SI7210_REG_CTRL2_SW_HYST_SHIFT , SI7210_REG_CTRL3_SLTIMEENA_MASK , SI7210_REG_POWER_CTRL_STOP_MASK , SI7210_REG_POWER_CTRL_USESTORE_MASK , SI7210_regClearBits() , SI7210_registerWrite() , SI7210_regSetBits() , SI7210_wakeUp() , and __HALL_Config::threshold .
| void HALL_deInit | ( | void | 
            | ) | 
De-initializes the Hall sensor. Disables the sensor power domain.
- Returns
- None
        Definition at line
        
         82
        
        of file
        
         hall.c
        
        .
       
References BOARD_hallSensorEnable() , BOARD_hallSensorEnableIRQ() , and HALL_deInitDevice() .
| uint32_t HALL_deInitDevice | ( | void | 
            | ) | 
Does device-specific de-initializaiton for the Si7210 chip.
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         89
        
        of file
        
         hall_si7210.c
        
        .
       
Referenced by HALL_deInit() .
| float HALL_getTamperLevel | ( | void | 
            | ) | 
Returns the tamper level configured in the chip.
- Returns
- The tamper level in mT
        Definition at line
        
         228
        
        of file
        
         hall_si7210.c
        
        .
       
| uint32_t HALL_init | ( | void | 
            | ) | 
Initializes the Hall sensor.
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         54
        
        of file
        
         hall.c
        
        .
       
References BOARD_hallSensorEnable() , BOARD_hallSensorEnableIRQ() , BOARD_hallSensorSetIRQCallback() , HALL_initDevice() , and UTIL_delay() .
| uint32_t HALL_initDevice | ( | void | 
            | ) | 
Does device-specific initializaiton for the Si7210 chip.
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         56
        
        of file
        
         hall_si7210.c
        
        .
       
References HALL_ERROR_DEVICE_ID_MISMATCH , HALL_OK , SI7210_identify() , and SI7210_wakeUp() .
Referenced by HALL_init() .
| uint32_t HALL_measure | ( | uint32_t | 
            scale,
            | 
| float * | 
            result
            | ||
| ) | 
Performs a measurement.
- Parameters
- 
         [in] scaleDesired scale in uT [out] resultThe measured field strength value in mT 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         202
        
        of file
        
         hall_si7210.c
        
        .
       
References SI7210_readmTDataSltimeena() .
| void HALL_registerCallback | ( | HALL_IntCallback | 
            callback
            | ) | 
Register GPIO interrupt callback function. This function will be called when the ALERT pin of the Hall sensor changes state and the interrupt functions are enabled.
- Parameters
- 
         [in] callbackPointer to the callback function 
- Returns
- None
        Definition at line
        
         105
        
        of file
        
         hall.c
        
        .