LEUART_TypeDef Struct ReferenceDevices > LEUART

LEUART Register Declaration

Definition at line 49 of file efr32fg13p_leuart.h.

#include <efr32fg13p_leuart.h>

Data Fields

__IOM uint32_t CLKDIV
 
__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t FREEZE
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t INPUT
 
__IOM uint32_t PULSECTRL
 
uint32_t RESERVED0 [3]
 
uint32_t RESERVED1 [2]
 
__IOM uint32_t ROUTELOC0
 
__IOM uint32_t ROUTEPEN
 
__IM uint32_t RXDATA
 
__IM uint32_t RXDATAX
 
__IM uint32_t RXDATAXP
 
__IOM uint32_t SIGFRAME
 
__IOM uint32_t STARTFRAME
 
__IM uint32_t STATUS
 
__IM uint32_t SYNCBUSY
 
__IOM uint32_t TXDATA
 
__IOM uint32_t TXDATAX
 

Field Documentation

__IOM uint32_t LEUART_TypeDef::CLKDIV

Clock Control Register

Definition at line 53 of file efr32fg13p_leuart.h.

Referenced by LEUART_BaudrateGet(), LEUART_BaudrateSet(), and LEUART_Reset().

__IOM uint32_t LEUART_TypeDef::CMD

Command Register

Definition at line 51 of file efr32fg13p_leuart.h.

Referenced by LEUART_Enable(), LEUART_Init(), LEUART_Reset(), LEUART_RxDmaInEM2Enable(), LEUART_TxDmaInEM2Enable(), and UARTDRV_InitLeuart().

__IOM uint32_t LEUART_TypeDef::CTRL

Control Register

Definition at line 50 of file efr32fg13p_leuart.h.

Referenced by LEUART_Init(), LEUART_Reset(), LEUART_RxDmaInEM2Enable(), and LEUART_TxDmaInEM2Enable().

__IOM uint32_t LEUART_TypeDef::FREEZE

Freeze Register

Definition at line 67 of file efr32fg13p_leuart.h.

Referenced by LEUART_FreezeEnable().

__IOM uint32_t LEUART_TypeDef::IEN

Interrupt Enable Register

Definition at line 64 of file efr32fg13p_leuart.h.

Referenced by LEUART_IntDisable(), LEUART_IntEnable(), LEUART_IntGetEnabled(), and LEUART_Reset().

__IM uint32_t LEUART_TypeDef::IF

Interrupt Flag Register

Definition at line 61 of file efr32fg13p_leuart.h.

Referenced by LEUART_IntGet(), and LEUART_IntGetEnabled().

__IOM uint32_t LEUART_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 63 of file efr32fg13p_leuart.h.

Referenced by LEUART_IntClear(), and LEUART_Reset().

__IOM uint32_t LEUART_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 62 of file efr32fg13p_leuart.h.

Referenced by LEUART_IntSet().

__IOM uint32_t LEUART_TypeDef::INPUT

LEUART Input Register

Definition at line 74 of file efr32fg13p_leuart.h.

__IOM uint32_t LEUART_TypeDef::PULSECTRL

Pulse Control Register

Definition at line 65 of file efr32fg13p_leuart.h.

Referenced by LEUART_Reset().

uint32_t LEUART_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 70 of file efr32fg13p_leuart.h.

uint32_t LEUART_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 73 of file efr32fg13p_leuart.h.

__IOM uint32_t LEUART_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 72 of file efr32fg13p_leuart.h.

Referenced by LEUART_Reset(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().

__IOM uint32_t LEUART_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 71 of file efr32fg13p_leuart.h.

Referenced by LEUART_Reset(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().

__IM uint32_t LEUART_TypeDef::RXDATA

Receive Buffer Data Register

Definition at line 57 of file efr32fg13p_leuart.h.

Referenced by LEUART_Rx(), and LEUART_RxDataGet().

__IM uint32_t LEUART_TypeDef::RXDATAX

Receive Buffer Data Extended Register

Definition at line 56 of file efr32fg13p_leuart.h.

Referenced by LEUART_RxDataXGet(), and LEUART_RxExt().

__IM uint32_t LEUART_TypeDef::RXDATAXP

Receive Buffer Data Extended Peek Register

Definition at line 58 of file efr32fg13p_leuart.h.

__IOM uint32_t LEUART_TypeDef::SIGFRAME

Signal Frame Register

Definition at line 55 of file efr32fg13p_leuart.h.

Referenced by LEUART_Reset().

__IOM uint32_t LEUART_TypeDef::STARTFRAME

Start Frame Register

Definition at line 54 of file efr32fg13p_leuart.h.

Referenced by LEUART_Reset().

__IM uint32_t LEUART_TypeDef::STATUS

Status Register

Definition at line 52 of file efr32fg13p_leuart.h.

Referenced by LEUART_Rx(), LEUART_RxDmaInEM2Enable(), LEUART_RxExt(), LEUART_StatusGet(), LEUART_Tx(), LEUART_TxDmaInEM2Enable(), and LEUART_TxExt().

__IM uint32_t LEUART_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 68 of file efr32fg13p_leuart.h.

Referenced by LEUART_FreezeEnable(), and UARTDRV_InitLeuart().

__IOM uint32_t LEUART_TypeDef::TXDATA

Transmit Buffer Data Register

Definition at line 60 of file efr32fg13p_leuart.h.

Referenced by LEUART_Tx().

__IOM uint32_t LEUART_TypeDef::TXDATAX

Transmit Buffer Data Extended Register

Definition at line 59 of file efr32fg13p_leuart.h.

Referenced by LEUART_TxExt().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG13P/Include/efr32fg13p_leuart.h