LESENSE_DecCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE decoder control descriptor structure.
       Definition at line
       
        670
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
| Data Fields | |
| bool | chkState | 
| LESENSE_DecInput_TypeDef | decInput | 
| bool | hystIRQ | 
| bool | hystPRS0 | 
| bool | hystPRS1 | 
| bool | hystPRS2 | 
| uint32_t | initState | 
| bool | intMap | 
| LESENSE_PRSSel_TypeDef | prsChSel0 | 
| LESENSE_PRSSel_TypeDef | prsChSel1 | 
| LESENSE_PRSSel_TypeDef | prsChSel2 | 
| LESENSE_PRSSel_TypeDef | prsChSel3 | 
| bool | prsCount | 
Field Documentation
| bool LESENSE_DecCtrlDesc_TypeDef::chkState | 
Set to enable decoder to check the present state in addition to the states defined in TCONF.
        Definition at line
        
         679
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput | 
Select input to the LESENSE decoder.
        Definition at line
        
         672
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ | 
Set to enable hysteresis in decoder for suppressing the interrupt requests.
        Definition at line
        
         699
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.
        Definition at line
        
         687
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.
        Definition at line
        
         691
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2 | 
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.
        Definition at line
        
         695
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| uint32_t LESENSE_DecCtrlDesc_TypeDef::initState | 
Initial state of the LESENSE decoder.
        Definition at line
        
         675
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::intMap | 
When set, a transition from state x in decoder will set the interrupt flag CHx.
        Definition at line
        
         683
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0 | 
Select PRS channel input for bit 0 of LESENSE decoder.
        Definition at line
        
         706
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1 | 
Select PRS channel input for bit 1 of LESENSE decoder.
        Definition at line
        
         709
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2 | 
Select PRS channel input for bit 2 of LESENSE decoder.
        Definition at line
        
         712
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3 | 
Select PRS channel input for bit 3 of LESENSE decoder.
        Definition at line
        
         715
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::prsCount | 
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
        Definition at line
        
         703
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_lesense.h