MSDSCSI_RequestSense_TypeDef Struct ReferenceKit Drivers > Msd
SCSI Request Sense Command Descriptor Block (CDB) typedef.
       Definition at line
       
        126
       
       of file
       
        msdscsi.h
       
       .
      
      
       #include <
       
     
        msdscsi.h
       
       >
      
| Data Fields | |
| struct { | |
| uint8_t Desc : 1 | |
| uint8_t Reserved1 : 7 | |
| }; | |
| uint8_t | AllocationLength | 
| uint8_t | Control | 
| uint8_t | OpCode | 
| uint8_t | Reserved2 | 
| uint8_t | Reserved3 | 
Field Documentation
| uint8_t MSDSCSI_RequestSense_TypeDef::AllocationLength | 
Number of sense data bytes requested.
        Definition at line
        
         134
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::Control | 
Control byte.
        Definition at line
        
         135
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::Desc | 
Descriptor format.
        Definition at line
        
         129
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::OpCode | 
Command opcode.
        Definition at line
        
         127
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::Reserved1 | 
Reserved, expect 0.
        Definition at line
        
         130
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::Reserved2 | 
Reserved, expect 0.
        Definition at line
        
         132
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSense_TypeDef::Reserved3 | 
Reserved, expect 0.
        Definition at line
        
         133
        
        of file
        
         msdscsi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       msdscsi.h