IDAC_Init_TypeDef Struct ReferenceEMLIB > IDAC

IDAC initialization structure, common for both channels.

Definition at line 167 of file em_idac.h .

#include < em_idac.h >

Data Fields

bool enable
IDAC_OutMode_TypeDef outMode
bool prsEnable
IDAC_PRSSEL_TypeDef prsSel
bool sinkEnable

Field Documentation

bool IDAC_Init_TypeDef::enable

Enable IDAC.

Definition at line 169 of file em_idac.h .

Referenced by IDAC_Init() .

IDAC_OutMode_TypeDef IDAC_Init_TypeDef::outMode

Output mode

Definition at line 172 of file em_idac.h .

Referenced by IDAC_Init() .

bool IDAC_Init_TypeDef::prsEnable

Enables Peripheral reflex system (PRS) to control IDAC output. If false, IDAC output is controlled by writing to IDAC_OUTEN in IDAC_CTRL or by calling IDAC_OutEnable() .

Definition at line 179 of file em_idac.h .

Referenced by IDAC_Init() .

IDAC_PRSSEL_TypeDef IDAC_Init_TypeDef::prsSel

Peripheral reflex system channel selection. Only applicable if prsEnable is enabled.

Definition at line 185 of file em_idac.h .

Referenced by IDAC_Init() .

bool IDAC_Init_TypeDef::sinkEnable

Enable/disable current sink mode.

Definition at line 188 of file em_idac.h .

Referenced by IDAC_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_idac.h