RTCCEMLIB

Detailed Description

Real Time Counter (RTCC) Peripheral API.

This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.

Data Structures

struct RTCC_CCChConf_TypeDef
struct RTCC_Init_TypeDef

Macros

#define RTCC_CH_INIT_CAPTURE_DEFAULT
#define RTCC_CH_INIT_COMPARE_DEFAULT
#define RTCC_CH_VALID (ch)    ( (ch) < 3)
#define RTCC_INIT_DEFAULT

Enumerations

enum RTCC_CapComChMode_TypeDef {
rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF,
rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE,
rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE
}
enum RTCC_CntMode_TypeDef {
rtccCntModeNormal = _RTCC_CTRL_CNTMODE_NORMAL,
rtccCntModeCalendar = _RTCC_CTRL_CNTMODE_CALENDAR
}
enum RTCC_CntPresc_TypeDef {
rtccCntPresc_1 = _RTCC_CTRL_CNTPRESC_DIV1,
rtccCntPresc_2 = _RTCC_CTRL_CNTPRESC_DIV2,
rtccCntPresc_4 = _RTCC_CTRL_CNTPRESC_DIV4,
rtccCntPresc_8 = _RTCC_CTRL_CNTPRESC_DIV8,
rtccCntPresc_16 = _RTCC_CTRL_CNTPRESC_DIV16,
rtccCntPresc_32 = _RTCC_CTRL_CNTPRESC_DIV32,
rtccCntPresc_64 = _RTCC_CTRL_CNTPRESC_DIV64,
rtccCntPresc_128 = _RTCC_CTRL_CNTPRESC_DIV128,
rtccCntPresc_256 = _RTCC_CTRL_CNTPRESC_DIV256,
rtccCntPresc_512 = _RTCC_CTRL_CNTPRESC_DIV512,
rtccCntPresc_1024 = _RTCC_CTRL_CNTPRESC_DIV1024,
rtccCntPresc_2048 = _RTCC_CTRL_CNTPRESC_DIV2048,
rtccCntPresc_4096 = _RTCC_CTRL_CNTPRESC_DIV4096,
rtccCntPresc_8192 = _RTCC_CTRL_CNTPRESC_DIV8192,
rtccCntPresc_16384 = _RTCC_CTRL_CNTPRESC_DIV16384,
rtccCntPresc_32768 = _RTCC_CTRL_CNTPRESC_DIV32768
}
enum RTCC_CompBase_TypeDef {
rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT,
rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT
}
enum RTCC_CompMatchOutAction_TypeDef {
rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE,
rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE,
rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR,
rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET
}
enum RTCC_DayCompareMode_TypeDef {
rtccDayCompareModeMonth = _RTCC_CC_CTRL_DAYCC_MONTH,
rtccDayCompareModeWeek = _RTCC_CC_CTRL_DAYCC_WEEK
}
enum RTCC_InEdgeSel_TypeDef {
rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING,
rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING,
rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH,
rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE
}
enum RTCC_PrescMode_TypeDef {
rtccCntTickPresc = _RTCC_CTRL_CNTTICK_PRESC,
rtccCntTickCCV0Match = _RTCC_CTRL_CNTTICK_CCV0MATCH
}
enum RTCC_PRSSel_TypeDef {
rtccPRSCh0 = _RTCC_CC_CTRL_PRSSEL_PRSCH0,
rtccPRSCh1 = _RTCC_CC_CTRL_PRSSEL_PRSCH1,
rtccPRSCh2 = _RTCC_CC_CTRL_PRSSEL_PRSCH2,
rtccPRSCh3 = _RTCC_CC_CTRL_PRSSEL_PRSCH3,
rtccPRSCh4 = _RTCC_CC_CTRL_PRSSEL_PRSCH4,
rtccPRSCh5 = _RTCC_CC_CTRL_PRSSEL_PRSCH5,
rtccPRSCh6 = _RTCC_CC_CTRL_PRSSEL_PRSCH6,
rtccPRSCh7 = _RTCC_CC_CTRL_PRSSEL_PRSCH7,
rtccPRSCh8 = _RTCC_CC_CTRL_PRSSEL_PRSCH8,
rtccPRSCh9 = _RTCC_CC_CTRL_PRSSEL_PRSCH9,
rtccPRSCh10 = _RTCC_CC_CTRL_PRSSEL_PRSCH10,
rtccPRSCh11 = _RTCC_CC_CTRL_PRSSEL_PRSCH11
}

Functions

__STATIC_INLINE uint32_t RTCC_ChannelCCVGet (int ch)
Get RTCC capture/compare register value (CCV) for selected channel.
__STATIC_INLINE void RTCC_ChannelCCVSet (int ch, uint32_t value)
Set RTCC capture/compare register value (CCV) for selected channel.
__STATIC_INLINE uint32_t RTCC_ChannelDateGet (int ch)
Get the calendar DATE register content for selected channel.
__STATIC_INLINE void RTCC_ChannelDateSet (int ch, uint32_t date)
Set calendar DATE register for selected channel.
void RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr)
Configure the selected capture/compare channel of the RTCC.
__STATIC_INLINE uint32_t RTCC_ChannelTimeGet (int ch)
Get calendar TIME register content for selected channel.
__STATIC_INLINE void RTCC_ChannelTimeSet (int ch, uint32_t time)
Set calendar TIME register for selected channel.
__STATIC_INLINE uint32_t RTCC_CombinedCounterGet (void)
Get combined CNT/PRECNT register content.
__STATIC_INLINE uint32_t RTCC_CounterGet (void)
Get RTCC counter value.
__STATIC_INLINE void RTCC_CounterSet (uint32_t value)
Set RTCC CNT counter.
__STATIC_INLINE uint32_t RTCC_DateGet (void)
Get DATE register value.
__STATIC_INLINE void RTCC_DateSet (uint32_t date)
Set RTCC DATE register.
__STATIC_INLINE void RTCC_EM4WakeupEnable (bool enable)
Enable/disable EM4 wakeup capability.
void RTCC_Enable (bool enable)
Enable/disable RTCC.
void RTCC_Init (const RTCC_Init_TypeDef *init)
Initialize RTCC.
__STATIC_INLINE void RTCC_IntClear (uint32_t flags)
Clear one or more pending RTCC interrupts.
__STATIC_INLINE void RTCC_IntDisable (uint32_t flags)
Disable one or more RTCC interrupts.
__STATIC_INLINE void RTCC_IntEnable (uint32_t flags)
Enable one or more RTCC interrupts.
__STATIC_INLINE uint32_t RTCC_IntGet (void)
Get pending RTCC interrupt flags.
__STATIC_INLINE uint32_t RTCC_IntGetEnabled (void)
Get enabled and pending RTCC interrupt flags.
__STATIC_INLINE void RTCC_IntSet (uint32_t flags)
Set one or more pending RTCC interrupts from SW.
__STATIC_INLINE void RTCC_Lock (void)
Lock RTCC registers.
__STATIC_INLINE uint32_t RTCC_PreCounterGet (void)
Get RTCC pre-counter value.
__STATIC_INLINE void RTCC_PreCounterSet (uint32_t preCntVal)
Set RTCC pre-counter value.
void RTCC_Reset (void)
Restore RTCC to its reset state.
__STATIC_INLINE void RTCC_RetentionRamPowerDown (void)
Power down retention RAM.
void RTCC_StatusClear (void)
Clear the STATUS register.
__STATIC_INLINE uint32_t RTCC_StatusGet (void)
Get STATUS register value.
__STATIC_INLINE uint32_t RTCC_TimeGet (void)
Get TIME register value.
__STATIC_INLINE void RTCC_TimeSet (uint32_t time)
Set RTCC TIME register.
__STATIC_INLINE void RTCC_Unlock (void)
Unlock RTCC registers.

Macro Definition Documentation

#define RTCC_CH_INIT_CAPTURE_DEFAULT
Value:
{ \
rtccCapComChModeCapture, /* Select input capture mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on capture. */ \
rtccPRSCh0, /* PRS channel 0. */ \
rtccInEdgeRising, /* Rising edge detection. */ \
rtccCompBaseCnt, /* Don't care. */ \
0, /* Don't care. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel input capture initialization structure.

Definition at line 292 of file em_rtcc.h .

#define RTCC_CH_INIT_COMPARE_DEFAULT
Value:
{ \
rtccCapComChModeCompare, /* Select output compare mode. */ \
rtccCompMatchOutActionPulse, /* Create pulse on compare match.*/ \
rtccPRSCh0, /* PRS channel 0 (not used). */ \
rtccInEdgeNone, /* No edge detection. */ \
rtccCompBaseCnt, /* Counter comparison base. */ \
0, /* No compare mask bits set. */ \
rtccDayCompareModeMonth /* Don't care */ \
}

Default RTCC channel output compare initialization structure.

Definition at line 280 of file em_rtcc.h .

#define RTCC_CH_VALID ( ch ) ( (ch) < 3)

Validation of valid RTCC channel for assert statements.

Definition at line 304 of file em_rtcc.h .

Referenced by RTCC_ChannelCCVGet() , RTCC_ChannelCCVSet() , RTCC_ChannelDateGet() , RTCC_ChannelDateSet() , RTCC_ChannelInit() , RTCC_ChannelTimeGet() , and RTCC_ChannelTimeSet() .

#define RTCC_INIT_DEFAULT
Value:
{ \
true, /* Start counting when initialization is done. */ \
false, /* Disable RTCC during debug halt. */ \
false, /* Disable pre-counter wrap on ch. 0 CCV value. */ \
false, /* Disable counter wrap on ch. 1 CCV value. */ \
rtccCntPresc_32, /* 977 us per tick. */ \
rtccCntTickPresc, /* Counter increments according to prescaler value.*/ \
false, /* No RTCC oscillator failure detection. */ \
rtccCntModeNormal, /* Normal RTCC mode. */ \
false, /* No leap year correction. */ \
}

Default RTCC initialization structure.

Definition at line 265 of file em_rtcc.h .

Referenced by UDELAY_Calibrate() .

Enumeration Type Documentation

Capture/Compare channel mode.

Enumerator
rtccCapComChModeOff

Capture/Compare channel turned off.

rtccCapComChModeCapture

Capture mode.

rtccCapComChModeCompare

Compare mode.

Definition at line 116 of file em_rtcc.h .

Operational mode of the counter.

Enumerator
rtccCntModeNormal

Normal counter mode. The counter is incremented by 1 for each tick.

rtccCntModeCalendar

Calendar mode. Refer to the RTCC chapter of the Reference Manual for more details on the calendar mode.

Definition at line 76 of file em_rtcc.h .

Counter prescaler selection.

Enumerator
rtccCntPresc_1

Divide clock by 1.

rtccCntPresc_2

Divide clock by 2.

rtccCntPresc_4

Divide clock by 4.

rtccCntPresc_8

Divide clock by 8.

rtccCntPresc_16

Divide clock by 16.

rtccCntPresc_32

Divide clock by 32.

rtccCntPresc_64

Divide clock by 64.

rtccCntPresc_128

Divide clock by 128.

rtccCntPresc_256

Divide clock by 256.

rtccCntPresc_512

Divide clock by 512.

rtccCntPresc_1024

Divide clock by 1024.

rtccCntPresc_2048

Divide clock by 2048.

rtccCntPresc_4096

Divide clock by 4096.

rtccCntPresc_8192

Divide clock by 8192.

rtccCntPresc_16384

Divide clock by 16384.

rtccCntPresc_32768

Divide clock by 32768.

Definition at line 86 of file em_rtcc.h .

Capture/Compare channel compare mode.

Enumerator
rtccCompBaseCnt

CCVx is compared with the CNT register.

rtccCompBasePreCnt

CCVx is compared with a CNT[16:0] and PRECNT[14:0].

Definition at line 163 of file em_rtcc.h .

Compare match output action mode.

Enumerator
rtccCompMatchOutActionPulse

Generate a pulse.

rtccCompMatchOutActionToggle

Toggle output.

rtccCompMatchOutActionClear

Clear output.

rtccCompMatchOutActionSet

Set output.

Definition at line 123 of file em_rtcc.h .

Day compare mode.

Enumerator
rtccDayCompareModeMonth

Day of month is selected for Capture/Compare.

rtccDayCompareModeWeek

Day of week is selected for Capture/Compare.

Definition at line 172 of file em_rtcc.h .

Input edge select.

Enumerator
rtccInEdgeRising

Rising edges detected.

rtccInEdgeFalling

Falling edges detected.

rtccInEdgeBoth

Both edges detected.

rtccInEdgeNone

No edge detection, signal is left as is.

Definition at line 155 of file em_rtcc.h .

Prescaler mode of the RTCC counter.

Enumerator
rtccCntTickPresc

CNT register ticks according to prescaler value.

rtccCntTickCCV0Match

CNT register ticks when PRECNT matches the 15 least significant bits of ch. 0 CCV register.

Definition at line 106 of file em_rtcc.h .

PRS input sources.

Enumerator
rtccPRSCh0

PRS channel 0.

rtccPRSCh1

PRS channel 1.

rtccPRSCh2

PRS channel 2.

rtccPRSCh3

PRS channel 3.

rtccPRSCh4

PRS channel 4.

rtccPRSCh5

PRS channel 5.

rtccPRSCh6

PRS channel 6.

rtccPRSCh7

PRS channel 7.

rtccPRSCh8

PRS channel 8.

rtccPRSCh9

PRS channel 9.

rtccPRSCh10

PRS channel 10.

rtccPRSCh11

PRS channel 11.

Definition at line 131 of file em_rtcc.h .

Function Documentation

__STATIC_INLINE uint32_t RTCC_ChannelCCVGet ( int ch )

Get RTCC capture/compare register value (CCV) for selected channel.

Parameters
[in] ch Channel selector.
Returns
Capture/compare register value.

Definition at line 320 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

__STATIC_INLINE void RTCC_ChannelCCVSet ( int ch,
uint32_t value
)

Set RTCC capture/compare register value (CCV) for selected channel.

Parameters
[in] ch Channel selector.
[in] value CCV value.

Definition at line 336 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

__STATIC_INLINE uint32_t RTCC_ChannelDateGet ( int ch )

Get the calendar DATE register content for selected channel.

Parameters
[in] ch Channel selector.
Returns
DATE register value.

Definition at line 352 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

__STATIC_INLINE void RTCC_ChannelDateSet ( int ch,
uint32_t date
)

Set calendar DATE register for selected channel.

Parameters
[in] ch Channel selector.
[in] date DATE value.

Definition at line 368 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

void RTCC_ChannelInit ( int ch,
RTCC_CCChConf_TypeDef const * confPtr
)

Configure the selected capture/compare channel of the RTCC.

Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.

Parameters
[in] ch A channel selector.
[in] confPtr A pointer to the configuration structure.

Configure the selected capture/compare channel.

Definition at line 81 of file em_rtcc.c .

References _RTCC_CC_CTRL_CMOA_SHIFT , _RTCC_CC_CTRL_COMPBASE_SHIFT , _RTCC_CC_CTRL_COMPMASK_MASK , _RTCC_CC_CTRL_COMPMASK_SHIFT , _RTCC_CC_CTRL_DAYCC_SHIFT , _RTCC_CC_CTRL_ICEDGE_SHIFT , _RTCC_CC_CTRL_MODE_SHIFT , _RTCC_CC_CTRL_PRSSEL_SHIFT , RTCC_CCChConf_TypeDef::chMode , RTCC_CCChConf_TypeDef::compBase , RTCC_CCChConf_TypeDef::compMask , RTCC_CCChConf_TypeDef::compMatchOutAction , RTCC_CCChConf_TypeDef::dayCompMode , RTCC_CCChConf_TypeDef::inputEdgeSel , RTCC_CCChConf_TypeDef::prsSel , RTCC , and RTCC_CH_VALID .

Referenced by RTCDRV_Init() .

__STATIC_INLINE uint32_t RTCC_ChannelTimeGet ( int ch )

Get calendar TIME register content for selected channel.

Parameters
[in] ch Channel selector.
Returns
TIME register value.

Definition at line 386 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

__STATIC_INLINE void RTCC_ChannelTimeSet ( int ch,
uint32_t time
)

Set calendar TIME register for selected channel.

Parameters
[in] ch Channel selector.
[in] time TIME value.

Definition at line 402 of file em_rtcc.h .

References RTCC , and RTCC_CH_VALID .

__STATIC_INLINE uint32_t RTCC_CombinedCounterGet ( void )

Get combined CNT/PRECNT register content.

Returns
CNT/PRECNT register value.

Definition at line 415 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE uint32_t RTCC_CounterGet ( void )

Get RTCC counter value.

Returns
Current RTCC counter value.

Definition at line 427 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_CounterSet ( uint32_t value )

Set RTCC CNT counter.

Parameters
[in] value CNT value.

Definition at line 439 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE uint32_t RTCC_DateGet ( void )

Get DATE register value.

Returns
Current DATE register value.

Definition at line 451 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_DateSet ( uint32_t date )

Set RTCC DATE register.

Parameters
[in] date DATE value.

Definition at line 463 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_EM4WakeupEnable ( bool enable )

Enable/disable EM4 wakeup capability.

Parameters
[in] enable Set to true to enable EM4 wakeup, set to false otherwise.

Definition at line 475 of file em_rtcc.h .

References RTCC , and RTCC_EM4WUEN_EM4WU .

void RTCC_Enable ( bool enable )

Enable/disable RTCC.

Parameters
[in] enable True to enable RTCC, false to disable.

Definition at line 105 of file em_rtcc.c .

References _RTCC_CTRL_ENABLE_SHIFT , BUS_RegBitWrite() , and RTCC .

Referenced by RTCDRV_DeInit() , and UDELAY_Calibrate() .

void RTCC_Init ( const RTCC_Init_TypeDef * init )

Initialize RTCC.

Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.

Parameters
[in] init A pointer to the RTCC initialization structure.

Definition at line 123 of file em_rtcc.c .

References _RTCC_CTRL_CCV1TOP_SHIFT , _RTCC_CTRL_CNTMODE_SHIFT , _RTCC_CTRL_CNTPRESC_SHIFT , _RTCC_CTRL_CNTTICK_SHIFT , _RTCC_CTRL_DEBUGRUN_SHIFT , _RTCC_CTRL_ENABLE_SHIFT , _RTCC_CTRL_LYEARCORRDIS_SHIFT , _RTCC_CTRL_OSCFDETEN_SHIFT , _RTCC_CTRL_PRECCV0TOP_SHIFT , RTCC_Init_TypeDef::cntMode , RTCC_Init_TypeDef::cntWrapOnCCV1 , RTCC_Init_TypeDef::debugRun , RTCC_Init_TypeDef::disLeapYearCorr , RTCC_Init_TypeDef::enable , RTCC_Init_TypeDef::enaOSCFailDetect , RTCC_Init_TypeDef::precntWrapOnCCV0 , RTCC_Init_TypeDef::presc , RTCC_Init_TypeDef::prescMode , and RTCC .

Referenced by RTCDRV_Init() , and UDELAY_Calibrate() .

__STATIC_INLINE void RTCC_IntClear ( uint32_t flags )

Clear one or more pending RTCC interrupts.

Parameters
[in] flags RTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.

Definition at line 496 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_IntDisable ( uint32_t flags )

Disable one or more RTCC interrupts.

Parameters
[in] flags RTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.

Definition at line 509 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_IntEnable ( uint32_t flags )

Enable one or more RTCC interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.
Parameters
[in] flags RTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.

Definition at line 527 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE uint32_t RTCC_IntGet ( void )

Get pending RTCC interrupt flags.

Note
Event bits are not cleared by using this function.
Returns
Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 543 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE uint32_t RTCC_IntGetEnabled ( void )

Get enabled and pending RTCC interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Returns
Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.

Definition at line 559 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_IntSet ( uint32_t flags )

Set one or more pending RTCC interrupts from SW.

Parameters
[in] flags RTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).

Definition at line 577 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_Lock ( void )

Lock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.

Definition at line 591 of file em_rtcc.h .

References CMU , CMU_LOCK_LOCKKEY_LOCK , CMU_LOCK_LOCKKEY_LOCKED , CMU_LOCK_LOCKKEY_UNLOCK , RTCC , and RTCC_LOCK_LOCKKEY_LOCK .

__STATIC_INLINE uint32_t RTCC_PreCounterGet ( void )

Get RTCC pre-counter value.

Returns
Current RTCC pre-counter value.

Definition at line 620 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_PreCounterSet ( uint32_t preCntVal )

Set RTCC pre-counter value.

Parameters
[in] preCntVal RTCC pre-counter value to be set.

Definition at line 632 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_RetentionRamPowerDown ( void )

Power down retention RAM.

Note
Once retention RAM is powered down, it cannot be powered up again.

Definition at line 646 of file em_rtcc.h .

References RTCC , and RTCC_POWERDOWN_RAM .

__STATIC_INLINE uint32_t RTCC_StatusGet ( void )

Get STATUS register value.

Returns
Current STATUS register value.

Definition at line 664 of file em_rtcc.h .

References RTCC , and RTCC_SYNCBUSY_CMD .

__STATIC_INLINE uint32_t RTCC_TimeGet ( void )

Get TIME register value.

Returns
Current TIME register value.

Definition at line 679 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_TimeSet ( uint32_t time )

Set RTCC TIME register.

Parameters
[in] time TIME value.

Definition at line 691 of file em_rtcc.h .

References RTCC .

__STATIC_INLINE void RTCC_Unlock ( void )

Unlock RTCC registers.

Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.

Definition at line 705 of file em_rtcc.h .

References CMU , CMU_LOCK_LOCKKEY_LOCK , CMU_LOCK_LOCKKEY_LOCKED , CMU_LOCK_LOCKKEY_UNLOCK , RTCC , and RTCC_LOCK_LOCKKEY_UNLOCK .

Referenced by RTCC_Reset() .