EZRADIODRV_AutoAckHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Auto_ACK_Plugin

EzRadio auto acknowledge plug-in instance initialization and handler structure.

Definition at line 78 of file ezradio_auto_ack_plugin.h .

#include < ezradio_auto_ack_plugin.h >

Data Fields

EZRADIODRV_AutoAckMode_t ackMode
Auto ack mode.
EZRADIODRV_PacketLengthConfig_t lenConfig
Pakcet length config for auto ack.
uint8_t * pktBuf
Pointer to the buffer that holds the auto ack packet.
uint16_t pktId
Auto ack packet ID.
EZRADIODRV_AutoAckPacketMode_t pktMode
Packet mode for aut ack.
EZRADIODRV_Callback_t userCallback
User callback.

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/ezradiodrv/plugins/inc/ ezradio_auto_ack_plugin.h