Auto_ACK_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Auto acknowledge plugin, see Plugin System Layer for detailed documentation.
.
         Data Structures | 
       |
| struct | EZRADIODRV_AutoAckHandle | 
| 
         EzRadio auto acknowledge plug-in instance initialization and handler structure.
          | 
       |
         Macros | 
       |
| #define | EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT | 
| 
         Configuration data for EzRadio auto acknowledge plug-in.
          | 
       |
         Typedefs | 
       |
| typedef struct EZRADIODRV_AutoAckHandle | EZRADIODRV_AutoAckHandle_t | 
| 
         EzRadio auto acknowledge plug-in instance initialization and handler structure.
          | 
       |
| typedef enum EZRADIODRV_AutoAckMode | EZRADIODRV_AutoAckMode_t | 
| 
         EzRadio auto acknowledge mode.
          | 
       |
| typedef enum EZRADIODRV_AutoAckPacketMode | EZRADIODRV_AutoAckPacketMode_t | 
| 
         EzRadio packet mode for auto acknowledge plug-in.
          | 
       |
         Enumerations | 
       |
| enum | 
         
          EZRADIODRV_AutoAckMode
         
         {
          ezradiodrvAutoAckDisabled = 0, ezradiodrvAutoAckImmediate = 1, ezradiodrvAutoAckSkipOne = 2 }  | 
       
| 
         EzRadio auto acknowledge mode.
          | 
       |
| enum | 
         
          EZRADIODRV_AutoAckPacketMode
         
         {
          ezradiodrvAutoAckPktDefault = 0, ezradiodrvAutoAckPktCustom = 1 }  | 
       
| 
         EzRadio packet mode for auto acknowledge plug-in.
          | 
       |
         Functions | 
       |
| void | ezradioDisableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) | 
| 
         Disables auto acknowledge sending feature.
          | 
       |
| void | ezradioEnableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) | 
| 
         Enables auto acknowledge sending feature.
          | 
       |
| void | ezradioSkipAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle) | 
| 
         Configures auto acknowledge sending feature so that there will be no acknowledge transmitted to the next received packet. This is usefull is both nodes of a link uses auto acknowledgement.
          | 
       |
Macro Definition Documentation
| #define EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio auto acknowledge plug-in.
        Definition at line
        
         92
        
        of file
        
         ezradio_auto_ack_plugin.h
        
        .
       
Enumeration Type Documentation
EzRadio auto acknowledge mode.
        Definition at line
        
         65
        
        of file
        
         ezradio_auto_ack_plugin.h
        
        .
       
EzRadio packet mode for auto acknowledge plug-in.
        Definition at line
        
         72
        
        of file
        
         ezradio_auto_ack_plugin.h
        
        .
       
Function Documentation
| void ezradioDisableAutoAck | ( | EZRADIODRV_AutoAckHandle_t * | 
           
            autoAckHandle
           
           | 
          ) | 
Disables auto acknowledge sending feature.
- Parameters
 - 
         
autoAckHandleAuto acknowledge plug-in handler.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         67
        
        of file
        
         ezradio_auto_ack_plugin.c
        
        .
       
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckDisabled .
| void ezradioEnableAutoAck | ( | EZRADIODRV_AutoAckHandle_t * | 
           
            autoAckHandle
           
           | 
          ) | 
Enables auto acknowledge sending feature.
- Parameters
 - 
         
autoAckHandleAuto acknowledge plug-in handler.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         53
        
        of file
        
         ezradio_auto_ack_plugin.c
        
        .
       
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckImmediate .
| void ezradioSkipAutoAck | ( | EZRADIODRV_AutoAckHandle_t * | 
           
            autoAckHandle
           
           | 
          ) | 
Configures auto acknowledge sending feature so that there will be no acknowledge transmitted to the next received packet. This is usefull is both nodes of a link uses auto acknowledgement.
- Parameters
 - 
         
autoAckHandleAuto acknowledge plug-in handler.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         83
        
        of file
        
         ezradio_auto_ack_plugin.c
        
        .
       
References EZRADIODRV_AutoAckHandle::ackMode , and ezradiodrvAutoAckSkipOne .