BC_TypeDef Struct ReferenceBSP > API for DKs
Board Controller Register definiton
       Definition at line
       
        53
       
       of file
       
        bsp_dk_bcreg_3201.h
       
       .
      
      
       #include <
       
     
        bsp_dk_bcreg_3201.h
       
       >
      
Field Documentation
| __IO uint16_t BC_TypeDef::ADC_READ | 
0x24 - AEM ADC SPI interface
        Definition at line
        
         73
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::ADC_STATUS | 
0x22 - AEM ADC SPI interface
        Definition at line
        
         72
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::ADC_WRITE | 
0x20 - AEM ADC SPI interface
        Definition at line
        
         71
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::ARB_CTRL | 
0x16 - Arbiter control, board control or EFM32GG access to display
        Definition at line
        
         66
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::BC_MBOX_TXCTRL | 
0x80 - BC <-> EFM32 communication channel
        Definition at line
        
         103
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::BC_MBOX_TXDATA | 
0x82
        Definition at line
        
         104
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::BC_MBOX_TXSTATUS0 | 
0x84
        Definition at line
        
         105
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::BC_MBOX_TXSTATUS1 | 
0x86
        Definition at line
        
         106
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::BUF_CTRL | 
0xc0 - Buffer Controller Control
        Definition at line
        
         117
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::CLKRST | 
0x26 - Clock and reset control
        Definition at line
        
         75
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::DISPLAY_CTRL | 
0x12 - SSD2119 TFT display control
        Definition at line
        
         64
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::EBI_CTRL | 
0x14 - Extended Address Mode control
        Definition at line
        
         65
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::EM | 
0x02 - Energy Mode indicator
        Definition at line
        
         55
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::FW_BUILDNO | 
0x2A - Firmware build number
        Definition at line
        
         78
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::FW_VERSION | 
0x2C - Firmware version
        Definition at line
        
         79
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::HW_VERSION | 
0x28 - Hardware version
        Definition at line
        
         77
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTCLEAR | 
0x44 - Interrupt clear
        Definition at line
        
         95
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTEN | 
0x42 - Interrupt Enable flags
        Definition at line
        
         94
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTFLAG | 
0x40 - Interrupt Status flags
        Definition at line
        
         93
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTPCTRL | 
0x48 - Interrupt pulse control
        Definition at line
        
         97
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTPHIGH | 
0x4C - Interrupt puls high period
        Definition at line
        
         99
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTPLOW | 
0x4A - Interrupt puls low period
        Definition at line
        
         98
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::INTSET | 
0x46 - Interrupt set
        Definition at line
        
         96
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::MAGIC | 
0x04 - Should always read 0xEF32
        Definition at line
        
         56
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::MBOX_TXCTRL | 
0xa2 - BC <-> EFM32 communication channel
        Definition at line
        
         110
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::MBOX_TXDATA | 
0xa4
        Definition at line
        
         111
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::MBOX_TXSTATUS0 | 
0xa6
        Definition at line
        
         112
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::MBOX_TXSTATUS1 | 
0xa8
        Definition at line
        
         113
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::PERICON | 
0x18 - Peripheral Control, on board switches
        Definition at line
        
         67
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::RESERVED4[0x0d] | 
0xa0 - Reserved
        Definition at line
        
         108
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::RESERVED5[0x0b] | 
0xaa - Reserved
        Definition at line
        
         115
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::RESERVERD0 | 
0x00 - Reserved
        Definition at line
        
         54
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::RESERVERD1[0x02] | 
0x1C - Reserved
        Definition at line
        
         69
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::RESERVERD3[0x19] | 
0x50 - Reserved
        Definition at line
        
         101
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_BC0 | 
0x38 - Board Control registers
        Definition at line
        
         88
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_BC1 | 
0x3A
        Definition at line
        
         89
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_BC2 | 
0x3C
        Definition at line
        
         90
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_BC3 | 
0x3E
        Definition at line
        
         91
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_COMMON | 
0x2E - Shared register between board controller and EFM32
        Definition at line
        
         81
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_EFM0 | 
0x30 - EFM32 accessible registers
        Definition at line
        
         83
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_EFM1 | 
0x32
        Definition at line
        
         84
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_EFM2 | 
0x34
        Definition at line
        
         85
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SCRATCH_EFM3 | 
0x36
        Definition at line
        
         86
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::SPI_DEMUX | 
0x1A - SPI DEMUX
        Definition at line
        
         68
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_AEM | 
0x0E - AEM button
        Definition at line
        
         62
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_CTRL | 
0x10 - CPLD control register
        Definition at line
        
         63
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_DIP | 
0x0A - DIP switch status
        Definition at line
        
         60
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_JOYSTICK | 
0x0C - Joystick presses
        Definition at line
        
         61
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_LEDS | 
0x06 - On board LEDs
        Definition at line
        
         58
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
| __IO uint16_t BC_TypeDef::UIF_PB | 
0x08 - Push button PB0-PB4 status
        Definition at line
        
         59
        
        of file
        
         bsp_dk_bcreg_3201.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/bsp/
       bsp_dk_bcreg_3201.h