WDOG_Init_TypeDef Struct ReferenceEMLIB > WDOG
Watchdog initialization structure.
       Definition at line
       
        132
       
       of file
       
        em_wdog.h
       
       .
      
      
       #include <
       
     
        em_wdog.h
       
       >
      
| Data Fields | |
| WDOG_ClkSel_TypeDef | clkSel | 
| bool | debugRun | 
| bool | em2Run | 
| bool | em3Run | 
| bool | em4Block | 
| bool | enable | 
| bool | lock | 
| WDOG_PeriodSel_TypeDef | perSel | 
| bool | resetDisable | 
| bool | swoscBlock | 
| WDOG_WarnSel_TypeDef | warnSel | 
| WDOG_WinSel_TypeDef | winSel | 
Field Documentation
| WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel | 
Clock source to use for watchdog.
        Definition at line
        
         158
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::debugRun | 
Counter keeps running during debug halt.
        Definition at line
        
         137
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::em2Run | 
Counter keeps running when in EM2.
        Definition at line
        
         140
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::em3Run | 
Counter keeps running when in EM3.
        Definition at line
        
         143
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::em4Block | 
Block EMU from entering EM4.
        Definition at line
        
         146
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::enable | 
Enable watchdog when initialization completed.
        Definition at line
        
         134
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::lock | 
Block SW from modifying the configuration (a reset is needed to reconfigure).
        Definition at line
        
         154
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel | 
| bool WDOG_Init_TypeDef::resetDisable | 
Disable watchdog reset output if true
        Definition at line
        
         179
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| bool WDOG_Init_TypeDef::swoscBlock | 
Block SW from disabling LFRCO/LFXO oscillators.
        Definition at line
        
         150
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel | 
Select warning time as % of the watchdog timeout
        Definition at line
        
         167
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
| WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel | 
Select illegal window time as % of the watchdog timeout
        Definition at line
        
         173
        
        of file
        
         em_wdog.h
        
        .
       
Referenced by WDOGn_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_wdog.h